全 2903 件が検索されました。(421 - 440件を表示)

  • カタログ

    ...: 0.1 to 30 s (Set the timer according to the duration of the startup current.) The setting range for the K8DT-AW3 is 10% to 100% of the rated current (i.e., 10 to 100 A). Pass the conductors through the CT five times ...

  • カタログ

    ...Supplementary comments on what to do or avoid doing, to use the product safely. Precautions for Correct Use Supplementary comments on what to do or avoid doing, to prevent failure to operate, malfunction, or undesirable effects on product performance. !CAUTION Doing ...

  • カタログ

    ... avoid doing, to prevent failure to operate, malfunction, or undesirable effects on product performance. !WARNING Electrical shock may occasionally cause serious injury. Confirm that the input voltage is OFF before starting any wiring work and wire all connections correctly. !CAUTION Doing ...

  • カタログ

    ... suddenly from 70% to 120% of the set value and measure the time until the Unit operates. Undervoltage Change the input suddenly from 120% to 70% of the set value and measure the time until the Unit operates. Operating Time Adjust the slide resistor ...

  • カタログ

    ... flash when the set value equals the input value. Use this as a guide to make the setting. The rated input depends on the model and the DIP switch setting. Example: K8DT-PZ1 with DIP switch Set to 200 V The rated input is 200 VAC, ...

  • カタログ

    ... is no specific symbol. Used to indicate prohibition when there is a risk of minor injury from electrical shock or other source if the product is disassembled. Used for general mandatory action precautions for which there is no specified symbol. !CAUTION Doing ...

  • カタログ

    ... avoid doing, to prevent failure to operate, malfunction, or undesirable effects on product performance. !WARNING Electrical shock may occasionally cause serious injury. Confirm that the input voltage is OFF before starting any wiring work and wire all connections correctly. !CAUTION Doing ...

  • カタログ

    ... avoid doing, to prevent failure to operate, malfunction, or undesirable effects on product performance. !WARNING Electrical shock may occasionally cause serious injury. Confirm that the input voltage is OFF before starting any wiring work and wire all connections correctly. !CAUTION Doing ...

  • カタログ

    ... Wiring (Power supply voltage and measurement voltage are shared.) • The Power Monitor has voltage input terminals V1, V2, V3, and VN, which function as both the operating power supply terminals and voltage measurement terminals. • Connect a branch circuit breaker between the voltage input terminals and the wiring ...

  • カタログ

    ... the latest commercial-quality antivirus software on the computer connected to a control/monitor system and maintain to keep the software up-to-date. Security measures to prevent unauthorized access Take the following measures to prevent unauthorized access to our products. • Install physical controls ...

  • カタログ

    ... The simple measurement function can be used to get an approximate power consumption of an installed circuit without wiring and measuring the voltage. Therefore, you must set the voltage and power factors to appropriate levels. • Fixed values are used for the voltage and power factor, ...

  • カタログ

    ... The simple measurement function can be used to get an approximate power consumption of an installed circuit without wiring and measuring the voltage. Therefore, you must set the voltage and power factors to appropriate levels. • Fixed values are used for the voltage and power factor, ...

  • カタログ

    ... Classification (First in the Industry) Three-state Energy Classification with three-color displays lets you know where energy can be saved. 1) Three-state Energy Classification divides the total power consumption into stopped power, standby power, and operating power depending on the power usage conditions ...

  • カタログ

    ... rate of a device can be measured by dividing the power consumption with the measured number of operations or operation time. 1) Three-state Energy Classification divides the total power consumption into stopped power, standby power, and operating power depending on the power usage conditions ...

  • カタログ

    ... M O U S MAT ERIAL T R AN S P O RTATI O N flexible functionality OMRON’s mobile solutions are extremely versatile and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, ...

  • カタログ

    ... for the operate and release values by increasing/decreasing the input voltage. • The LG2 can be used for undervoltage detection by using the RESET knob for the operate value and the SET knob for the release value. The Relay will normally be ON, however, and ...

  • カタログ

    ... applications where pickup and drop-off stands can be used, reducing the need for equipment as well as the risk of injury. All OMRON mobile robots can be managed on the OMRON Fleet Manager platform, which is capable of controlling up to 100 mobile robots ...

  • カタログ

    ... never moves. However preparation is necessary for an accident. 2 Locations for Introducing Measuring and Monitoring Relays and Their Functions Various machines operate at production sites. Such industrial machines are used as the power source for motors and heaters on production lines, ...

  • カタログ

    ... smart camera. Select the appropriate power supply based on the power consumption of the devices. Your device configuration may also require a touch finder, LCD monitor, etc. Be sure to consider all needed devices when selecting the power supply, camera cables, Ethernet cables, and ...

  • カタログ

    ...60 230 140 100 100 6 6.4 16.5 11.5 3G3AX-AL2025/AL2055/AL4025/AL4055/AL4110 Ground terminal (M5) Terminal screw 6-M K D max. E max. W Ro R So S To T W = Terminal width H max. H1 max. X±1 Y±1 A max. C max. Four, J dia. (Cutout) 27 Multi-function Compact Inverter MX2-Series V2 type 3G3AX-AL2110/AL2220/AL2330/AL4220/AL4330 Terminal hole Six, K dia. A max. Ro R ...