全 2903 件が検索されました。(381 - 400件を表示)
- カタログ
...K2 K2 * * Wiring of Inputs and Outputs Signal name Power supply input Terminal name A1, A2 Description of operation The input terminals for power supply. Connect the power source to the A1 and A2 terminals. DC inputs have polarity, ...
- カタログ
...24V Safety Input1 Safety Input2 A2 T21 T22 Reset/ Feedback Input Auxiliary output X1 PLC etc. Motor controller 13 23 37 47 Note: The lock release enable signal must be configured so that it should turn ON after dangerous movement is stopped and safety is ensured for the door to open. Safety Output (Instant aneous) Safety Output (OFFdelay) 14 24 38 48 KM1 KM2 Operation command KM1 KM2 M 15 G9SE Safety Precautions Be sure to read the Common Precautions for Safety Warning at the following URL: http://www.ia.omron.com/. Indication and Meaning for Safe Use WARNING Indicates ...
- カタログ
... appropriate safety system as shown in the following table. Switching function Machine Safety system configuration example Switching function Manual switching Serious injury may possibly occur due to loss of required safety functions. Wire the G9SX properly ...
- カタログ
... Timer ■ Output Methods (Control Methods) Timers are available with relay outputs or transistor outputs. Output types Features Contact (relay) output Relatively large currents can be switched. Either AC or DC load voltages can be used. Transistor output There are no contacts, ...
- カタログ
... as an external signal input device, pay attention to the following points to prevent shortcircuiting due to a sneak current to the transformerless power supply. If a relay or transistor is connected to two or more Timers, the input terminals of those Timers must be wired properly ...
- カタログ
... allowable range. • If a voltage that exceeds the rating is applied, internal components may be destroyed. • Wire all terminals correctly. • Use only the specified wires for wiring. Applicable wire gauge: AWG18 to AWG22 (for stranded wire) • Install and clearly label a switch or circuit breaker ...
- カタログ
... following points to prevent short-circuiting due to a sneak current to the transformerless power supply. t: Mounting clearance (mm) 37 H3DS If a relay or transistor is connected to two or more Timers, the input terminals of those Timers must be wired properly ...
- カタログ
... damaged if you insert the screwdriver straight in. • Do not allow the flat-blade screwdriver to fall out while it is inserted into a release hole. • Do not bend a wire past its natural bending radius or pull on it with excessive force. Doing ...
- カタログ
... used by opening terminals 21 and 22. When using an external resistor (1 MΩ for H3FA-A/-SA, 3 MΩ for H3FA-B/ -SB), connect it between terminals 21 and 23. 4 H3FA Operation Timing Charts and External Connections Wire the inputs ...
- カタログ
... operating environment, the setting dial, indicators and plastic parts may deteriorate faster than expected, causing the indicators to fail. Periodically perform inspections and replacements. We recommend that you use a surge absorber if surge voltages may occur. When you dispose of the Timer, do ...
- カタログ
...34.8 44.3 1.3 4.8 16.5 7 H5F Precautions Refer to Safety Precautions for All Timers. Operating Environment !CAUTION Do not touch any of the terminals while power is being supplied. Doing so may result in electric shock. Be sure to mount the terminal cover after wiring. Do not use the Time Switch in locations subject to flammable or explosive gases. Doing ...
- カタログ
... (such as a breaker, or fuse) for the power supply of the Time Switch. 18.When using heaters, be sure to use a thermal switch for the load circuit. 19.Always maintain the load current within specifications. 20.Use a switch, relay, or other contacts ...
- カタログ
...H7EC Reset Key Reset the count value. Not operable under key-protect. Counting speed switch Key-protect Switch For all models except for H7EC-NFV-@. If the counting speed setting is changed, the present value will not be held and ...
- カタログ
... loose or excessively tightened. If the knurled screws are excessively tightened with pliers or other tool, damage may result. The panel cutout is as shown below (according to DIN 43700). The mounting panel thickness must be 1 to 5 mm. Mount the Counter ...
- カタログ
.... No. W500). Precautions for Correct Use Read the following precautions carefully before using an SD Memory Card. For details, refer to user's manuals for the device on which the card is mounted. Formatting The SD Memory Cards are formatted and shipped, ...
- カタログ
... and build to eliminate faults caused by complexity and, with other unique design features, to maximize uptime and reduce costs. The future will be IT driven: Omron’s IPC platform will make you part of it. Simplicity improves reliability Unnecessary complexity causes problems, ...
- カタログ
... add up to two PCI Express boards. Specifications Industrial PC Platform NY Series NYB1E-£££££ Windows® 10 IoT Enterprise 2016 LTSB (64 bit) CPU Intel® Xeon® Processor E3-1515M v5 (2.8 GHz/3.7 GHz, 4 cores/8 threads) Main memory ...
- カタログ
...ロン製産業用PCプラットフォーム NYシリーズの 仕様 商品名 Intel® Xeon® Processor E3-1515M v5 (2.8GHz/3.7GHz、4Core/8Thread) メインメモリ SO-DIMM 最大32GB(ECC対応)、DDR4 SDRAM ストレージ Intel® RST機能にてRAID0/1構成(Hot Swap除く) キッティングサービスで対応 内蔵ポート Ethernet ×3、USB 2.0 ×2、USB 3.0 ...
- カタログ
..., visit https://io-link.com/en/ Third party compatibility All IO-Link sensors have an IODD Controller Controller (Input Output Data Description) file that lists the component type and what parameters need to be set. IODD files are a global standard, ...
- カタログ
...it easy to integrate vision systems and switch from horizontal to vertical centering modes. The Robot Vision Manager is supported by sample wizards providing quick & easy setup for basic applications. CAD models of the hopper and feeder can be integrated into the ACE platform, ...