全 2903 件が検索されました。(501 - 520件を表示)

  • カタログ

    ... scale value. SDV-F@@ Voltage multiplying factor setting: The voltage multiplying factor is selected according to the maximum and minimum factors and a sticker is attached. The calculation method is as follows: The PICK UP index scale value is between 1.0 and 3.0, ...

  • カタログ

    .... when it is stopped by the relay operation. 4. Turn off SW2. Open-phase 1. Open (burn-out) any one of the Current Converter input 1. Open (burn-out) any one of the Current Converter input phases. Adjust the voltage regulator ...

  • カタログ

    ...[-] Safety Precautions for Sensing Bands and Liquid Leakage Point Sensors Safety Precautions for Sensing Bands and Liquid Leakage Point Sensors CSM_SensingBand_CN_E_1_2 !WARNING Do not touch the terminals while power is being supplied. Doing ...

  • カタログ

    ... rises, the image quality will deteriorate and cause noise problems. IMX991 and IMX991 adopted cameras with a thermoelectric cooling element to improve image quality and reduce noise problems by performing more efficient heat dissipation. The OMRON SENTECH camera has a special heat dissipation design ...

  • カタログ

    ...-VSP2 5M 5m FJ-VSP2 10M 10 m Note. When wiring a camera, be sure to refer to its specification document to check its external connector specifications. Incorrect wiring can lead to failure. Note. Do not connect the shell, for doing ...

  • カタログ

    ... Shape Sectional Area Measurement Shape2D_Area 2D Shape Sectional Area Measurement 2 Shape2D_Area2 2D Shape Comparison Measurement 2D Shape Comparison Measurement 2 Shape2D_Compare Shape2D_Compare2 Converts from the line measurement data to the 2D shape data. Correction is performed ...

  • カタログ

    ... Manual To learn how to set-up of Confocal Fiber Type Displacement Sensor of ZW8000/7000/5000 series Describes how to set-up of Confocal Fiber Type Displacement Sensor of ZW-8000/7000/5000 series. Z930 NX-SL@@@@ NX-SI@@@@ NX-...

  • カタログ

    ... for use of all OnRobot grippers. Each kit includes: - Quick OnRobot Changer robot side - Screws - Torx key Quick OnRobot Changer - Tool side 102014 Manual tool changer to attach on the tool side. (All OnRobot grippers have this component integrated, ...

  • カタログ

    ...complicated safety calculations to set up a safe application. A landmark is a physical object that can be recognized by the robot’s built-in camera, and acts as a beacon to help the robot navigate. The robot uses a Landmark as a reference point ...

  • カタログ

    ... for use of all OnRobot grippers. Each kit includes: - Quick OnRobot Changer robot side - Screws - Torx key Quick OnRobot Changer - Tool side 102014 Manual tool changer to attach on the tool side. (All OnRobot grippers have this component integrated, ...

  • カタログ

    ... CNC machines, injection molding machines, stamping and punch pressers, grinding, and cutting machines. Our robots can pick up, inspect, and sort products directly from a moving conveyor belt. Our robots are highly flexible and have a small footprint, ...

  • カタログ

    ...Low contrast Distortion Dots 1 Distance Variations There are two models in the lineup to let you select the field of view or installation distance that is best for 93 the equipment type. Both models are the same size, ...

  • カタログ

    ...strobe lighting. Strobe lights are triggered using Output 3 on the M12 IO connector through a flying leads cable. Omron also offers a line of Smart Lights that can be used in continuous or strobed mode. NERLITE Smart Series Lights have a built-in strobe controller, ...

  • カタログ

    .... Raster scanning enables reading Bar Codes even if they are partially dirty or missing. Dirt Wear Blurring Shiny background Inconsistent background Dots Resists Ambient Light Interference Operation is possible with ambient illumination of up to 80,000 lx (sunlight), ...

  • カタログ

    ... before using it. 6. The DC power supply must be within the specified rating (24 VDC +10%/−15%). 7. Do not reverse the power supply connection. 8. Do not insert water, wire, etc., into any of the gaps in the case. Doing ...

  • カタログ

    ..., such as accidentally mounted, automatic mold checks performed mechanical flags, enables the build-out of maintenance-free before the molding process can prevent production of defects. systems with very few failures. 6 Massive System Variation We provide a wide variety of RFID components ...

  • カタログ

    ...No interference of wiring helps improve workability and safety Improved wiring workability by unified I/O terminal positions on the top and bottom Inputs Outputs BEFORE Hard wiring due to mixed I/O terminals located on the top and bottom Unified method ...

  • カタログ

    ...: 120 ms Vibration settling time: 100 ms 20 x 20 = 400 chips per pallet Resonance frequency of pallet: 30 Hz Vision inspection Handling time per pallet: 220 ms per chip x 400 chips = 88 s Application The XY stage moves a pallet ...

  • カタログ

    ... remove the two screws to mount the switch in any of the four possible orientations. If changing the direction of the head, pay attention to the orientation of the operation plunger. Roller Lever Bolt Set Position Marker Plate Set the indicator needle ...

  • カタログ

    ...actuator) to increase resistance to oils, chemicals, and weather. Cables attached. Uses an airtight built-in switch. The case cover and box interior are molded from epoxy resin to increase the seal. The cover cannot be removed. The SC connector can be removed, ...