全 2903 件が検索されました。(521 - 540件を表示)

  • カタログ

    ... colors correspond to the pin clamp numbers that are identical to the connector pin numbers. Insertion Pin Block Pin Clamp Key groove Key groove Key XS2C use XS2G use 6±0.5 • Tentatively insert the pins to the pin block holes ...

  • カタログ

    ...humidity can cause bad connections and damage through corrosion, leading to degraded performance, therefore do not use these products in such environments. • Do not pull on the Connectors or cables with excessive force. • Do not step on or place any objects on the Connectors. Doing ...

  • カタログ

    .... Connector Connection and Disconnection • When connecting or disconnecting Connectors, be sure to hold the Connectors by hand. • Do not hold the cable when disconnecting Connectors. Use after confirming the direction of the polarity key groove. • Do not touch wiring with wet hands. Doing ...

  • カタログ

    ...For 5 to 8-mm dia., just remove the tabbed, waterproof bushing. *A 5-mm dia. cable connects with or without the bushing. Anyone... Visual confirmation is possible. ...with no torque management The tightened ti position is clear, ...

  • カタログ

    .../O unit XW2K series For PLC Connection P.2 Flexibly achieve the smallest configuration by combining with common terminal blocks For PLC Connection • This product is the industry’s smallest*1 and is mountable in two ways (vertical and horizontal)*2, ...

  • カタログ

    ...2 1 37 38 4 3 21 22 20 19 19 20 22 21 3 4 38 37 1 2 40 39 Triangular mark Note: Wire the connector terminals 1:1 so that the connector terminal numbers coincide. Cable length L (m) L 4 XW2R Models for Connection to OMRON PLCs with power supply terminals e-CON Type Ordering Information Appearance I/O Points Input/Output 16 Input Model Dimension A (mm) XW2R-N16GD-C1-COM 98.5 XW2R-N32GD-C1-COM 32 186.7 XW2R-N32GD-C2-COM Ratings and Specifications Power supply terminal block: 4 A/16 poles ...

  • カタログ

    ...Precautions for Correct Use Wiring Precautions • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...

  • カタログ

    ...Precautions for Correct Use Wiring Precautions • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...

  • カタログ

    ... icing) *3 Note: This cable is for fixed parts. Do not use it for moving parts. *1. Contact resistance for the Connector. *2. Dielectric strength for the Connector. *3. However, when bending the cable to perform wiring, maintenance, and other work, do ...

  • カタログ

    ...Precautions for Correct Use Wiring • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...

  • カタログ

    ...Precautions for Correct Use Wiring • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...

  • カタログ

    ... icing) *3 Note: This cable is for fixed parts. Do not use it for moving parts. *1. Contact resistance for the Connector. *2. Dielectric strength for the Connector. *3. However, when bending the cable to perform wiring, maintenance, and other work, do ...

  • カタログ

    ... Required The retightening that is required for screw terminal blocks is not required for Push-in Plus terminal blocks. Your work load is reduced not only when wiring, but also for inspections, delivery (shipping), and maintenance. Safety The structure provides finger protection ...

  • カタログ

    ... identify wiring. (Material: PA resin, blank) XW5@-P4.0-@ Note: 1. Different models are used for the top and side surfaces. 2. There is no place to mount the Top-surface Labels on Two-tier Terminal Blocks with a width of 3.5 mm, ...

  • カタログ

    ... to 14 10 mm • Do not drop the Terminal Block. Terminal Block functionality may be inhibited. • Terminal Block is designed to satisfy the functions when mounting on the DIN Track. Always mount on the DIN Track. • Do not exceeds the ratings. Doing ...

  • カタログ

    .... 12x the conventional sensitivity 2.5x 10x the conventional inclination tolerance the conventional speed Measurement can be performed at a stable level in a large amount of ambient light, even on objects that do not reflect light ...

  • カタログ

    ... maximum and minimum air volume and feedback time can be set to any desired values. Once a cleanliness threshold has been exceeded, the level of cleanliness can be increased in a short time by applying the maximum air volume. Constant feedback is provided ...

  • カタログ

    ...combustion or rupture may occasionally result in serious injury. Do not disassemble, deform under pressure, heat to 100°C or higher, or incinerate the battery. CAUTION Do not use the Power Monitor in locations where flammable or explosive gases are present. Doing ...

  • カタログ

    ... manuals for the right page. Previous displays LD ON LD ON LD ON LD ON 6 ZP-L display Required action as well as error displayed in multiple languages PATENT PENDING *1 ZP-L’s display supports four languages, ...

  • カタログ

    ... not expose your eyes to the laser radiation either directly or indirectly (i.e., after reflection from a mirror or shiny surface). The laser radiation has a high power density and exposure may result in loss of sight. Do not disassemble the product. Doing ...