全 2903 件が検索されました。(461 - 480件を表示)
- カタログ
...-series NX102 CPU Unit, NX Units, and an End Cover. Up to 32 NX Units can be connected. Safety CPU Unit NX-SL3@@@ NX-series NX102 CPU Unit System Unit NX-PF@@@@ Safety I/O Units NX-SI@@@@/ NX-SO@@@@ NX Units (32 Units max.) End Cover SD Memory Card Built-in EtherNet/IP Port (PORT1) Built-in EtherNet/IP Port (PORT2) Built-in EtherCAT Port (PORT3) FSoE Up to 32 Units can be mounted to each CPU Rack. For restrictions of the NX unit, refer to NX-series NX102 CPU Unit Hardware User’s Manual (Cat. No. W593)....
- カタログ
...-series NX102 CPU Unit, NX Units, and an End Cover. Up to 32 NX Units can be connected. Safety CPU Unit NX-SL5 NX-series NX102 CPU Unit System Unit NX-PF Safety I/O Units NX-SI/ NX-SO NX Units (32 Units max.) End Cover SD Memory Card Built-in EtherNet/IP Port (PORT1) CIP Safety Built-in EtherNet/IP Port (PORT2) CIP Safety Built-in EtherCAT Port (PORT3) FSoE Up to 32 Units can be mounted to each CPU Rack. For restrictions of the NX unit, refer to NX-series NX102 CPU Unit Hardware User’s ...
- カタログ
... sensor or when there is a difference in measured value from other measuring instruments. One-point correction and two-point correction methods are provided. All models Input Digital Filter This function sets the time constant applied to the first-order lag operation filter ...
- カタログ
...H1.5/14 1.5 (#16) H1.5/16 * Some AWG 14 wires exceed 2.0 mm2 and cannot be used in the screwless clamping terminal block. When you use any ferrules other than those in the above table, crimp them to the twisted wires ...
- カタログ
....) CRIMPFOX 6 (0.25 to 6 mm2, AWG24 to 10) 2.0 * * Some AWG14 wires exceed 2.0 mm2 and cannot be used in the FG terminal block. When you use any ferrules other than those in the above table, crimp them to the twisted wires ...
- カタログ
...B Battery slot Allows a separately-sold backup battery to be mounted into the CPU Unit. C SD Memory Card connector Connects the SD Memory Card to the CPU Unit. D SD Memory Card power supply switch Turns OFF the power supply ...
- カタログ
...Connects the SD Memory Card to the CPU Unit. B DIP switch Used in Safe Mode *1 or when backing up data *2. Normally, turn OFF all of the pins. C SD Memory Card power supply switch Turns OFF the power supply ...
- カタログ
... c u r a te a n a l ys i s r e q u i r e s fas t a n d a c c u r a te Defect occurred collection of high‐resolution data in chronological order, the amount of data is so large that the data transfer to databases becomes a bottleneck. N X5 Temperature, pressure, flow rate With approximately four times the data transfer capability of the previous model Time It takes time to transfer data and feed back analysis results, resulting in low yield. *1 , NX5 can transfe r all of ...
- カタログ
...) (O) (P) (F) (Q) (R) (S) Letter Name Function A SD Memory Card connector Connects the SD Memory Card to the CPU Unit. B SD Memory Card power supply switch Turns OFF the power supply so that you can remove the SD Memory Card. C Slider The slider is used to slide the X Bus Unit when installing or removing. D DIN Track mounting hooks These hooks are used to mount the CPU Unit to a DIN Track. E Terminal block The terminal block is used for wiring for the Unit power supply and grounding cable. F Unit hookup ...
- カタログ
... control system demands increasing levels of flexibility. The NX I/O enables connection with various controllers through the global standard network, which expands system configuration possibilities. Modular remote I/O systems offer flexibility in I/O configuration and a wide choice off signal types and performance levels ...
- カタログ
... Machine Controller NY5@@-1 CSM_NY5__-1_DS_E_5_8 The future will be IT driven, we make you part of it Our IPC Machine Controller combines proven machine automation with the freedom to use PC technology: working together but independently. ...
- カタログ
... Switches D4ER-□ N E3ZR-C Oil-resistant Proximity Sensors E2ER/E2ERZ Proximity Sensors and Photoelectric Sensors, Limit Switches, Connectors Previous Models Cable Sheath: PVC or PUR Water-insoluble cutting oils deteriorate PVC and water-soluble cutting oils deteriorate PUR, ...
- カタログ
... or maintenance of the machinery and the hazards involved.” The machine requirements The main unit must be securely mounted and its cable connectors must be tightly attached. The OS32C must not be mounted behind glass or within a secondary enclosure. Failure to do ...
- カタログ
... and wiring The series meets the requirements for PELV circuits as specified by EN/IEC 60204-1, which are required to supply power to control circuits. In general, using a PELV circuit as a power supply output requires grounding a negative terminal, ...
- カタログ
...Transport conveyor motor insulation degradation monitoring Heater Condition Monitoring Device K7TM Insulation Resistance Monitoring Device K7GE-MG Error Mode Quality defects in electronic parts due to heater burnout Detection principle Firing furnaces operate 24 hours a day, ...
- カタログ
...degradation 4 Error Mode Electric shock accidents and fire caused by short circuit due to degradation of machining motor insulation Detection principle When coolant or sawdust penetrate the inside of a motor, the insulation resistance value of the motor changes, ...
- カタログ
...K7DD Insulation Resistance Monitoring Device K7GE-MG Error Mode Quality defects due to presence of foreign matter Detection principle Load changes occur when stirring blades come into contact with foreign matter. This will appear as variation in power, ...
- カタログ
... r n a l l y. E v e n i f l o c a l p e r s o n n e l w a n t t o c a r r y o u t maintenance, they lack the know-how to do so. Therefore, there is a risk that equipment will suddenly fail, and production will not be able to continue. AFTER By digitalizing maintenance, degradation of facility equipment can be monitored and scheduled maintenance that does not affect the production floor can be performed By digitalizing maintenance activities that could previously only...
- カタログ
...Transportation • Do not use a Socket that has fallen to the floor or ground. The performance of a Socket that has been dropped may be reduced. • Do not drop the Socket or subject it to abnormal vibration or shock during transportation or mounting. Doing ...
- カタログ
... supported Supported *8 Supported *1. Production was discontinued. *2. The function to show the serial number controlled by OMRON in 1018h-04 hex. *3. Setting the communications cycle to 500 μs or less does not enable the FIR filter function, although doing ...