全 2903 件が検索されました。(401 - 420件を表示)
- カタログ
... a phase failure protection function as standard, if all phases are not energized, the operating current may be low and unnecessary operation may occur. Perform either (A) or (B) when applying the product to single-phase motor circuits or DC circuits. (A) Connect the wires ...
- カタログ
.... Start-up Detecting Circuit (Instantaneous Type) Instantaneous-type models output a trip signal instantaneously when the motor current exceeds the overcurrent operating value (115% of the set current value). At the start of motor operation, a starting current several times the rated current flows and ...
- カタログ
... VAC K2CU-F10A-FGS K2CU-F20A-FGS K2CU-F40A-FGS K2CU-F80A-FGS Note: A model with a gate input terminal is required to combine the K2CU with a temperature controller that uses PID control for temperature control of a heater. To do ...
- カタログ
... detect human forms either directly or indirectly for the purpose of ensuring safety. Do not use this product as a detection device to protect people. Never use this product with AC power supply or with voltage in excess of the rated voltage as doing ...
- カタログ
... set as desired. If the decimal point is to be displayed, it is necessary to consider the number of digits to be displayed past the decimal point when setting the scaling display value. Note: When pulse input is used, the base point is the 0 point, ...
- カタログ
...Y92A-49N Rubber Packing K32-P1 If the rubber packing is lost or damaged, it can be ordered using the following model number: K32-P1. (Depending on the operating environment, deterioration, contraction, or hardening of the rubber packing may occur and ...
- カタログ
... the K3MA-J. Rubber Packing K32-P1 If the rubber packing is lost or damaged, it can be ordered using the following model number: K32-P1. (Depending on the operating environment, deterioration, contraction, or hardening of the rubber packing may occur and ...
- カタログ
...Y92A-49N Rubber Packing K32-P1 If the rubber packing is lost or damaged, it can be ordered using the following model number: K32-P1. (Depending on the operating environment, deterioration, contraction, or hardening of the rubber packing may occur and ...
- カタログ
... prevent multicast packets from reaching the K6CM. *4. Can be used only with EIP CPU version 1.2 or higher. *5. Except when a magnet mounting attachment is used. *6. Even if the motor is not moving, the value of velocity may appear slightly, ...
- カタログ
... Vibration & temperature type only) The Acceleration alarm, velocity alarm threshold setting guide is displayed on the right side of the Alarm Settings Screen for K6CM-VB. You can automatically set the threshold by entering the Motor shaft diameter, Rotation speed, capacity and ...
- カタログ
... pump, causing an air lock * K6CM does not output electric current waveform data. Alarm threshold degradation level 1 for this application (examples) Alarm threshold (Warning) 30 Alarm threshold (Critical) 50 Expected implementation effects Detects air locks in pumps and other abnormal conditions ...
- カタログ
... not be correct if the direction is wrong. • Release the split/fastening hook and clamp the special CT on the line for each phase and then press the hook firmly until you hear it lock into place. • Do not ground the special CT. Doing ...
- カタログ
... production that can react to such changes. We propose a new form of maintenance that watches all kinds of production facilities and equipment without relying on human senses. Developing a people-friendly style of Condition Based Maintenance Reactive maintenance has been the standard maintenance strategy ...
- カタログ
... Is a Single-Phase/3-Phase Induction Motor (Direct Connection to Commercial Power Supply) Install a contactor between the power line and the motor. Do not connect any other device such as a transformer or a filter between the contactor and the motor. Doing ...
- カタログ
... K7GE is capable of measuring insulation resistance each time under the same conditions with high reproducibility. Delivers safe and secure measurement by monitoring the operating status of the measurement target. In addition, increasing its frequency of automatic measurement allows for understanding the degradation trend, which was ...
- カタログ
... connect to terminals 2, 3, and 4 on the Unit. Connect the Sensing Band between terminals 2 and 4. 12 to 24 VDC * Output Circuit Examples The NPN open-collector output of the K7L-U/UB is isolated from the internal circuits by a photocoupler, ...
- カタログ
..., refer to your OMRON website. Overview The K7TM is a device for supporting condition monitoring of heaters by measuring the resistance values of the heaters. The Unit calculates a resistance value by measuring the voltage at both ends of the heater and its current, ...
- カタログ
... depend on skilled personnel. Ready to perform maintenance based on the degree of deterioration from heater resistance values The K7TM can monitor the state of the heater by the rate of change of the heater resistance value and monitor the state and tendency of each heater, ...
- カタログ
.... 16.Do not install the product near equipment that generates high frequencies or surges. 17.The product may cause incoming radio wave interference. Do not use the product near radio wave receivers. 18.Install an external switch or circuit breaker and label it clearly ...
- カタログ
...: 0.1 to 30 s (Set the timer according to the duration of the startup current.) The setting range for the K8DT-AS3 is 10% to 100% of the rated current (i.e., 10 to 100 A). Pass the conductors through the CT five times ...