全 2903 件が検索されました。(361 - 380件を表示)
- カタログ
... Visual Studio® and Application Producer easily. Macro Processing Items You can implement even advanced calculations on the processing flow as a Macro processing items easily. It allow you to edit the program on the controller and the compiling is not necessary. ...
- カタログ
...-brightness Models FL Series Maintaining light intensity even with long wiring distances Twice* Camera Brighter Light L Light 10-m long, distances result in voltage drops and lower light intensity. Power is supplied through the Camera, ...
- カタログ
... Specular Reflections Polarizing Filter A polarizing filter is included to cut specular reflection from glossy surfaces. This enables stable code reading even for metallic or other glossy surfaces. Communications with Host Devices Ethernet Connection The compact body also provides an Ethernet connector ...
- カタログ
...Only 2 Controller Camera Console Monitor Lens Lighting Sensor Monitoring and Setup Tool Touch Finder or Touch Finder for PC Power supply of lighting Easy Installation The camera and lighting have been integrated into a single unit, ...
- カタログ
... polarity of the positive and negative output terminals. Close Mounting of Multiple Relays If multiple Relays are mounted side by side, be aware that the outer wall of each SSR works as a heat sink. The SSR casing serves to dissipate heat. Install the Relays ...
- カタログ
... polarity of the positive and negative output terminals. Close Mounting of Multiple Relays If multiple Relays are mounted side by side, be aware that the outer wall of each SSR works as a heat sink. The SSR casing serves to dissipate heat. Install the Relays ...
- カタログ
... of the Thyristor Module and heat sink. Apply a thin, even coating of new grease (provided) to the contact surfaces, and tighten the screws labeled "D" tentatively and then tighten them evenly to 2.5 to 4.0 N·m. The silicon grease should be thin enough ...
- カタログ
... G3PJ units and a system of three closely mounted conventional OMRON G3PE-245B (or G3PE-545B) units, with both systems carrying a current of 25 A at an ambient temperature of 40°C. Better Temperature Characteristics and Reinforced Insulation for Safety Standard Compliance UL-listed components, ...
- カタログ
... socket type, appearance, and dimensions. 2. Use the Short Bars for crossover wiring within one Socket or between Sockets. 3. Use the short bars on the lower section of the socket. When using the short bars on the upper section of the socket, insert them ...
- カタログ
... socket type, appearance, and dimensions. 2. Use the Short Bars for crossover wiring within one Socket or between Sockets. 3. Use the short bars on the lower section of the socket. When using the short bars on the upper section of the socket, insert them ...
- カタログ
.... The switch settings are read only when the power supply is turned ON. • Use a flat-blade screwdriver to set the switches and be sure not to leave a switch set between two settings. Communications Unit Number Set a communications unit number on SW1 ...
- カタログ
... (x103 operations) Switching current (A) 4,000 Number of switching operations (×104 times) Note: 1. Measurement values taken from production line samples have been plotted in graphs to provide this data. Use this data only as a guide. Relays are mass-produced, ...
- カタログ
... 68 × 80 × 44 mm (W × H × D, when mounted upright). • Independent contacts and short bar allow easy common connections. • The common can now be connected with a short bar in the G70D-SOC08. • No tools are required to remove Relays, ...
- カタログ
... from the side wall. • Turn the screws further counterclockwise, remove the screws, and then remove the relay block. Fig. 2 Mounting the expansion terminal block • Insert the catches on the expansion terminal block into the mounting holes in the terminal block, and slide ...
- カタログ
... from the side wall. • Turn the screws further counterclockwise, remove the screws, and then remove the relay block. Fig. 2 Mounting the expansion terminal block • Insert the catches on the expansion terminal block into the mounting holes in the terminal block, and slide ...
- カタログ
... injury or in property damage. Supplementary comments on what to do or avoid doing, to use the product safely. !CAUTION Do not pass currents of 6 A or more when using this product in combination with the P7S-14F/14P/14A Socket. Doing ...
- カタログ
... the flat-blade screwdriver is inserted straight in. • Do not allow the flat-blade screwdriver to fall when you are holding it in a release hole. • Do not bend a wire past its natural bending radius or pull on it with excessive force. Doing ...
- カタログ
... for Input Blocks (XW2Z-R) and Cables for Output Blocks (XW2Z-R). Be sure to purchase the correct Cable for the application. Microload Switching Input Relays (DC coil type) and I/O SSRs (DC input type) can be mounted onto an Output Block. Doing ...
- カタログ
...-44 and terminals 53-54 are OFF-delayed outputs. *1 Wiring of Inputs and Outputs Signal name Terminal name Description of operation The input terminals for power supply. Connect the power source to the A1 and A2 terminals. DC inputs have polarity, ...
- カタログ
...4 G9SA Wiring of Inputs and Outputs Signal name Power supply input Terminal name A1, A2 Description of operation The input terminals for power supply. Connect the power source to the A1 and A2 terminals. DC inputs have polarity, ...