全 2903 件が検索されました。(341 - 360件を表示)
- カタログ
... product to break or burn; During operating, if applying voltages below the rated voltage range may cause the output to shut down. At that time, please restart the power. (2) Avoid wiring the product's cables parallel to power lines or highvoltage lines. Doing ...
- カタログ
... 20004 20003 00003 20004 00002 20003 Converts gray code to binary (CIO 200). Sets the unused bits (10 to 15 bits) of CIO 200 to unused (always 0). 20300 20301 20302 20002 Resolution is 720, so 152 is subtracted. No subtraction would be necessary for resolution of 256 or 1,024. If resolution was 360, 76 would be subtracted. TABLE COMPARE Instruction BCMP(68) If the Encoder value (CIO 202) 202 is within a range in the DM6200 conversion table set in DM 203 6200 to DM 6231, the corresponding bit in CIO 203 will turn ON. 01000 SUB(...
- カタログ
... and response frequency. There is a tendency that the residual voltage increases or a waved distortion occurs, due to changes in the cable resistance and the capacity between cables. • Do not lay the cables in parallel with high-voltage lines or power lines. Doing ...
- カタログ
... center Problems [Tool gripping force declines due to hydraulic oil leak] • Hydraulic oil temperature rises with repeated tool changes. • Pipe packing deteriorates, resulting in hydraulic oil leak. • Oil pressure reduction causes reduction in processing quality. • The hydraulic pressure system is divided into multiple sections, ...
- カタログ
...Safety Precautions Be sure to read the precautions for E9NC-T in the website at: http://www.ia.omron.com/. Sensor Heads WARNING Do not forcibly bend or pull the cables. Do not put a heavy object on them or heat them. Doing ...
- カタログ
... emitter (GaAs infrared LED) and receiver (Si photo IC) are positioned across from each other inside the sensor and light is received when there is no sensing object. When the sensing object presses the actuator, the light path between the emitter and receiver is broken ...
- カタログ
... to the Safety Precautions on page 5. For the most recent information on models that have been certified for safety standards, refer to your OMRON website. Features Mount Using M2 or M3 Screws The EE-SX95 can be mounted using M2 or M3 screws, ...
- カタログ
...Built-in Thermal Shutdown Circuit Control output 2 on models with NPN outputs is protected from output overcurrents by a built-in thermal shutdown circuit. Display Two Outputs: Light-ON and Dark-ON All models provide both a light-ON and dark-ON output ...
- カタログ
...exceeding the operating voltage range. Applying any excessive voltage or supplying AC power (100 VAC or higher) to a DC-type sensor may cause the Sensor to explode or burn. Load Short-circuit Do not short-circuit the load. Doing ...
- カタログ
... kbps 6 Set to ON to display the output status on the operation indicators. OFF: The operation status is displayed (PWR, RUN, ERR, and ALM). ON: The output status is displayed (outputs 1, 2, 3, and 4). Note: Normally keep this pin set to OFF ...
- カタログ
...[-] Safety Precautions for Electrodes and Electrode Holders Safety Precautions for Electrodes and Electrode Holders CSM_ElectrodeCommodity_CN_E_3_3 ● Electrodes must be cleaned. !WARNING Do not touch the terminals while power is being supplied. Doing ...
- カタログ
...6 Easy Integration with IT Systems Reduces wasted time and movement by continuously looking ahead to anticipate which robots will be best positioned for upcoming tasks. Performs updates automatically across the entire fleet. Enterprise Manager can connect to your MES, ERP and WMS ...
- カタログ
..., refer to Mounting Method in the operation manual packaged with the humidity sensor or temperature/humidity sensor. 5. When turning on the power supply, set the warm-up time as three seconds or more. 6. Ensure sufficient space around the main unit case ...
- カタログ
...(Refer to Dimensions on page 1.) Sensing Band Sticker Note: 1. When using the F03-26PES (adhesive-tape model), be sure to wipe all moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do ...
- カタログ
...(Refer to Dimensions on page 2.) Sensing Band Sticker Note: 1. When using the F03-26PES (adhesive-tape model), be sure to wipe all moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do ...
- カタログ
...Remarks 2 for an emitter, 2 for a receiver, total of 4 per set F39-LJ1 (provided with the F3SJ) F39-LJ2 Use these small-sized brackets when performing side mounting 2 for an emitter, with standard mounting brackets, ...
- カタログ
... specified symbol. WARNING Serious injury may possibly occur due to breakdown of safety outputs. Do not connect loads beyond the rated value to the safety outputs. Serious injury may possibly occur due to loss of required safety functions. Wire F3SP-B1P properly ...
- カタログ
...SW 1-1 SW 1-2 OFF OFF All lighting (All six indicators light.) ON OFF All flashing (All six indictors flash simultaneously.) OFF ON Elevator-like lighting (Two adjacent indicators simultaneously light ...
- カタログ
... in Japan. (As of January 2023) 6 Breaking the challenge of emptying all bins with less blind spots There are blind spots where a fixed camera cannot detect parts inside the bin. To detect these parts, an operator must reposition items in the bin ...
- カタログ
...Smart Value, Smarter Vision Powered by AI 3 Setup completed in just a few minutes Intuitive UI for effortless use How-to Video How-to Video Presence/Product Detection/Product type Defect Check The AI Detection Camera is ...