全 2903 件が検索されました。(321 - 340件を表示)

  • カタログ

    ...high resistance to cold environments. Improved Matching of Optical Axis and Mechanical Axis for Through-beam Models and Retro-reflective Models 30 m mechanical 2.5° max. axis The offset between the optical axis and the mechanical axis is kept within ±2.5°, ...

  • カタログ

    ... indented mounting portion Protruding portion Slit Lower mounting Sensor intended portion Mounting method 1. Hook the upper protruding portion of the Slit to the upper indented mounting portion of the Sensor and adjust the position of the Slit ...

  • カタログ

    ... Protection This Sensor is equipped with load short-circuit protection, but be sure to not short circuit the load. Be sure to not use an output current flow that exceeds the rated current. If a load short circuit occurs, the output will turn OFF, ...

  • カタログ

    ... Protection This Sensor is equipped with load short-circuit protection, but be sure to not short circuit the load. Be sure to not use an output current flow that exceeds the rated current. If a load short circuit occurs, the output will turn OFF, ...

  • カタログ

    ...-C features a simple shape and structure, and yet provides IP67 protection and oil resistance (oil resistant to OMRON in-house standard). This performance exceeds any previous models from OMRON. The protective structure eliminates the need for screws to hold a cover, ...

  • カタログ

    ... Protection This Sensor is equipped with load short-circuit protection, but be sure to not short circuit the load. Be sure to not use an output current flow that exceeds the rated current. If a load short circuit occurs, the output will turn OFF, ...

  • カタログ

    ... Protection This Sensor is equipped with load short-circuit protection, but be sure to not short circuit the load. Be sure to not use an output current flow that exceeds the rated current. If a load short circuit occurs, the output will turn OFF, ...

  • カタログ

    ... your OMRON website. Be sure to read the “Safety Precautions” on page 10. Features Can be Used as Safety Function of PLc/Safety Category 2 in combination with a Safety Controller (G9SP-series/NX-series Safety Control Unit). G9SP E3ZS NX-SL/SI/...

  • カタログ

    ... E4E2 needs a maximum of 100 ms to be ready to operate after the E4E2 is turned ON. If power is supplied to the E4E2 and the load independently, be sure to turn ON the E4E2 first. • Installation Mounting Mount the Emitter and Receiver ...

  • カタログ

    ...safety standards, refer to your OMRON website. Application Examples Detecting slackness in sheet materials Detecting liquid levels Remotely detecting LCD wafers Detecting dies Features  High-precision detection with a wide range of measurements.  The Sensor is ultrasonic, ...

  • カタログ

    ... (mm) 11.5 11.5 15 C (mm) 10 10 13 Brass pipe Screw Shielded glass-wool lead wire Installation Example Cut a thread into the workpiece, and screw in the thermocouple while pushing in so that the tip makes complete contact. End Workpiece Note: E52-CA1DY with the same shape and multiple element wires are also available (E52-CA1DY-40). Refer to page 34 for details. Protective tubing length (mm) Lead wire length (m) Element type: K (CA) Element type: J (IC) Model M6 screw M8 screw W1/4 screw 1 E52-CA1DY M6 1M E52-IC1DY M6 ...

  • カタログ

    ... mm E5EC-T: 18 mm E5CC-T: 15.2 mm Three-level Display that is easy to understand.*2 You can display the PV (white) and the SV (green) along with the program progression (PRG and SEG (yellow)). These are all visible simultaneously ...

  • カタログ

    ... Setup to Adjustment and Operation. You can perform the following operations with the CX-Thermo. • Setting and saving parameters *USB-Serial Conversion Cable • Logging, browsing, and exporting data (Sold Separately) • Printing parameter lists, and more Also, power is supplied through the Bus Power, ...

  • カタログ

    .... There were therefore some effects on quality. In response to this situation, OMRON developed temperature controllers that includes "adaptive control technology." This makes it possible to detect the changes in the status which will have an effect on quality and to automatically control the temperature ...

  • カタログ

    ... the E5C2 and the load, the supply voltage of the power supply may vary greatly when the load is open or closed if the capacity of the power supply is not large enough. Make sure that the capacity of the power supply is large enough ...

  • カタログ

    ... Terminal Cover: E53-COV19 (sold separately) • USB-Serial Conversion Cable: E58-CIFQ2 (sold separately) • Recommended panel thickness is 1 to 5 mm. • Do not vertically mount Controllers side by side. (Allow mounting clearance between the Controllers.) • To install the Controller ...

  • カタログ

    ...45 3 45 4.5 16.3 9 2 1 11 10 6 6.2 8.7 Note: The Y92A-48G Finger Safe Terminal Cover is also available. Note: Do not use any other types of Sockets. Doing so will adversely affect the accuracy. Applicable Thermistors Hard Protective Cover Use Element Interchangeable Thermistors (E52-THE5A, E52THE6D, and E52-THE6F) to connect to the E5CS-@GU. For details on Sensors, refer to E52. The Y92A-48B Hard Protective Cover is available for the following applications. • To protect the set from dust and dirt. • To prevent the panel from being accidentally touched ...

  • カタログ

    .... 2. The setting protection indicator ( ) and set value indicator ("SV") will be continued even when settings are protected, except when a memory error occurs. 7 E5L Safety Precautions CAUTION Do not touch the terminals while power is being supplied. Doing ...

  • カタログ

    ...3 Brown 12 to 24 V 4 1 2 Black (phase A) White (phase B) Orange (phase Z) Rotary Encoder Blue (0 V) Shield Note 1: Used only to reset the counter using phase Z. When doing so, set the phase ZZ switch to Z and use a Rotary Encoder with an Open-collector Output. 2: When using phase Z, be sure that the width of phase Z is the same as or wider than the width of phase A. 3. Use one of the following Rotary Encoders: E6A2-CW3C, E6A2-CW5C, E6A2-CWZ3C, E6B2CWZ6C, E6H-CWZ6C, E6C2-CWZ6C, or ...

  • カタログ

    .... Do not use the product in excess of the rated voltage. Applying voltages beyond the rated voltage range may cause the product to break or burn. 2. Avoid wiring the product's cables parallel to power lines or high voltage lines. Doing ...