全 2903 件が検索されました。(301 - 320件を表示)
- カタログ
... laser radiation either directly (i.e., after reflection from a mirror or shiny surface). Loss of sight may possibly occur in case of the exposure to laser high power density. (Applicable to the E3C-LD11N/E3C-LR11N) Do not disassemble the product. Doing ...
- カタログ
... indented mounting portion Protruding portion Slit Lower mounting Sensor intended portion Mounting method 1. Hook the upper protruding portion of the Slit to the upper indented mounting portion of the Sensor and adjust the position of the Slit ...
- カタログ
... laser beam has a high power density and exposure may result in loss of sight. Attention Use of controls or adjustments or performance of procedures other than those specified herein may result in hazardous radiation exposure. Do not disassemble the Sensor Head. Doing ...
- カタログ
...light level Conventional emitted laser Emitted light level Multiple wavelengths of light are emitted. A single wavelength of light is emitted. beams have a single wavelength. With high-frequency Modulation, the emitted laser beam is controlled ...
- カタログ
...Passing time O U T D DPC ST Passing time Difference in incident level Difference in incident level The incident light level difference is 4,000 when the level is 5,000 with a workpiece, so a threshold of 3,000 is OK. The passing time is "13 ms", ...
- カタログ
...DPC Passing time ST L O U T 41a 4999 D DPC Difference in Passing time incident level ST Difference in incident level The difference in incident level is large, so use B. 4 L O U T 13a 4000 D DPC Passing time The passing time is "13 ms", ...
- カタログ
... 2M E32-D11R 2M M6 Sensing distance (mm) Giga mode E32-LD11 2M 820 330 250 74 E32-LD11R 2M 790 310 240 71 *1. The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Sensing direction Size 1 dia. Throughbeam Reflective 1.5 dia. Top-view 3 dia. Side-view Model Sensing distance (mm) Giga mode Standard mode High-speed mode Super-high-speed mode E32-T223R 2M 520 260 150 E32-T22B 2M 750 370 220 45 65 E32-T12R 2M 1,870 910...
- カタログ
... Use 1. Do not use the product in environments subject to flammable or explosive gases. 2. Do not use the Sensor in environments where the cables may become immersed in oil or other liquids or where liquids may penetrate the Sensor. Doing ...
- カタログ
... E3S-C with a hammer, or the E3S-C will loose watertightness. • Use M4 screws to mount the E3S-C. The tightening torque of each screw must be 1.18 N·m maximum. Mounting Bracket • When mounting the E3S-C with the mounting bracket ...
- カタログ
... times clockwise or counterclockwise to set the sensing distance. The number of turns will be displayed by the indicator. Setting distance adjuster 6 E3S-CL Safety Precautions Refer to Warranty and Limitations of Liability. WARNING • Also, mount the Sensor ...
- カタログ
...I want stable detection of aluminum vapor deposition material and other glossy packaging.” The intensity of the light received by the Saturated; unable to detect (Fig. 1) Sensor sensor from highly-reflective glossy packaging Threshold is too strong, ...
- カタログ
... object, the amount of light received varies with the direction of the cylindrical object. To prevent this, locate the E3S-R as shown in the following illustration. Precautions for Safe Use The following precautions must be observed to ensure safe operation. 1. Doing ...
- カタログ
... application conditions, such as the ambient temperature and the power supply voltage. Attention must be paid during operation or cleaning. If the sensing object has a metallic or shiny surface, the E3SR may not detect it properly. To avoid this situation, place the sensing object ...
- カタログ
... the E3T. Use of E39-E10 Sensitivity Adjustment Unit (Dark-ON: E3T-ST12) (At Min.) (At Center) (At Max.) Indicator Adjuster Mounting When mounting the Sensor, never strike it with a heavy object, such as a hammer. Doing ...
- カタログ
...-CC200 2M E32-LD11 2M E32-LD11R 2M Giga mode 2,000 4,000 * 2,000 4,000 * 4,000 * 110 290 840 780 840 140 * The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Sensing distance (mm) High-speed Standard mode mode 1,000 700 3,500 2,300 1,000 700 4,000 * 2,700 3,500 2,300 50 46 130 90 350 240 350 320 350 240 60 40 Super-highspeed mode 280 920 280 1,080 920 14 39 100 100 100 16 330...
- カタログ
...You get maintenance-free operation that withstands the ambient environments. . Long-term stable detection with no maintenance Even if the incident level is decreased due to dirt or mechanical vibration, Omron’s proprietory Smart Power Control combines APC and DPC to automatically compensate the power ...
- カタログ
...° E32-T61-S 2M + E39-F2 12° E32-T51 2M + E39-F1-33 6° E32-T51 2M + E39-F16 Reflective Top-view 4° E32-D16 2M Integrated lens *1. The fiber length is 10 m on each side, so the sensing distance is given as 20,000 mm. *2. The fiber length is 2 m on each side, ...
- カタログ
...-ZV 3 L o w Pric e “Amazing price” achieved by carefully selecting the functions and performance required to detect presence or absence Fiber sensors are used in large quantities in parts feeders, roll presses for secondary batteries, assembly machines for digital products, and ...
- カタログ
... (ground) terminals, otherwise the Sensor may malfunction. Mounting Mounting the Sensor • If Sensors are mounted face-to-face, make sure that the optical axes are not in opposition to each other. Otherwise, mutual interference may result. • Always install the Sensor carefully ...
- カタログ
.... Refer to the user's manual for details. Usage Environment Water Resistance The Sensor is rated IP67. Do not use it in water, in the rain, or outdoors. Ambient Environment Do not install the product in the following locations. Doing ...