全 2903 件が検索されました。(281 - 300件を表示)

  • カタログ

    ...E2CY-C2A(F) E2CY-V3A 6 Dimpled end of 7 to 11.5 mm set screw (M3) Item A B 20 15 30 12 A *1. Be sure to turn over the braided shield so that none of its thin wires are left. *2. Make sure that an insulation distance of at least 2.5 mm is maintained. (Unit: mm) *1 5 *2 2.5 4 to 5 7 to 8 14 max. The length compensation range for cutting or extending the cable is 0.5 to 5 m. When extending the cable, use a 1.5D-2V (equivalent to...

  • カタログ

    ... connecting the power supply. 6. Dispose of this product as industrial waste. Precautions for Correct Use Do not use this product under ambient conditions that exceed the ratings.  Operating Environment 1. Do not install the product in the following locations. Doing ...

  • カタログ

    ... distance models is nearly double that of previous models. For example, the sensing distance of M12 models is 7 mm, which is the same as conventional M18 models.Using the E2E NEXT Proximity Sensor together with the e-jig allows you to easily upgrade your existing equipment ...

  • カタログ

    ... all angles, reducing the time required for operation checks after sensor replacement. Visible even in areas deep inside the equipment, allowing for quicker replacement 11 Replacements in as little as 10 seconds*1 using e-jig Using e-jig eliminates the need for adjustment ...

  • カタログ

    ...-X10D2-M1J-T 0.3M *1. Models with different frequencies are also available. The model number is E2E-X @D15 (example: E2E-X3D15-N 2M). *2. Refer to page 15 for details. *3. The residual voltage for models without polarity is 5 V, ...

  • カタログ

    ... connecting the power supply. 6. Dispose of this product as industrial waste. Precautions for Correct Use Do not use this product under ambient conditions that exceed the ratings.  Operating Environment 1. Do not install the product in the following locations. Doing ...

  • カタログ

    .... When turning on the power by influence of temperature environment, an outputmis-pulse sometimes occurs. After the sensor has passed for 300 msec after turning on, please use in the stable state. 6. The sensor is adjusted with a high degree of accuracy, ...

  • カタログ

    .... When turning on the power by influence of temperature environment, an outputmis-pulse sometimes occurs. After the sensor has passed for 300 msec after turning on, please use in the stable state. 6. The sensor is adjusted with a high degree of accuracy, ...

  • カタログ

    .... When turning on the power by influence of temperature environment, an outputmis-pulse sometimes occurs. After the sensor has passed for 300 msec after turning on, please use in the stable state. 6. The sensor is adjusted with a high degree of accuracy, ...

  • カタログ

    ...Mutual Interference When installing Sensors face-to-face or side-by-side, ensure that the minimum distances given in the following table are maintained. Face-to-face Mounting Parallel Mounting Sensing is enabled within 200 ms for the E2K-C20M@@. Design the system ...

  • カタログ

    ...nearby. For major measures, refer to Noise of Warranty and Limitations of Liability for Photoelectric Sensors. z Wiring The characteristics of the E2K-F will not change if the cable is extended. Extending the cable, however, will result in a voltage drop, ...

  • カタログ

    ... to water, oil, chemicals, or condensation by falsely detecting these as sensing objects. The E2KQ-X is of water-resistant construction. To increase the reliability of the E2KQ-X in operation, however, it is recommended that the E2KQ-X be protected with an appropriate cover ...

  • カタログ

    ... the rated voltage. Excess voltage may result in malfunction or fire. Never use the product with an AC power supply. Otherwise, explosion may result. Precautions for Safe Use The following precautions must be observed to ensure safe operation of the product. Doing ...

  • カタログ

    ... elements may explode or burn. Be sure to insert a load when connecting the power supply. 6. Dispose of this product as industrial waste. Precautions for Correct Use Operating Environment 1. Do not install the product in the following locations. Doing ...

  • カタログ

    ... supply. 6. Dispose of the product according to applicable regulations (laws). Precautions for Correct Use Do not use this product under ambient conditions that exceed the ratings. Operating Environment 1. Do not install the product in the following locations. Doing ...

  • カタログ

    ..., Oil-resistant Opposite side: 7, Thickness: 2.4 (Nickel-plated brass) Washers (Nickel-plated iron) Lens (PMMA) Aperture angle Small Spot High Power Narrow view BGS * The optical fiber is 2 m long on each side, ...

  • カタログ

    ... fiber, preventing stable detection. OMRON’s original tool-friendly construction allows the wrench to fit all the way onto the nut without coming into contact with the cable. The Fiber Unit is not accidentally damaged. Easy Cable Routing The cable opening is wide, ...

  • カタログ

    ...Search for the page in the model index. 102 Page Search for the model on the corresponding pages. Each Page Fiber Unit Index Cylindrical Models Easily mount tightening just one nut. The cable follows the wall, ...

  • カタログ

    ...misalignment Optical axis can be easily adjusted in three directions: vertical, horizontal, and angular. This bracket can be mounted to any photoelectric sensor with a 25.4 mm mounting hole pitch as well as the E3AS Sensors. The E3AS Series is classified as Class 1, ...

  • カタログ

    ... maintenance frequency P.10 3 Design Complex-shaped, colored, patterned, or glossy surfaces can be detected Stable detection for variable workpieces eliminates the need for redesign Conventional sensors have to be selected each time the shape, color, pattern, or reflectivity of the workpiece changes, ...