全 2903 件が検索されました。(261 - 280件を表示)
- カタログ
...changes to specifications. Tag name Data The addresses in PLC assigned to tag names can be changed without creating additional work. CJ2 (with EtherNet/IP functionality) or NJ/NX/NY * Name server FROM PLC data was accessed using addresses, ...
- カタログ
... User's Manual Safety Control Unit/Communication Control Unit (Cat. No. Z395). . Type OMRON Single-beam Safety Sensors OMRON Non-contact Safety Door Switches Model and corresponding PL and safety category E3ZS D40A-2, D40A Safety Output Units NX-...
- カタログ
... used alone for safety functions. Safety controllers available to match the scale of your application. Connects to safety controllers for applications ranging from simple safety interlocks to large equipment requiring multi-axis control. G9SX-NS/NSA G9SP NX-SL3/SI/...
- カタログ
...!WARNING Serious injury may possibly occur due to breakdown of safety outputs. Do not connect loads beyond the rated value to the safety outputs. Serious injury may possibly occur due to loss of required safety functions. Wire the D40A and G9SX-NS properly ...
- カタログ
... Safety Symbols General prohibition Instructions on unspecified prohibited action. General instructions Instructions on unspecified general action. WARNING Use only appropriate components or devices complying with relevant safety standards corresponding to the required performance level and safety category. Failure to do ...
- カタログ
...24V X1 X2 IN Y1 Y2 OUT 5 6 4 3 7 GND 1 8 2 The cable entry is realized by a metric M20 gland. This gland must be measured by the user so that it is suitable for the cable used. A cable gland with strain relief and suitable IP protection class must be used. Length X of the cable at terminals: 8.0 mm (for screw terminals of -T1) 40 10 X X D41G Wiring Example The application examples shown are suggestions. However, these do not exempt the user from carefully checking whether the safety door switch...
- カタログ
.... Be sure to apply the proper torque to tighten each screw. Mounting Dimensions (M5) Standard Model Precautions for Safe Use • Do not use the Switch submerged in oil or water, or in locations continuously subject to splashes of oil or water. Doing ...
- カタログ
... N·m 5. Two, M5 Operation Key mounting screw 3. Four, M3.5 head-mounting screw Precautions for Safe Use • Do not use the Switch submersed in oil or water or in locations continuously subject to splashes of oil or water. Doing ...
- カタログ
...Be sure to read the precautions for All Safety Door Switches in the website at:http://www.ia.omron.com/. Precautions for Safe Use • Do not use the Switch submersed in oil or water or in locations continuously subject to splashes of oil or water. Doing ...
- カタログ
...or avoid doing, to prevent failure to operate, or undesirable effect on product performance. Precautions for Safe Use • Do not use more than one D4F side-by-side. • Do not switch circuits for two or more standard loads (125 VAC, 1 A). Doing ...
- カタログ
...Black 21.5 to 24 Operation key insertion position Operation key insertion radius (R ≥ 50) * Red Adjusting screw Black (29.8±1) Note 1: When determining the operation key insertion radius, adjust the adjusting screw ...
- カタログ
... S4 Guard can be opened M A2 S14 S24 KM1 KM2 L1 L2 X2 Reset switch S3 PLC etc. KM1 and KM2 (NO) X1 Motor M rotation Note: The lock release enable signal must be configured so that it should turn ON after dangerous movement is stopped and safety is ensured for the door to open. 22 D4JL/D4JL-SK40 Safety Precautions Be sure to read the precautions for All Safety Door Switches in the website at:http://www.ia.omron.com/. Indication and Meaning for Safe Use DANGER Indicates an imminently hazardous situation which, if not avoided, is ...
- カタログ
... humidity 95% max. Weight Approx. 92 g (D4N-1A20R) Note: 1. The above values are initial values. 2. Once a contact has been used to switch a standard load, it cannot be used for a load of a smaller capacity. Doing ...
- カタログ
...Approx. 82 g (D4N-1120) Approx. 99 g (D4N-6120) Note: 1. The above values are initial values. 2. Once a contact has been used to switch a standard load, it cannot be used for a load of a smaller capacity. Doing ...
- カタログ
...opening mechanism. The terminals 11-12, 21-22 and 33-34 can be used as unlike poles. Note: 1. Terminals are numbered according to EN50013. Contact forms are according to EN60947-5-1. 2. MBB (Make Before Break) contacts have an overlapping structure, ...
- カタログ
... door can be opened and closed easily when replacing workpieces or parts. Spring Lock plate The door is locked only when the solenoid is turned ON. This means that the door will be unlocked if there is a power interruption and ...
- カタログ
... a certified direct opening mechanism. Stroke Operation Key insertion completion position Extraction completion position The terminals 11-12, 21-22 and 33-34 can be used as unlike poles. * MBB (Make Before Break) contacts have an overlapping structure, ...
- カタログ
...selected from the RUN/SET selector. (6) PWR/ALM Indicator Power ON: Green light Sensor error: Red light 4 D7F Safety Precautions Precautions for Safe Use Do not perform wiring work or touch any terminals with power supplied. Doing ...
- カタログ
...A B C D Note: 1. Mutual Interference Prevention: When mounting Sensors with the same diameter and cable length in parallel, set the DIP switch to modes that differ by 1 m in cable length. Specifications, however, may not be sufficiently met, ...
- カタログ
... at close range, make sure that the sensing objects move through the sensing range slowly (guideline: 20 ms or longer). 6 Make sure that the Sensor is in operating condition before making sensitivity adjustments. *1. Be sure to turn over the braided shield ...