全 2903 件が検索されました。(1861 - 1880件を表示)
- カタログ
...: 1.76 mm F39-TC5P01 9 6 F39-TC5 Safety Precautions !WARNING The muting and override functions disable equipment safety functions. Use separate procedures to ensure safety when the muting and override functions are operating. Position the Muting Sensors ...
- カタログ
...Top/bottom adjustable bracket (for user-made mounting part) (sold separately) Standard adjustable bracket (sold separately) This bracket provides vertical as well as horizontal adjustment of ±15º. ±15° The wall mounting bracket k ket is not provided ...
- カタログ
...Safety Precautions !WARNING Do not operate the product in atmospheres containing flammable or explosive gas. Arcs or heating of relays during switching may cause fire or explosion. Do not use a load that exceeds the contact ratings or switching capacity. Doing ...
- カタログ
...ON Safety output 1 OFF ON Safety output 2 OFF External Test Function OFF signal 40µs max. This function stops emission by test input. It creates a state in which the F3SR-B is blocked using external signals ...
- カタログ
...-E cause any problem conflicting with local laws or related to product liability locally, however, OMRON shall, without exception, assume no responsibility for it. CAUTION Before using more than one F3W-E Sensor in parallel or series, take necessary countermeasures against mutual interference ...
- カタログ
...-brightness Models FL Series ●Maintaining light intensity even with long wiring distances Twice* Camera Brighter Light L Light 10-m long, distances result in voltage drops and lower light intensity. Power is supplied through the Camera, ...
- カタログ
...-brightness Models FL Series Maintaining light intensity even with long wiring distances Twice* Camera Brighter Light L Light 10-m long, distances result in voltage drops and lower light intensity. Power is supplied through the Camera, ...
- カタログ
...-brightness Models FL Series Maintaining light intensity even with long wiring distances Twice* Camera Brighter Light L Light 10-m long, distances result in voltage drops and lower light intensity. Power is supplied through the Camera, ...
- カタログ
... Ethernet. The The FQ-M is able to output position communication wizard lets you easily coordinates and the correlative encoder configure any robot protocol both as a values and is able to manage the object server or as a client without complex queue, ...
- カタログ
... of important judgment values for inspections to easily manage and then adjust them later. Also, if you isolate in advance the settings that are critical to inspection performance (and normally known only to the designer) as user data, the locations that require adjustment can be clarified ...
- カタログ
... a personal computer or PLC. Connect a track ball, mouse and USB memory. A total of four USB ports are provided and any of them can be used. However, when connecting two or more USB memories, do not connect them to adjacent ports. Doing ...
- カタログ
....However, it is possible to extend the length (max. 15m) by jointing cables (max. 3 pieces), when using Camera Cable Extension Unit (FZ-VSJ). *2 This strobe controller is recognized as type FZ-SLC100 in FZ3-(H)3** / (H)7** series (previous ver2.12). And ...
- カタログ
... are recognized as an edge code and geometric calculations determine the center of the circle and circumference edge. Even if the circle is broken, it is recognized as a circle, i.e., as the measurement object. Dirt and other abnormalities in the measurement region are differentiated ...
- カタログ
.../DC48V DC G2RV-SR700/500-AP AC100V 48 G2RV-1-S-AP-G DC48 G2RV-SR700/500-AP AC110V G2RV-SR700/500-AP AC200V G2RV-SR700/500-AP AC230V Note: Voltage is reduced within the socket for the slim I/O relay, so...
- カタログ
... × 55 mm (W × H × D, when mounted upright). • Independent contacts and short bar allow easy common connections. • The common can now be connected with a short bar in the G70D-SOC08 and G70R-SOC08. • No tools are required to remove Relays, ...
- カタログ
... proximity sensors according to the following description: • To avoid interference from surrounding metal and mutual interference, specified proximity sensors should be correctly installed. • For handling of proximity sensors, see the instruction manual for the E2E. • Connect two proximity sensors of the same type. • Install proximity sensors ...
- カタログ
... allows the operator to immediately turn OFF the power, and label it to clearly indicate its function. • Be sure to wire the terminals correctly. • Do not install input lines in the same duct or conduit as power supply or other high-voltage lines. Doing ...
- カタログ
...: The Y92S-35 is not provided with H3AM. Order separately ,if water protection is required. Use Waterproof Packing to provide a level of water protection that complies with IP65 standards. Depending on the operating environment, the Waterproof Packing may deteriorate, contract, or harden and ...
- カタログ
... output Control output (See note 2) (See note 2) Time up indication Time up indication Reset input indication Reset input indication Note: 1. For models with memory backup (H5AN-@M), you cannot perform a power-OFF reset, ...
- カタログ
... electric shock under specific conditions. Used for general prohibitions for which there is no specific symbol. Used for general mandatory action precautions for which there is no specified symbol. CAUTION Do not touch the terminals while power is being supplied. Doing ...