全 2903 件が検索されました。(1921 - 1940件を表示)
- カタログ
... open — Programmable g Multi Axis Controller "PMAC" Omron keeps believing in human potential In order to satisfy diverse consumer needs and deal with short product life cycles, manufacturers need to boost both their productivity and their manufacturing quality. Omron is doing ...
- カタログ
...Rail stopper To improve and maintain the reliability of the power supply over a long period of time, adequate consideration must be given to heat radiation. The power supply is designed to radiate heat by means of natural airflow. Therefore, mount the power supply ...
- カタログ
... dissipation and may occasionally result in deterioration or damage of internal parts. Do not use any mounting method other than the standard one. 2. Take adequate measures to ensure proper heat dissipation to increase the long-term reliability of the S8M. 3. Install the S8M ...
- カタログ
... terminals. Specified by performance of S8TS-06024@ Basic Block. Specified by S8TS-06024@ connection. The output voltage will be 21.0 V (min.) when switching to backup operation. The life of the battery will greatly reduced when operating below the minimum output. Design the loadcircuit ...
- カタログ
...100 Output current (%) The values shown in the above diagram are for reference only. Note: Internal parts may occasionally deteriorate or damaged if a short-circuited or overcurrent continues for 20 min. or longer. Overvoltage Protection An overvoltage protection function is provided ...
- カタログ
... heat dissipation and may occasionally result in deterioration or damage of internal parts. Use the Power Supply within the derating curve for the mounting direction that is used. 2. Use the metal plate as the mounting panel (*1). 3. Install the Power Supply ...
- カタログ
...[-] Safety Precautions for Sensing Bands and Liquid Leakage Point Sensors Safety Precautions for Sensing Bands and Liquid Leakage Point Sensors CSM_SensingBand_CN_E_1_2 !WARNING Do not touch the terminals while power is being supplied. Doing ...
- カタログ
...-VSP2 5M 5m FJ-VSP2 10M 10 m Note. When wiring a camera, be sure to refer to its specification document to check its external connector specifications. Incorrect wiring can lead to failure. Note. Do not connect the shell, for doing ...
- カタログ
... Safety Mats are being combined. In addition to joining the Safety Mats, the Joining Trims preserve the Safety Mat's sensitivity at the joints. Aluminum Ramp Trim: UMAL Secures the edges of the Safety Mat to the floor. The Aluminum Ramp Trim is hollow, ...
- カタログ
... to joining the Safety Mats, the Joining Trims preserve the Safety Mat's sensitivity at the joints. UMOC UMMA-1000-1000-2 UMIC Aluminum Ramp Trim: UMAL Secures the edges of the Safety Mat to the floor. The Aluminum Ramp Trim is hollow, ...
- カタログ
...[Q158-E1] V400-R Catalog It's so small ! Side view type Paper/Label Front view type Both 2D & 1D code compatible Ultra-small multi code reader V400-R series reading that automatically recognizes • Multi-code major paper/label 1D and 2D codes Example of supported code types • 1.3 Mega pixels (SXGA) CMOS image sensor feature (Green LED) to quickly condition • Aiming the reading area for recognition view/Side view types available for flexible • Front installation Data matrix (Automobile parts) QR code (HDD) Code 39 (Printed circuit board) System configuration Specifications Connection cable for IBM PC/AT or ...
- カタログ
...システム形V750シリーズ EPC EP Cglo Cgl Cg loba bal Cl bal C ass1 s1 Gen e er e at atiio ion2 2 (ISO (I SO/I SO /IEC C1 180 8000 80 00-6 6T Typ ype yp e C) 規格対応規格対応 長距離交信で広がるアプリケーション製造現場情報を一括管理 本製品本製品は本本製品は、 本製製品...
- カタログ
...No interference of wiring helps improve workability and safety Improved wiring workability by unified I/O terminal positions on the top and bottom Inputs Outputs BEFORE Hard wiring due to mixed I/O terminals located on the top and bottom Unified method ...
- カタログ
...Precautions for Correct Use Wiring Precautions • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...
- カタログ
...V: Vertical screw mounting Blank: Horizontal screw mounting Horizontal Screw Mounting Select the Best Type for Actual Case of Use Vertical screw mounting Horizontal screw mounting All Models Mount to DIN Track The ribs for screw mounting are positioned within the DIN Track ...
- カタログ
...Precautions for Correct Use Wiring • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...
- カタログ
...Precautions for Correct Use Wiring • Do not perform wiring work, remove connectors, or connect connectors while power is being supplied. Electric shock or damage to the device may result. • Double-check all wiring before turning ON the power supply. • After wiring, route the cable ...
- カタログ
... and it is impossible for the Sensor to process the light reflected to the Sensor. The indicator is lit when the amount of light is less than what is required for computation by the Sensor. When the ALM indicator is lit, make necessary adjustments ...
- カタログ
... Error vs. Object Material When detecting a variety of objects successively, refer to the offset error graph below. The graph illustrates the change in sensor output characteristics when black paper is compared to white paper. To reduce the offset error value, install the Sensor ...
- カタログ
... the product. Minor burns may occasionally occur. Do not touch the product while power is being supplied or immediately after power is turned OFF. Minor fires may occasionally occur. Tighten terminal screws to a torque of 0.5 to 0.6 N·m ...