全 2903 件が検索されました。(1881 - 1900件を表示)

  • カタログ

    ... 4 digits), the largest class in the industry. The wide viewing angle and brightness provide excellent visibility. The number of display segments has also been increased to make settings easier to understand, and the present value display can be switched between red, green and orange ...

  • カタログ

    ... separately) P3G-08 (order Waterproof Packing Flush Mounting Adapter separately) Back-connecting Socket Note: 1. The mounting panel thickness should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted ...

  • カタログ

    ...Preset Preset Display Display 1st 1st 0 0 Count out 1st 1st Control outputs 2nd Count out Control outputs Count out Count out 2nd Note: Two-stage counters, set the counters so that the interval between 1st and 2nd count out will be more than 5 ms. For Incrementing/ Decrementing switchable counters, only the 2nd value will be effective if the 1st value is larger than the 2nd value. The Incrementing/Decrementing Counters give outputs in the following order; 1st to 2nd to 1st to 2nd. Totalizing Counters Incrementing/Decrementing selectable mode Incrementing mode Reversible mode Incrementing/Decrementing A, B, ...

  • カタログ

    ... of electric shock under specific conditions. Used for general prohibitions for which there is no specific symbol. Used for general mandatory action precautions for which there is no specified symbol. !CAUTION Do not touch the terminals while power is being supplied. Doing ...

  • カタログ

    ... digits, the largest class in the industry. The wide viewing angle and brightness provide excellent visibility. The number of display segments has also been increased to make settings easier to understand, and the present value display can be switched between red, green, and orange ...

  • カタログ

    ...Flush Mounting Adapter separately) Back-connecting Socket 58 (51) 48 7.5 Note: 1. The mounting panel thickness should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted ...

  • カタログ

    ... allows the operator to immediately turn OFF the power, and label it to clearly indicate its function. • Be sure to wire the terminals correctly. • Do not install input lines in the same duct or conduit as power supply or other high-voltage lines. Doing ...

  • カタログ

    ... Safety Precautions for All Counters. !CAUTION Tighten the terminal screws to the specified torque (approx. 0.5 N⋅m). Fire or malfunction may result if the screws become loose. Do not use the product in locations subject to flammable or explosive gases. Doing ...

  • カタログ

    .... • Make sure there is no foreign matter in the Connector before connecting it to the Encoder. 17 H8PS Safety Precautions for Cam Positioners Refer to Safety Precautions for All Counters. !CAUTION Tighten terminal screws to a torque of 0.80 N·m ...

  • カタログ

    .... No. W500). Precautions for Correct Use Read the following precautions carefully before using an SD Memory Card. For details, refer to user's manuals for the device on which the card is mounted. Formatting The SD Memory Cards are formatted and shipped, ...

  • カタログ

    .... No. W500). Precautions for Correct Use Read the following precautions carefully before using an SD Memory Card. For details, refer to user's manuals for the device on which the card is mounted. Formatting The SD Memory Cards are formatted and shipped, ...

  • カタログ

    ... and build to eliminate faults caused by complexity and, with other unique design features, to maximize uptime and reduce costs. The future will be IT driven: Omron’s IPC platform will make you part of it. Simplicity improves reliability Unnecessary complexity causes problems, ...

  • カタログ

    ...80 30 3 23.5 51.5 78 72±0.3 Note: DIN track mounting is also possible. 7 K3SC Safety Precautions !CAUTION Do not touch any of the terminals while power is being supplied. Doing so may result in electric shock. Do not allow metal objects or wire cuttings to enter the product. Doing ...

  • カタログ

    ... use the Digital Panel Meter in locations where corrosive gas (particularly sulfide or ammonia gas) is generated. Water-resistive Soft Front Cover Before mounting the Digital Panel Meter to a panel, attach the waterresistive soft front cover and mounting bracket to the Digital Panel Meter properly ...

  • カタログ

    ...Calibration The front panel cover is removed when setting the decimal point position or performing calibration. Do not, however, touch any parts other than the slide switches or adjustment knob or come close to any metal parts. Calibrate the Digital Panel Meter regularly ...

  • カタログ

    ... Correct Use Accessories (Order Separately) Refer to Safety Precautions for All Digital Panel Meters. Water-resistive Soft Front Cover Mounting Before mounting the Digital Panel Meter to a panel, attach the waterresistive soft front cover and mounting bracket to the Digital Panel Meter properly ...

  • カタログ

    ... g Approx. 480 g Approx. 700 g Approx. 6.6 kg Approx. 1.3 kg Approx. 2.5 kg Approx. 3.5 kg Note: Do not connect ZCT output terminals k and l to ground. Doing so may result in damage to the Relay. 3 K6EL Internal Block Diagram X/c 9 Delayed models only 8 Operating time selection switch 11 X/a Operating time setting circuit 6 Reset button 3 From OTG ZCT * Input protection circuit 4 Operating value setting circuit Sensitivity selection switch (not provided on the K6EL-30) Amplifier circuit 7 Switching circuit X Ground fault...

  • カタログ

    ...出力1 ON OFF TM1設定時間 警報出力2 Io値 Ior値 警報出力時 ON OFF TM2設定時間 本製品は株式会社So Brainの特許ライセンスを受けています。 種類/標準価格(◎印の機種は標準在庫機種です。 無印(受注生産機種)の納期についてはお取引き商社にお問...

  • カタログ

    ...る値を“0”にシフトし、その後の絶縁劣化の傾向をロギングにより管理・確認することができます。 本製品は株式会社So Brainの特許ライセンスを受けています。 お問い合わせ 0120-919-066 最新情報は www.fa.omron.co.jp 1 K6ER 高調波やノイズに左右されな...

  • カタログ

    ...-10 to 55 °C Ambient humidity 25 to 85 % Weight Approx. 32 g 11 K7L-UP-FLK Precautions Caution Tighten the terminal screws to the recommended torque of 0.5 to 0.6 N•m. Failure to do so may occasionally cause physical damage due to fire. Do not use the product in an environment with flammable or explosive gas. Doing ...