全 2903 件が検索されました。(1821 - 1840件を表示)
- カタログ
... Power Coupler between the B7A Input Unit and B7A Output Unit, it is possible to transmit multiple switch signals without contact from input devices to controllers. When using the B7AP Power Coupler in this way, it is possible to transmit power via electromagnetic coupling, ...
- カタログ
...-digit accumulated signals. Accumulated Value Input/Contact Output Converts 4-digit accumulated value signals to low-speed contact pulses before they are output. Others Analog/Pulse Width Converter (See note 1.) Changes the ON/OFF duration ratio in a constant cycle duration ...
- カタログ
...Supported (called global subroutines). 0.5 ms min. 0.7 ms min. I/O Area 2,560: CIO 000000 to CIO 015915 (160 words from CIO 0000 to CIO 0159) The setting of the first word can be changed from the default (CIO 0000) ...
- カタログ
... 3.0 or later only) Languages in function block definitions: ladder programming, structured text I/O Area 1,280: CIO 000000 to CIO 007915 (80 words from CIO 0000 to CIO 0079) The setting of the first word can be changed from the default (CIO 0000) ...
- カタログ
... 3.0 or later only) Languages in function block definitions: ladder programming, structured text I/O Area 1,280: CIO 000000 to CIO 007915 (80 words from CIO 0000 to CIO 0079) The setting of the first word can be changed from the default (CIO 0000) ...
- カタログ
... on a host computer or with Support Software, such as the CX-Programmer. • Use the clock on an SNTP server to automatically adjust the clocks in the PLCs connected to the Ethernet network. (An SNTP server is required separately.) • An FTP server is built in, ...
- カタログ
... (total 32) Number of allocated words Input: 1 word, Output: 1 word Weight 185 g max. CQM1H Word Allocation In the CQM1H PLCs, an I/O Link Unit is treated just like an I/O Unit with one input word and one output word, ...
- カタログ
... in a status area in the Slave Unit will turn ON to notify the Master Unit. The notification details can be read using the CX-Integrator or using explicit messages. Note 1. The minimum communications power voltage for the CompoNet network itself is 14 V, ...
- カタログ
...Units mountable to PLC 63 *2 Fixed allocations 3 User-set allocations 16 172 g max. *1. Refer to the DeviceNet Operation Manual (W267) for the communications power supply specifications. *2. The Device Unit uses a node, and ...
- カタログ
... on a host computer or with Support Software, such as the CX-Programmer. • Use the clock on an SNTP server to automatically adjust the clocks in the PLCs connected to the Ethernet network. (An SNTP server is required separately.) • An FTP server is built in, ...
- カタログ
... CPU Unit’s cycle time. The actual sampling interval will always be longer than the CPU Unit’s cycle time even if the sampling interval is set shorter than the cycle time. *2. The Data Collection Patterns use the data collected by the Basic Collection Pattern, ...
- カタログ
...configuration for only the necessary data from PLC memory. The data to be collected can be stored in files in the required data type, such as BOOL, REAL, INT, BCD, or STRING. Data configuration files required for the host computer can be created, ...
- カタログ
...For the most recent information on models that have been certified for safety standards, refer to your OMRON website. • The D4GL Vertical Electromagnetic Lock and Safety-door Switches easily mount to a 40 × 40-mm aluminum frame section. • The Switches are made of resin ...
- カタログ
... notice. Cat. No. F091-E1-02 0914(0813) Visualization of Air Flow, Pressure, Leakage quantity enable more Energy Savings in production site. Air compressors consume a much electrical energy in production sites. Production sites, however, prioritize improving productivity, and ...
- カタログ
...5.9 N⋅m 15 N⋅m 39 N⋅m Part B Torque 9.8 N⋅m 45 N⋅m 78 N⋅m * If the thickness of the mounting bracket (t) exceeds 5 mm, be sure to install the Sensor so that ℓ ≥ 2, d (dia.) ≥ 45, and D ≥ 2. Mutual Interference When installing Sensors face-to-face or side-by-side, be sure that the minimum distances given in table 2 are maintained. B A Chart 2. Mutual Interference Item Model E2V-X2 30 20 E2V-X5 50 30 (Unit: mm) E2V-X10 100 50 Model E2V-X4 35 25...
- カタログ
...IP40 (IEC 60529) *1. Sensing distance values are for white paper. *2. These sensing distance values apply when a E39-R12 Reflector is used. The MSR function is built-in. The reflected light from the object being measured may affect the sensing accuracy, ...
- カタログ
.... Light level 4-2. Teaching a Reflective Fiber Unit without a Workpiece A value about 6% greater than the incident light level (minimum difference) can be set as the threshold. This method is ideal when using a Reflective Fiber Unit to detect workpieces ...
- カタログ
...Sensor a distance away from the mirror-like object as shown below. 50 N max. 10 N max. ● Adjusting Indicators Sensing object Mirror-like object Incident level • The following illustration indicates the operating levels of the E3G. • Set the E3G ...
- カタログ
...approximately in the middle between the background and sensing object. Thresholds (a and b) are set in the sensing distance on condition that the difference between these thresholds are approximately 10% of the whole sensing distance. The threshold is set ...
- カタログ
... the Industry Patent Pending In Amplifiers with wire-saving connectors, the power supply is distributed to 1-conductor slave connectors through a 3conductor master connector. This design has three major advantages. 1. Wiring time is significantly reduced. 2. Relay connectors are unnecessary, ...