全 2903 件が検索されました。(1841 - 1860件を表示)
- カタログ
...Easy operation makes for assured line quality Only one click of the Mode key! There are no complicated settings to perform—Incident level is adjusted automatically to suit any application. In addition, the meaning of the display will not change as the sensor is operated, ...
- カタログ
...1,000 600 400 180 E32-LD11 2M 860 610 360 250 110 E32-LD11R 2M 840 600 350 240 100 E32-CC200 2M * The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Sensing direction Size 1 dia. Top-view 1.5 dia. Throughbeam Sensing distance (mm) Model Tough mode High-resolution mode Standard mode High-speed mode Super-highspeed mode E32-T223R 2M 450 300 250 150 60 E32-T22B 2M 680 480 400 220 90 E32-T12R 2M 2,000 1,400 1,000...
- カタログ
...Top-view 4° E32-D16 2M 40 to 1,000 40 to 700 40 to 450 40 to 240 40 to 600 40 to 490 40 to 300 40 to 240 Integrated lens *1. The fiber length is 10 m on each side, so the sensing distance is given as 20,000 mm. *2. The fiber length is 2 m on each side, ...
- カタログ
... the sub-display. If that occurs, repeat the operation from the beginning. 4-1. Setting the Threshold at Maximum Sensitivity The threshold can be set to the maximum sensitivity. This method is ideal when using a Through-beam Fiber Unit to detect workpieces ...
- カタログ
... and a multi-RGB processing system combine to cover all RGB wavelengths, enabling easy and accurate detection of workpieces without having to use a different light source to match each one. No Need to Select Changes in the three parameters are processed as a ratio, ...
- カタログ
...[E388-E1-02] E3X-SD Data Sheet Simple Fiber Amplifier E3X-SD The Standard for Fiber Amplifiers with Simple Operation and High Performance ■ Operation so simple that essentially anyone can use the amplifier right way. ■ Immediately determine operation and amount of light with a simple, bright display. ■ General-purpose capabilities to simply handle a broad range of applications. Ordering Information Amplifier Units Amplifier Unit Connectors (Order Separately) Digital Display and Direct Key Setting Item Appearance Standard models Note: Stickers for Connectors are included as accessories. Model Connection Ratings and method Specifications Pre-wired NPN output Item PNP output Appearance...
- カタログ
... Each of the following illustrations indicates the operating zone with the E4A-3K mounted to the ceiling for the purpose of detecting the human body. In either case, make sure that the lower limit of the sensing range is approximately 0.5 m above the floor ...
- カタログ
... the midpoint of the range within which the STABILITY indicator is lit. Range in which the STABILITY indicator (green) is lit Optimum line Range in which the SENSING indicator (red) is lit Pass the sensing object through the sensing range and adjust the sensitivity ...
- カタログ
...Safety Precautions for E5@N/E5@N-H/E5@N-HT CSM_E5_N_E5_N-H_CN_E_3_5 Safety Precautions Refer to Safety Precautions for All Temperature Controllers. !CAUTION Do not touch the terminals while power is being supplied. Doing ...
- カタログ
...(Accessory) Terminal Cover (E53-COV16) (Accessory) Crimp terminal size: M3.5 • Recommended panel thickness is 1 to 8 mm. • Group mounting is not possible in the vertical direction. (Maintain the specified mounting space between Controllers.) • To mount the Controller ...
- カタログ
...) Panel Cutout Group Mounted Mounted Separately 45 +0.6 0 • Recommended panel thickness is 1 to 5 mm. • Group mounting is not possible in the vertical direction. (Maintain the specified mounting space between Controllers.) • To mount the Controller ...
- カタログ
...) Weight Approx. 100 g Mounting bracket: Approx. 10 g 5 E5ZN Installation ■ Connection Diagrams • Voltage output (control output) is not electrically isolated from internal circuitry. Therefore, when using grounded thermocouples, do not ground control output terminals. (Doing ...
- カタログ
...CSM_E5ZN_operation_TG_E_2_2 Nomenclature E5ZN (Orders for the E5ZN series will not be accepted after March 31, 2019.) • The E5ZN is a Temperature Controller that features the ability to be built into equipment. • The E5ZN is equipped with RS-485 communications, ...
- カタログ
... atmospheres or environments that exceed product ratings. ● Installation Do not use the Sensor in an environment subject to corrosive or combustible gas. ● Wiring If no linear output is used, cut the gray lead wire short and apply insulating tape to the lead wire ...
- カタログ
... power supply before connecting or disconnecting wires. Do not attempt to disassemble, repair, or modify the product in any way. When disposing of the product, treat it as industrial waste. Do not use the Sensor in water, rain, or outdoors. Process the unwired terminals ...
- カタログ
...Safety Precautions Refer to Warranty and Limitations of Liability. WARNING This product is not designed or rated for ensuring safety of persons either directly or indirectly. Do not use it for such purposes. Axis Adjustment (1)Tentatively mount the emitter and receiver ...
- カタログ
...3 3 Slit C 3 0.5 Slit D 3 1 Note: These are pressure sensitive adhesive-type stickers. Peel off the seal and stick it on the lens. Optical Axis Adjustment (1)Set the Sensor so that the center of the lens in the emitter and receiver form one line. (2)Having checked that the Sensor is correctly wired, turn ON the power. The operation indicator on the amplifier of the emitter will light. Check to make sure the light goes ON and OFF when an opaque object is moved in and out between the emitter and receiver. (3)...
- カタログ
...6 Easy Integration with IT Systems Reduces wasted time and movement by continuously looking ahead to anticipate which robots will be best positioned for upcoming tasks. Performs updates automatically across the entire fleet. Enterprise Manager can connect to your MES, ERP and WMS ...
- カタログ
...(Refer to Dimensions on page 1.) Sensing Band Sticker Note: 1. When using the F03-26PES (adhesive-tape model), be sure to wipe all moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do ...
- カタログ
...(Refer to Dimensions on page 2.) Sensing Band Sticker Note: 1. When using the F03-26PES (adhesive-tape model), be sure to wipe all moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do ...