全 2903 件が検索されました。(1961 - 1980件を表示)
- マニュアル
... in death or serious injury Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Warnings and Cautions WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Caution Operating Environment Precautions ! Warnings and Cautions ! WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Caution Operating Environment Precautions ! Warnings and Cautions ! WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... or death. Additionally there may be significant property damage. Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury or in property damage. WARNING Never attempt to disassemble any Units while power is being supplied. Doing ...
- マニュアル
..., or other foreign material to enter any Unit. 8 B Otherwise,Unit burning, failure, or malfunction may occur. Cover the Units or take other suitable countermeasures, especially during wiring work. • Do not allow foreign matter to enter the openings in the Unit. Doing ...
- マニュアル
... or serious injury. Caution Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Warnings and Cautions WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... allow wire clippings, shavings, or other foreign material to enter any Unit. Otherwise,Unit burning, failure, or malfunction may occur. Cover the Units or take other suitable countermeasures, especially during wiring work. • Do not allow foreign matter to enter the openings in the Unit. Doing ...
- マニュアル
...Indicates an imminently hazardous situation which, if not CXQKFGFYKNNTGUWNVKPFGCVJQTUGTKQWUKPLWT[ Indicates a potentially hazardous situation which, if not CXQKFGFEQWNFTGUWNVKPFGCVJQTUGTKQWUKPLWT[ Indicates a potentially hazardous situation which, if not CXQKFGFOC[TGUWNVKPOKPQTQTOQFGTCVGKPLWT[QTRTQRGTV[ damage. Warnings and Cautions WARNING &QPQVCVVGORVVQVCMGCP[7PKVCRCTVYJKNGVJGRQYGTKUDGKPI supplied. Doing ...
- マニュアル
... or serious injury. Caution Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Warnings and Cautions WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... the requirements of the following EC Directives: Machinery Directive 2006/42/EC SAFETY PRECAUTION ●Definition of Precautionary Information Before changing the head direction always ensure that the release key is set to "UNLOCK", or that the Operation Key is inserted. Not doing ...
- マニュアル
... die Abdeckung öffnen. Es besteht die Gefahr eines elektrischen Schlages." 8. Lassen Sie das Produkt auf keinen Fall fallen, sonst kann es zu Funktionsstörungen des Schalters kommen. 9. Es besteht Verletzungsgefahr! Das Produkt beim Anbringen nicht fallen lassen! 10. Installieren Sie den Betätiger ...
- マニュアル
... noise from them may cause malfunction or breakdown of the product. ・Do not insert or remove a connector, etc. with power supply applied. 3. Others ・Do not use the product as scaffolding. ・Take caution not to mount the status indicator downward. Doing ...
- マニュアル
.... 11) Optical communications are not possible with an E3X-DA-N Amplifier Unit. 12) Depending on the application environment, time may be required for the detection level to stabilize after the power supply is turned ON. 13) Output pulses may occur when the power is interrupted and ...
- マニュアル
...9) Optical communications are not possible with an E3X-DA-N Amplifier Unit. 10) Depending on the application environment, time may be required for the detection level to stabilize after the power supply is turned ON. 11) Output pulses may occur when the power is interrupted and ...
- マニュアル
...Iron with galvanizing ■EFFECTS OF SURROUNDING METAL ■EXTERNAL DIMENSIONS When mounting the proximity switch in a metal panel, maintain the clearances given in table 2. When installing it with the nut, the value is different depending on the kind of the nut used, ...
- マニュアル
...CAUTION E2FM-X1R5□ B C D Toothed washer When mounting the proximity sensor in a metal panel, maintain the clearances given in table3. When installing it with the nut, the value is different depending on the kind of the nut used, ...
- マニュアル
...) ・T形溝以外のシリンダに取り付ける場合は、 別売の取付金具をご使用ください。 ・Please use an attached cable clip. ・The protrusion wears away when installing.So this product is fixed temporarily. ・Please fix this product with an attached screw. (Tightening Torque:max.0.4N・m) ・When this product is installed in other than T-groove cylinder, please use the mounting brackets(order separately). 0V 当社適合コネクタコード: XS2Fシリ...
- マニュアル
...) ・T形溝以外のシリンダに取り付ける場合は、 別売の取付金具をご使用ください。 ・Please use an attached cable clip. ・The protrusion wears away when installing.So this product is fixed temporarily. ・Please fix this product with an attached screw. (Tightening Torque:max.0.4N・m) ・When this product is installed in other than T-groove cylinder, please use the mounting brackets(order separately). 0V Precautions For Safe Use 以下に示すような項目...
- マニュアル
... it after confirming the installation distance by following (a) and (b) with an actual sensing object when you install the sensor. (a)The detection distance receives the influence by the material of the sensing object, thickness, shape, and the size. ...
- マニュアル
... communications are not possible with an E3X-DA-N Amplifier Unit. 12) Depending on the application environment, time may be required for the incident light level to stabi-lize after the power supply is turned ON. 13) Output pulses may occur when the power is interrupted and ...