全 202 件が検索されました。(81 - 100件を表示)
- マニュアル
... treated as X-Y plane. This function makes it possible to transplant programs used with the CV500-MC421 or CV500-MC221. The following program performs circular interpolation in the X-Y plane. : : N010 G90 ABSOLUTE SPECIFICATION N011 G17 N012 G03 ...
- マニュアル
... pulses by the pulse weight (0.1000 to 3.2000) is used. Stepdown When the accumulated value is used, this function prevents accumulated value overflow by reducing the number of input pulses. The actual number of input pulses is multiplied by one of four factors (x1, ...
- マニュアル
...P1 Input 0 to 9999 0 Yes r – – – S 2 d value input Parameter 009 Digit shift -3 to +1 0 – R/W(S) – – – – 1 (10x, -3: x0.001, -2: x0.01, *2 -1: x0.1, 0: x1, 1: x10) 010 PV instantaneous value 0 to 100.000 – R/W(S) – – – – 4 conversion coefficient 99999.9999 0 (number of pulses per second at instantaneous value output 100% is set) 011 Number of moving average 1 to 16 16 – R/W(S) – – – – 1 data at PV instantaneous value conversion Accumu-late 012 Q1 Accumulated value (lower 0000 to 9999 0 Yes...
- マニュアル
... - Yn}/{Xn+1 - Xn}] x {input data S - Xn} Y Equation: Yn+1−Yn f (Y)= Yn+ Xn+1−Xn (S−Xn) Yn+1 D Calculation result Yn+1-Yn Yn Xn+1−Xn S−Xn X0 Xn S Xn+1 X Input data Y0 179 Section 7-14 Improved Instructions Content of the First Word Address of Linear Data (T) 15 14 13 12 11 10 9 T 0 0 0 1 1 0 8 7 6 5 4 3 2 1 0 0 m−1 (00 to FFHex) m: Number of coordinates minus one (0 < m < 257)...
- マニュアル
... Hex is set.) 89 Section 2-14 Special Math Instructions The coordinates of the m+1 points, which define m line segments, are entered in a linear data table beginning from C+1 as shown below. Enter all coordinates in hexadecimal form. ...
- マニュアル
... Units OPERATION MANUAL (CJ1W-NC214/234/414/434) 7-68 Memory Operation A factor can be set for the speed that is used for automatic replay. The factor is x1 when the memory operation preview is started. The replay speed can be selected from ...
- マニュアル
...D200 8 APR C C:Control word S S:Source word D D:Result word Scaled data 8-1-4 Flow of Operation Descriptions of APR Instruction Y1 D Scaled result Y0 X0 S Input data X1 Unscaled data CP1E CPU Unit Hardware User’s Manual(W479) 8-13 8 Using Expansion Units and Expansion I/O Units C: Control word Set for “Signed Integer Data (Binary)”. Control word setting #0800: Binary numeral (0000 1000 0000 0000) 8 15 14 13 12 11 10 9 C 0 0 0 0 1 0 7 6 5 4 3 2 1 The ...
- マニュアル
...Number of coordinates minus one (m-1), 00 to FF hex (1 ≤ m ≤ 256) Floating-point specification for S and D 1: Single-precision floating-point data 16-bit BCD16-bit binary (signed or unsigned) or 16-bit BCD data C+1 ...
- マニュアル
... top of the trapezoid (unit: mm) Rbottom The radius of the bottom of the trapezoid (unit: mm) Cartesian3DWorkspace The shape of Cartesian3D workspace is a rectangular solid. Workspace dz Zm dy Ym dx Origin of the workspace (...
- マニュアル
...be used for the two-point correction of the channel analog input measured value. -400 to 5000 Set the decimal point position for the channel analog input measured value (INT and DINT). 0: ×1 °C or °F 1: ...
- マニュアル
... transformation of data from the NX-series High-speed Analog Input Unit. FB/FUN name Scale transformation for NX-series Highspeed Analog Input Unit FUN Graphic expression ST expression ScaleTrans_HAD( SclIn, SclOut, ...
- マニュアル
...Movement_X: Total travel distance (X) Movement_Y: Total travel distance (Y) Xone: 1 time travel distance (X) Xone = Movement_X/ 4 Yone: 1 time travel distance (Y) Yone = Movement_Y/ 4 (X2,Y2) Movement_Y (X1,Y1) Start position (...
- マニュアル
...D200 8 APR C C:Control word S S:Source word D D:Result word Scaled data 8-1-4 Flow of Operation Descriptions of APR Instruction Y1 D Scaled result Y0 X0 S Input data X1 Unscaled data CP2E CPU Unit Hardware User’s Manual(W613) 8-13 8 Using Expansion Units and Expansion I/O Units C: Control word Set for “Signed Integer Data (Binary)”. Control word setting #0800: Binary numeral (0000 1000 0000 0000) 8 15 14 13 12 11 10 9 C 0 0 0 0 1 0 7 6 5 4 3 2 1 The ...
- マニュアル
... sent forward. F Move to trigger position Button Click this button to move to the time at which the file save trigger changed to TRUE. G Playback speed multiplier Drop-down list You can select the playback speed from among ...
- マニュアル
...&) * 2 ^ I& Next RESPONSECODE& = -1 RESPONSEVALUE&(0) = ERROR& Return EndIf If ANGLE# > 180 Then RADIAN# = (ANGLE# - 360) / 180 * PI# Elseif ANGLE# <= -180 Then ANGLE# = RADIAN# = (ANGLE# + 360) / 180 * PI# Else RADIAN# = ANGLE# / 180 * PI# EndIf RBT_...
- マニュアル
...07h Offset value for zero reset Zero reset mode 02h 03h LOW threshold value HIGH threshold value 30h Unit No. and Parameter No. 2Eh Section 3 01h 0: OFF 1: ON -20000 to 20000 (X0.0001) 2Dh Scaling mode Remarks 0: OFF 1: PEAK 2: BOTTOM 3: P-P 4: AVERAGE 5: SAMPLE 0: External 1: Self-up trigger 2: Self-down trigger -999999999 to 999999999 (nm) 0: REAL 1: HOLD -999999999 to 999999999 (nm) -999999999 to 999999999 (nm) ZS Series CompoWay/F Communication Command Reference 3-7 Section 3 Setting Value Obtaining and Changing Command (Note 2) The same ...
- マニュアル
... reading result coincides the number of times you have set, the reading result is output to the RS-232C interface. The verification system is AND verification (Continuous coincidence system). (This cannot be changed.) Menu sheet Reading once and verification zero times Command ...
- マニュアル
... reading result coincides the number of times you have set, the reading result is output to the RS-232C interface. The verification system is AND verification (Continuous coincidence system). (This cannot be changed.) Menu sheet Reading once and verification zero times Command ...
- マニュアル
...Scroll X This is the amount of position -99,999.9999 to 99,999.9999 compensation for the X coordinate. DY Scroll Y This is the amount of position -99,999.9999 to 99,999.9999 compensation for the Y coordinate. ...
- マニュアル
... function (order of the measurement data) The measurement data is output in order. Format: LPR(start_number,number_of_data,data_1, data_2,...data_5) You can omit data 2 to data 5. Examples: LPR (0, 3, I0.X, I0.Y, I0.Z) ...