全 202 件が検索されました。(181 - 200件を表示)
- マニュアル
... - Yn}/{Xn+1 - Xn}] x {input data S - Xn} Y Equation: Yn+1−Yn f (Y)= Yn+ Xn+1−Xn (S−Xn) Yn+1 D Calculation result Yn+1-Yn Yn Xn+1−Xn S−Xn X0 Xn S Xn+1 X Input data Y0 179 Section 7-14 Improved Instructions Content of the First Word Address of Linear Data (T) 15 14 13 12 11 10 9 T 0 0 0 1 1 0 8 7 6 5 4 3 2 1 0 0 m−1 (00 to FFHex) m: Number of coordinates minus one (0 < m < 257)...
- マニュアル
... Hex is set.) 89 Section 2-14 Special Math Instructions The coordinates of the m+1 points, which define m line segments, are entered in a linear data table beginning from C+1 as shown below. Enter all coordinates in hexadecimal form. ...
- マニュアル
... = INT((Search model quantity + 11)/12)*(33.3 or 16.7) ms (0, 0) 1 2 3 Model image 0 B C If the search processing function is executed on models “A” to “3” in the figure, respective coordinate positions (...
- マニュアル
...-1 ZEN-10C@@@-@ I0 to Ib (12 bits) f (16 bits) 0 to D0 to Df (16 bits) Work bits M0 to Mf (16 bits) Holding bits H0 to Hf (16 bits) Expansion I/O Unit input bits X0 to Xb (12 bits) Expansion I/O Unit output bits Y0 to Yb (12 bits) Analog comparators A0 to A3 (4 bits) Comparators P0 to Pf (16 bits) 7 (8 bits) D0 to D7 (8 bits) Application Precautions for Differences between Versions Memory Cassette Compatibility Be aware of the following restrictions when using a Memory Cassette containing a program that ...
- マニュアル
... with 10 I/O points @ @ @ @ @ @ @ @ Q0 Q1 Q2 Q3 Q4 Q5 Q6 Q7 CPU Units with 20 I/O points When One or More Expansion I/O Units Are Connected Expansion I/O Unit input bit (X) status ( : OFF/●: ON) X0 X1 X2 X3 X4 X5 X6 X7 X8 X9 Day display SU: Sunday MO: Monday TU: Tuesday WE: Wednesday TH: Thursday FR: Friday SA: Saturday Xa Xb Note: The display depends on the number of input points on the connected Expansion I/O Units. Expansion I/O Unit output bit (Y) status (@: OFF/■: ON) ( ( ( ( ( ( ( ( ( ( ( ( Ya Yb Y0 Y1 ...
- マニュアル
...: Expansion 0, Y0 to Y3 Bits 4 to 7: Expansion 1, Y4 to Y7 Bits 8 to 11: Expansion 2, Y8 to YB --- 0016 Expansion I/O input bit status H'00000000 to H'00000FFF (-) Bits 0 to 3: Expansion 0, X0 to X3 Bits 4 to 7: Expansion 1, X4 to X7 Bits 8 to 11: Expansion 2, X8 to XB --- 0017 8-digit comparator bit status H'00000000 to H'0000000F Comparator number specified by leftmost 2 digits of address. Bit 0: G0 Bit 1: G1 Bit 2: G2 Bit 3: G3 --- Data range (unit) Remarks Page • ...
- マニュアル
...07h Offset value for zero reset Zero reset mode 02h 03h LOW threshold value HIGH threshold value 30h Unit No. and Parameter No. 2Eh Section 3 01h 0: OFF 1: ON -20000 to 20000 (X0.0001) 2Dh Scaling mode Remarks 0: OFF 1: PEAK 2: BOTTOM 3: P-P 4: AVERAGE 5: SAMPLE 0: External 1: Self-up trigger 2: Self-down trigger -999999999 to 999999999 (nm) 0: REAL 1: HOLD -999999999 to 999999999 (nm) -999999999 to 999999999 (nm) ZS Series CompoWay/F Communication Command Reference 3-7 Section 3 Setting Value Obtaining and Changing Command (Note 2) The same ...
- マニュアル
... reading result coincides the number of times you have set, the reading result is output to the RS-232C interface. The verification system is AND verification (Continuous coincidence system). (This cannot be changed.) Menu sheet Reading once and verification zero times Command ...
- マニュアル
...Reference angle ST Reference angle Detection point X RX Detected coordinate X Detection point Y RY Detected coordinate Y Correlation 0 CR00 Correlation 0 108 Shape Search+ FZ3 Processing Items List Manual X00 Position ...
- マニュアル
...Length difference among the 4 corners. Defect depth 0 DP0 0.0000 to 99999.9999 Defect depth of defect No. 0. Defect width 0 WD0 0.0000 to 99999.9999 Defect width of defect No. 0. Defect position X0 DX0 -99999.9999 to 99999.9999 X coordinate of defect No. 0 Defect position Y0 DY0 -99999.9999 to 99999.9999 Y coordinate of defect No. 0 Defect depth 99 DP99 0.0000 to 99999.9999 Defect depth of defect No. 99. Defect width 99 WD99 0.0000 to 99999.9999 Defect width of defect No. 99. Defect position X99 DX99 -...
- マニュアル
...0 to 99999.9999 0 W --- Reference width Acquisition only 0 to 99999.9999 0 SW --- 7 Width difference Acquisition only 0 to 99999.9999 0 DF Logged data 8 Edge position X0 Acquisition only −99999.9999 to 99999.9999 0 --- --- 9 Edge position Y0 Acquisition only −99999.9999 to 99999.9999 0 --- --- 10 Edge position X1 Acquisition only −99999.9999 to 99999.9999 0 --- --- 11 Edge position Y1 Acquisition only −99999.9999 to 99999.9999 0 --- --- 12 Reference position ...
- マニュアル
... types of multiple data output functions. • Data logging order: LPR function The measurement data is output in order. Format: LPR (start_number,number_of_data,data_A, data_B,data_C...) Output Example: LPR(0,3,I0.X,I0.Y,I0.Z) ...
- マニュアル
...Reference Reference angle ST Reference angle Detection point X RX Detected coordinate X Detection point Y RY Detected coordinate Y Correlation 0 CR00 Correlation 0 124 Shape Search+ FZ4 Processing Items List Manual Position ...
- マニュアル
.../FZ5 Series Macro Customize Functions Programming Manual (Z367) Int (Reference: Details (p.309)) UnitData (Reference: Details (p.520)) Ut (Reference: Details (p.534)) Macro Command Reference 199 DrawBox Draws a rectangle on the image window. Format DrawBox <...
...構いません。 ) Turbo PMAC アプリケーションから Power PMAC への変換 118 Power PMAC アプリケーションノート 2019 年 6 月 • CompTable[m].X0[0] = 0 // Turbo のテーブルが、ソースのゼロ点位置から常時開始 • CompTable[m].Dx[0] = z // ソースモータのカウント単位での、テーブルのスパン Turbo PMAC のテ...
...値は y0 です。 4. ACC59E3_0_IN1 の M 変数によって表示されるソフトウェアカウントを監視および記録します。 この値は x0 です。 ソフトウェアカウント Sin を入力電圧 Vin [V]に変換する較正後の方程式は、次のようになります。 (𝑦 −𝑦0 ) 𝑆𝑖𝑖 1 −𝑥0 ) 𝑉...
- ソリューション
... B M - 0 0 0 形式 2 7, 5 0 0 34,500 25,000 2 7, 5 0 0 3 7, 0 0 0 2 7, 5 0 0 標準価格 (¥) ◎ E 5 D C - R X0 A B M - 0 15 25,000 ー ◎E5DC-R X2 ABM- 000 22,000 ー ー ◎E5DC-R X2DBM- 000 22,000 ー ー ◎ E 5 D C - Q ...
... for scaling settings Unscaled value (original data D300) Analog output word (CIO 102) *: Refer to page 4 for the detail of the APR instruction. Reference: Detail of APR instruction Scaled data Y1 D Scaled result Y0 ...
...APR 命令の説明は 4 ページを参照ください。 参考:APR 命令の説明スケーリング後のデータ Y1 D 変換結果 Y0 X0 S 入力データ X1 スケーリング前のデータ C:コントロールデータ先頭チャネル 「符号付き整数データ(BIN)指定時」の設定を行います。...
...を求めるDIST関数」を使用します。 X 座標直線 方法 1:近似直線 垂線 処理項目:近似直線 ・距離 Y 点 (座標 X0,Y0) 複数の座標から近似直線を算出し、 その近似直線と任意の点との垂線の距離を求めることができます。 計測フロー 「機能選択」 にて n.近...