全 202 件が検索されました。(21 - 40件を表示)
- マニュアル
...長 00Hex 07Hex 08Hex AAHex データ部 データ部距離データ PCD ヘッダ x76799 y76799 z76799 LSB LSB LSB MSB MSB MSB … x0 LSB y0 MSB LSB z0 MSB LSB MSB 結果取得フォーマットが、0100Hex:距離データ(極座標形式)+振幅データの場合、 横 320 ピクセル、縦 240 ピクセル、各画素 2 バイトの距離データに続けて、横 ...
- マニュアル
... pressed. (1) Mount the Amplifier Units one at a time onto the DIN track. Fix the sensor head with M3 screws. Apply tightening torque of 0.5N・m for fixing. ON Operation level x1.1 Operation level Operation level ...
- マニュアル
... setting: Adjust the received light amount to "0" when the button is pressed. Threshold setting: Set the light intensity of approximately 7% when the button is pressed. 9999 ■Joining Amplifier Units ON Operation level x1.1 Operation level Operation level ...
- マニュアル
... Display * Stable operation area * Unstable operation area [OUT Indicator:Orange] * Turns ON when Output is ON. Stable operation [STABILITY Indicator: Green] area Operation level x1.1 Operation level Operation level ...
- マニュアル
... there is a risk of minor injury from electrical shock or other source if the product is disassembled. STABILITY indicator 28.9 Emitter center Centre de l’émetteur ON Operation level x1.1 Operation level Operation level ...
- マニュアル
.... It represents the least unit count among the mutual interference prevention unit count of E3NX and E3NC. Check the mutual interference prevention unit count and response speed of each model. BANK saving available STND GIGA SHS 250μs 1ms 16ms 50μs x1 ...
- マニュアル
... receiving light amount) hs 3000 UP/DOWN HS High-speed Mode stnd 3000 3000 Giga Power Mode Light amount difference(ms or μs) BANK saving available STND GIGA SHS 250μs 1ms 16ms 50μs x1 x0.33 1 (reference) x1 Response time Light quantity Time off Problem Cause Remedy Nothing is shown on the indication. No power supplied or the cable broken Check the wiring, connector connection, power supply voltage and power supply capacity again. Refer to "1-2 Input/Output Circuit Diagram" Nothing is shown on the digital indication. Eco mode is ON. Turn OFF Eco mode. Sensing/...
- マニュアル
.... MODE Move to Detection Mode by holding the button for 3 seconds or longer. A *1. The relationship between the control output and output switch during area detection mode is as follows: ] Function Selection: [ A Cause Error Name / Display ...
- マニュアル
... pressing the f ---fd Model Eco function ON MODE (a)Off-delay Timer 4-2 Ratings and Specifications *1 Refer to "⑤Detailed Settings". *2 Refer to "1-3 Mounting Amplifier Unit" *3 Refer to "③Convenient Setting Features" Error Name / Display ...
- マニュアル
... the digital indication. Sensing/Detection not possible despite the minimum threshold level The OUT indicator blinking DPC OFF Light amount difference Passing time(ms or μs) Disable Release the button to stop holding f nd SHS 50μs ...
- マニュアル
... Refer to "③Convenient Setting Features" Model Control output Connection method Light source (Wavelength) Power supply voltage Power consumption *1 Control output Incident light level displayed The zero reset function is enabled. in a negative value Error Name / Display ...
- マニュアル
...for E3NX-FA11-5. fd A 4-1 Troubleshooting Lost tracking of the settings made 50 shs %ff Normal MODE f ---- bar 14. Inverted Display *7 Mounting Amplifier in Inverted Direction The display reverses. x0.1 4. Timer Function Setting Output Timer (Two outputs are displayed for the two-output type) (a) 0 x8 GIGA Giga Mode (a)Off-delay Timer 4 Maintenance Problem DPC ON Light amount difference Passing time(ms or μs) 0m x1 %n Passing time and light amount difference are displayed. MODE 1 (reference) SHS2* 60μs 150p MODE UP/DOWN dpc Time Off Passing time Light ...
- マニュアル
...Lost tracking of the settings made. The light intensity level display changes. shs GIGA Giga Power Mode CH number (e) Bottom receiving light amount 8000 2000 (b) MODE MODE Time Off 4 Maintenance Problem ...
- マニュアル
...(a) to set to [SoLU on]. To release the setting, press the [MODE] and [L/D] buttons for at least 3 seconds to set to [SoLU oFF]. Let the workpiece pass. 0m 4-1 Troubleshooting The light intensity level display changes. ...
- マニュアル
...Or check the settings again. *2 corrected, Hold the 24 Long-press the button for 7 seconds or longer in the Detection Mode to set this function. Percentage tuning ON Failed internal data read / out SHS 100μs ...
- マニュアル
... Error Displayed incident light level 24 n tune Tuning Initializing all settings to factory-set defaults Setting initialization Tuning Error Stabilizes the displayed incident level by correcting internal incident level changes. shs SHS 50μs ...
- マニュアル
... Function Increasing / decreasing emission power The emission level can be increased / decreased with 4. Selection of EASY / PRO Mode Changing settings of 5 to 16 Incident light level is too low. Incident light level is too high. shs SHS 50μs ...
- マニュアル
...ホールド設定に遷移します。 m e a s XXXX 補正元流量値 【4-4】補正先流量値 検出流量 補正先流量値 係数 x0.75 係数 x1.5 ※【4-1】スケーリングモード設定が流量入力モードのとき表示補正先の流量値を入力します。 c o r r XXXX 補正先流量値 6...
- マニュアル
... the user's manuals for Communications Coupler Units. If you will use a Communications Coupler Unit, refer to Related Manuals on page 30 to identify the manual for your Unit. • This user's manual omits the "x" sign for units displayed in decimals. For example, "...
- マニュアル
... the user's manuals for Communications Coupler Units. If you will use a Communications Coupler Unit, refer to Related Manuals on page 29 to identify the manual for your Unit. • This user's manual omits the “x” sign for units displayed in decimals. For example, “...