全 2903 件が検索されました。(221 - 240件を表示)
- カタログ
... and becoming damaged, or hitting someone and causing injury. 4. Do not use the product if the product is dropped by mistake, as the inside of the product may be damaged. 5. Install a switch or circuit breaker and provide an appropriate indication ...
- カタログ
... close gates. Water level monitor Not just liquids, but any conductive detection object can be detected. One side of the 61F is connected to an Electrode and wire and the other side is connected to ground. The winding machine must also be grounded, ...
- カタログ
... to MAINTENANCE mode during operation. Locking the A22LK-2RLB-@ in the RUN position prevents the facilities from being stopped unintentionally. Guard Lock Safety Door Switch D4SL-N Safety Key Selector Switch A22TK I take the key with me when I enter, ...
- カタログ
...transportation, use, and disposal of the control panel (product). According to OMRON investigation in May 2023. 4 Pushbutton Switches Push-In Plus Terminal Block Series - A22N-P/A30N-P/M22N-P/A22NE-P Improved Workability in Wiring and Installation Rear Insertion Is Used, ...
- カタログ
... damaged if you insert the screwdriver straight in. • Do not allow the flat-blade screwdriver to fall out while it is inserted into a release hole. • Do not bend a wire past its natural bending radius or pull on it with excessive force. Doing ...
- カタログ
... meet the specified panel dimensions. Panel hole dimension Panel thickness 22.3 dia. 1 to 5 mm 22.3 +0.4 0 • Do not tighten the Tightening Nut more than necessary using tools such as pointed-nose pliers. • Doing ...
- カタログ
...Operation double-stopped Key: Cannot be removed Key: Can be removed Guard Lock Safety-door Switch Safety Key Selector Switch 2 D4JL A22TK 3 1 4 I take the key with me when I enter, so there is no worry of becoming trapped inside! D4JL 4 Lock the door UNLOCK A22TK 3 LOCK Operation starts End maintenance MAINTENANCE Operation stopped Key: Can be removed Key: Cannot be removed Furthermore 2 Same Key By using the Enabling Grip Switch during maintenance and by using a Safety Laser Scanner or Safety Mat to detect the presence of operators, equipment malfunctions can be ...
- カタログ
.... Use the switch within the operating range. (Refer to the diagram below.) Even when using microload models within the operating range shown below, if inrush current occurs when the contact is opened or closed, it may cause the contact surface to become rough, and ...
- カタログ
..., if not avoided, will result in minor or moderate injury, or may result in serious injury or death. Additionally there may be significant property damage. Do not wire the Switch or touch any terminal of the Switch while power is being supplied. Doing ...
- カタログ
... Key Selector Switch KM1 to KM4: Magnetic contactors M1 to M2: Motor Timing Chart
(10) Emergency Stop Switch S1 Reset switch S2 Unit 1 S14, S24 Note: The lock release enable signal must be configured ... - カタログ
... one of the three phases is reversed, the Relay does not turn ON and the contactor is not energized. • To protect the motor from damage due to open phase, the wiring must be performed in exactly the same way as shown in this figure (i.e., ...
- カタログ
... following precautions. *2. You cannot use the interrupt inputs for interrupts. You can use them as normal inputs. *3. Change the power supply voltage from 12 VDC to 24 VDC. CQM1-IA121 CJ1W-IA111*4 *4. The CJ1W-IA111 provides 16 points, ...
- カタログ
...Note: 1. Connect the shield wire at both ends of the cable carrying RS-422A/485 signals to ground, and ground the ground terminal on the Power Supply Unit of the CPU or Expansion Rack to 100 Ω max. 2. The CJ1W-CIF11 is not insulated, ...
- カタログ
...for optical transmission systems of C-series SYSBUS, SYSMAC LINK, and Controller Link. Optical Fiber Assembly Tool * Manufacturer Standards Sumitomo Electric Industries, Ltd. CAK-0057 − * There is a risk of quality problems when using cables assembled by typical users, ...
- カタログ
... or baud rates: Trunk line and branch lines Connections for Slave Units and Repeater Units: T-branch or multidrop connections *1. FINS message communications are supported by CJ-series Controllers only. *2. Drop-line connections are not supported with a baud rate of 4 Mbps, ...
- カタログ
... of Fixed allocations Units mountable to User-set allocations Controller 3 Weight 118 g max. 16 *1. Refer to the DeviceNet Operation Manual (W267) for the communications power supply specifications. *2. The Device Unit uses a node, and ...
- カタログ
...-CN313 0.3 m CS1W-CN713 0.7 m CS1W-CN223 2m CS1W-CN323 3m CS1W-CN523 5m CS1W-CN133 10 m CS1W-CN133-B2 12 m • Install the Racks and select I/O Connecting Cables so that the total length of all I/O Connecting Cables does not exceed 12 m. • The following diagram shows where each I/O Connecting Cable must be connected on each Rack. The Rack will not operate if the cables aren't connected properly. (The "up" direction is towards the CPU Unit and "down" is away from the CPU Unit.) CPU Rack Power ...
- カタログ
... connected as one of the five Units immediately next to the CPU Unit. If an Interrupt Input Unit is connected in any other position, an Incorrect Unit/Expansion Rack Connection error will occur. • Set the pulse width of signals input to the Interrupt Input Unit ...
- カタログ
... the PCU beforehand to perform a series of operations automatically. Continuous positioning and speed changes are also possible. Sequence function Memory operation data incorporates a sequence feature that allows for repetition of a given operation, start/end of operation data via external inputs, and ...
- カタログ
...Current consumption at 5 V (internal logic power supply) Current consumption at 24 V (relay driving power supply) Condition 2: Power Requirements For each Rack, the upper limits are determined for the current and power that can be provided to the mounted Units. Design the system ...