全 50426 件が検索されました。(2361 - 2380件を表示)
- マニュアル
... firmly. Also, be sure that the coaxial cable is locked before use. Attaching Connectors to Coaxial Cable Assemble the connector parts as shown below. Contact clip Body Sleeve Ferule Contact Approx. 24.3 mm A hand crimp tool (...
- マニュアル
... that the current will be converted into Joule heat by the resistance of the inductive load. This time lag, between the moment the circuit is opened and the moment the load is reset, caused by this method is longer than that caused by the ...
- マニュアル
...(Any other setting disables the start code, causes a non-fatal error, and turns ON AR 1302.) 12 to 15 End code selection for no-protocol communications 0 (Hex): Disables end code; 1 (Hex): Enables end code in DM 6649; 2 (Hex): Sets end code of ...
- マニュアル
... characters Data Format Byte +0 P (See note 1.) Note +1 +2 +3 +4 +5 Data on the number of rotations Sign (+ or -) Whole numbers (5 digits of decimal numbers) +6 +7 CR 1. “P" of ASCII code. It is 50 Hex in hexadecimal. 2. The range of No. of rotations that can be received by the unit is between +65535 to -65535. 3. For details of the data on the number of multi-turns received from a servo driver, please check the manual of the servo driver in use. 4. Please set the unit function setting "high-speed ...
- マニュアル
... locked securely before starting operation. 2-1-4 Attaching Connectors to the Coaxial Cable The following diagram shows the parts that make up the BNC connector. Body Sleeve Contact crimp Ferrule Contact Approx. 24.3 mm A hand crimp tool (...
- マニュアル
...Transfer direction Method Max. amount of data Data transmission Execution of TXD(236)/ 256 bytes (PLC → External device) TXDU(256) in the program* Frame format Start code End code Yes: 00 to FF Yes: 00 to FF or ...
- マニュアル
... strength value of the diode may be two to three times circuit is opened and the moment the load is reset, caused by this method is larger than the supply voltage if the surge protector is applied to electronic longer than that caused by the ...
- マニュアル
... system × 2 m • Total cable length ≤ 20 m • Length of a single cable ≤ 4 m (for a 1:1 connection) 15 devices max. including the GP-IB Interface Unit GP-IB device address Delimiters 0 to 30 Select from the following: ...
- マニュアル
...× 4 Rotary: 1V/250r/min × 10 Linear: 1V/100mm/s 7 Motor rotation speed × 8 Rotary: 1V/125r/min × 100 Linear: 1V/10mm/s 8R Reserved 9R Reserved AR Reserved BR Reserved CR Reserved DR Reserved ER Reserved Reserved 1 Analog monitor 2 2 Reserved --- 0 3 Reserved --- 0 S Reserved 0 Reserved 1R Reserved constant 0-F Enable ● --- Motor rotation speed Rotary: 1V/1000r/min, Linear: 1V/1000mm/s R Support tool initial value 0002H 2 0 F Pn004 Lower limit 2 Advanced function selection switch 3 0 Unit 2 --- 0000H 1210H --- 0200H ∆ 0 0 ∆...
- マニュアル
...1011 B 1100 C 1101 D 1110 E 1111 F 0000 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0001 1 DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US 0010 2 Space ! ” # $ % & ’ ( ) * + , . / 0011 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 0100 4 @ A B C D E F G H I J K L M N O 0101 5 P Q R S T U V W X Y Z [ \ ] ^ _ 0110 6 a b c d e f g...
- マニュアル
....) is being sent as an attached file in TXT format, the data is stored with the following procedure. 1. The word data is converted to ASCII. 2. The word data is delimited by hard tabs ([HT]: 09). 3. A return and line feed ([...
- マニュアル
...1011 B 1100 C 1101 D 1110 E 1111 F 0000 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0001 1 DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US 0010 2 Space ! ” # $ % & ’ ( ) * + , . / 0011 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 0100 4 @ A B C D E F G H I J K L M N O 0101 5 P Q R S T U V W X Y Z [ \ ] ^ _ 0110 6 a b c d e f g...
- マニュアル
... to EC Directives Countermeasure Examples When switching an inductive load, connect an surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes Yes Power supply Inductive load ...
- マニュアル
.../Parallel Structure 13 Illegal Axis Declaration 14 Position Specification Error 15 Speed Specification Error 16 Time Specification Error 98 Detailed description Number of blocks of programming exceeded 800. ----Number of characters in one block exceeded 128 including ...
- マニュアル
... to EC Directives Countermeasure Examples When switching an inductive load, connect an surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes Yes Power supply Inductive load ...
- マニュアル
...2 outputs CRT1-DA02 I/O capacity 4 inputs Model CRT1-VAD04S 2 outputs CRT1-VDA02S 4 inputs CRT1-VAD04ML 2 outputs CRT1-VDA02ML X1 X10 63] [0- 04 AD T1- AL CR MIN N TER RO G ALO OM AN Features I/O range: 0 to 5 V, 1 to 5 V, 0 to 10 V, −10 to 10 V, 0 to 20 mA, 4 to 20 mA Units with Connectors Type Analog I/O Slave Units with e-CON Connectors Analog I/O Slave Units with MIL Connectors 24 Appearance Features I/O range: 0 to 5 V, ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
...times Capacitor Relay Approx. 2 to 3 times Approx. 20 to 50 times Resistance load 1 • Absorption Element Example Absorption element Effectiveness 16 Diode Diode + Zener diode Varistor CR ❍ ❍ ∆ ✕ Normal current As an absorption element, the diode is the most effective at suppressing the counter-electromotive force. The release time for the solenoid or electromagnetic valve will, however, increase. Be sure to check the circuit before use. To shorten the time, connect a Zener diode and a regular diode in series. The release time will be shortened at the same rate that the Zener voltage (Vz) of the Zener diode ...
- マニュアル
.... Unit 8 bits @ 0 X Always 0. Bank X X Header code (2 letters) Point X X Address X X Data code X Text X FCS * CR Terminator Start character Range for FCS calculation Each block begins with a start character, @ (40hex), and the unit number of the E5ZD which is to receive or send the block, and ends with an FCS and a terminator. The data code identifies the type of text being transmitted. The unit number must be between 0hex and Fhex. The terminator consists of * (2Ahex) and a carriage return (0Dhex). 3-2-3 Communications Errors...