全 50426 件が検索されました。(2341 - 2360件を表示)
- マニュアル
..., or 1:1 link slave NODE NO DELAY START CODE END CODE DATA LINK AREAS 0 0 None None None 00 to 31 0 to 9,999 ms 00 to FF 00 to FF or CR, LF LR 00 to LR 63, LR 00 to LR 31, or LR 00 to LR 15 Determines the settings used when a device, such as a Programmable Terminal or bar code reader is connected to the RS-232C port. Do not set the node number to a number already used by another Unit connected in the same communications system (e.g., Host ...
- マニュアル
... the current will be converted into Joule heat by the resistance of the inductive load. This time lag, between the moment the circuit is opened and the moment the load is reset, caused by this method is longer than that caused by the ...
- マニュアル
... least five times as large as the circuit voltage. 92 Section 3-1 Settings DC Relay DC RY AC RY Surge absorption diode (Fuji Denki's ERB44-06 or equivalent) AC Relay Surge absorber (Okaya Denki's CR-50500 or equivalent) Solenoid Solenoid Surge absorber (Okaya Denki's ...
- マニュアル
...9 1010 A 1011 B 1100 C 1101 D 1110 E 1111 F SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US ! ” # $ % & ’ ( ) * + , . / 1 2 3 4 5 6 7 8 9 : ; < = > ? A B C D E F G H I J K L M N O Q R S T U V W X Y Z [ \ ] ^ _ p a b c d e f g h i j k l m n o q r s t u v w...
- マニュアル
...utdevicesbased卯the ONゆFFstatusofinputdevicesandwritethisprogramintothememoryon theCPUBoardusingtheProgra而mingConsole. NoteRefertotheMin'H-typePCs,:C20128/401160H(VVf76]CPPera伽 〃a旬a'fordeta目sonwri肋gtheprogram・ 2 ` ---------------------[End of Page 6455]--------------------- '■rC..." ミ・ミ 、17(.イ〆.r〆..(レ ...
- マニュアル
... 0001 equals 10 ms Node number (Host link) 00 to 31 (BCD; default: 00)) Start code enable (RS-232C) 0: Disable (default); 1: Set End code enable (RS-232C) 0: Disable (default; number of bytes received) 1: Set (specified end code) 2: ...
- マニュアル
... the current will be converted into Joule heat by the resistance of the inductive load. This time lag, between the moment the circuit is opened and the moment the load is reset, caused by this method is longer than that caused by the ...
- マニュアル
... non-procedure mode start code enable cedure 0: Disabled (default); 1: Enabled 12 to 15 Non-pro- Port B non-procedure mode end code enable cedure 0: Disable (Specify the number of receive data items) (default) 1: Enable (Specify the end code) 2: ...
- マニュアル
...Section 4-1 Overview 4-1 Overview The following operations are covered in this section. Operation Command/function Opening a communications port OPEN command Sending data PRINT command (The LPRINT command executes device: LPRT.) Receiving data ...
- マニュアル
... transmission method Asynchronous Baud rate 9,600 bps Start bit 1 bit Stop bit 1 bit Parity Even Character code ASCII 7 bits Data format 8 characters (P or A) (+ or –) (0 to 9) x 5 digits (CR) Serial Data P or A, Start bit 0 to 9 + or – Data ...
- マニュアル
...'scomplementofSUM. 3.CRC(CyclicRedundancyCheckCode) Thismoderegardsthewholedataasabitstring(messagepolynomial),divides thisstringbythefixedconstant(geRerativepolynomial),anddefinestheremain・ derasthecheckcode. CRCdetectserrorsbetterthantheverticalparityorhorizontalparity,andisused widelyinLANs,etc(Forexample,theSYSMACLINKusesCRC-CCI"). VariouskindsefCRCcanbeused.Thecalculationmodedefinedaccordingto theCCITTrecommendationisca‖edCRC-CCIrr,where×16+×12+X5+1is usedasthegenerativepolynomial.(incidentally,CRC-16(×16+X12+X2+1)is alsooftenusedasageneratingPolynomiat.) ∠「・、=CheckCode ...
- マニュアル
...256 01 1 to to FF 256 Value (Hex) No-protocol Mode end code setting 0 None (Specify the amount of data being received) 1 Yes (Specify the end code) 2 End code is set to CR+LF Value (Hex) No-protocol Mode start code setting 0 None 1 Yes Address 166@@@@ RS-232C port Value (Hex) 0000 0001 to 0007 Maximum Unit No. in NT Link Mode No. 0 No. 1 to No. 7 Address 195@@@@ Value (Hex) Scheduled interrupt time units 0000 10 ms 1.0 ms 0001 Note These settings are not supported for CS1D Duplex-CPU ...
- マニュアル
...1011 B 1100 C 1101 D 1110 E 1111 F 0000 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0001 1 DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US 0010 2 Space ! ” # $ % & ’ ( ) * + , . / 0011 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 0100 4 @ A B C D E F G H I J K L M N O 0101 5 P Q R S T U V W X Y Z [ \ ] ^ _ 0110 6 a b c d e f g...
- マニュアル
... the port parameters as follows: • Port 1 Parameters Data length: 8 bits Parity: None Stop bits: 1 Header code: Disabled Delimiter code: Enabled Flow control: Enabled Baud rate: 9,600 bps Delimiter code ...
- マニュアル
... PC is built are switched 5 times or more a minute, then measures need to be taken. Examples Inductive Load Surge Suppressor Connect a surge suppressor or diode in parallel with the load, as shown in the following diagrams, when switching inductive loads. ...
- マニュアル
... 15 of Wd after execution. Flags ER (A50003): CY (A50004): EQ (A50006): N (A50008): Example When CIO 000000 is ON in the following example, the status of bit 15 of CIO 0100 is shifted into bit 00 of CIO 0100 and into ...
- マニュアル
...xxi 6 EC Directives Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC Power supply Yes Yes Inductive load ...
- マニュアル
... times or more per minute. Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC Yes Power supply xxii Inductive load ...
- マニュアル
... that the current will be converted into Joule heat by the resistance of the inductive load. This time lag, between the moment the circuit is opened and the moment the load is reset, caused by this method is longer than that caused by the ...
- マニュアル
...., a setting of 0001 equals 10 ms protocol 00 to 07 Host Link unit number 00 to 31 (BCD) Start code enable 0: Disable; 1: Set End code enable 0: Disable (number of bytes received) 1: Set (specified end code) 2: ...