全 50426 件が検索されました。(2421 - 2440件を表示)
- マニュアル
...- (Data Storage Unit system clock) p.3-36 HOUR LENGTH 8BIT 8BIT, 7BIT p.4-5 PARITY NONE NONE, ODD, EVEN STOP 1BIT 1BIT, 2BIT BAUDRAT 38400 9600A19200A38400A57600 A115200 DELIMIT CR CR, LF, CR+LF MODE COMPWAY COMPWAY, NORMAL p.4-5 NODE 0 0 to 16 p.4-5 FORMAT - - p.3-37 FILE No. (current start No.) 0 to 999 p.3-37 KEYLOCK OFF OFF, ON p.3-37 LANGUAG Japanese Japanese, English p.3-38 Section 3 SETUP INFO p.3-35 *1: When [IMAGE] - [SOURCE] - [IMGSAVE] is ON *2: When [IMAGE] - [SOURCE] - [IMGSAVE] is ...
- マニュアル
... is 5 times per minute or higher. Countermeasure Examples When switching an inductive load, connect an surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current C R Power supply Inductive load ...
- マニュアル
...1 1 B VT ESC + ; K [ k { 1 1 0 0 C FF FS , < L \ l | 1 1 0 1 D CR GS - = M ] m } 1 1 1 0 E SO RS . > N ^ n ~ 1 1 1 1 F SI US / ? O _ o DEL R INDEX INDEX A O addresses ................................................................... 14 analog comparator .................................................... 18 ASCII list .................................................................. 42 operation command ...................................................32 B BCC .......................................................................... 10 BCC calculation example ......................................... 11 bit position .......................................................... 16, 21 C calendar timer ........................................................... 25 changing from RUN Mode to STOP Mode ................ 5 command frame ........................................................ 10 command text ........................................................... 10 communications baud rate .......................................... 4 communications data .......................................... 12, 35 communications data length ..........................................
- マニュアル
... with a plurality of pages as a block. (1) Operation to read data in page 1 through 30 as a block The data read process is divided into two steps: read of page 1 through 14 and that of page 15 through 30. ➀0100 0000FFFC [...
- マニュアル
... mode, the basic screen below will appear on the terminal display of the upstream 63 Section 5 Setup Mode To set up a parameter, send the following instructions from the terminal software. Instruction Format Action Parameter definition "(Tag name)" + "=" + "(setting value)" + ...
- マニュアル
...Setting Contents Command 9,600 bps (Use initial setting.) Data length 8 bits (Use initial setting.) Parity Even L3 Stop bits 1 bit (Use initial setting.) Header None (Use initial setting.) Footer CR (Use initial setting.) RS/CS control None P0 Read failure processing Sends ?[...
- マニュアル
... frame (including the terminator) consists of up to 4,106 characters for commands and 4,102 characters for responses. 1 frame Command and Response Format Section 3 Command code × Data × × Terminator × 2 × ...
- マニュアル
...Sending the message data “OMRON” from Controller No. 2. Command Command code Controller No. @ 0 2 T Message data O S R M Terminator FCS O N 1 * 4 CR 2 5 2 2 Command code Message data FCS Terminator 3 Response Controller No. @ 0 2 T O S R M 2 3 O N 1 5 * 4 ...
- マニュアル
... the controller version) p.3-20 DATA BIT 8BIT 8BIT, 7BIT p.4-9 PARITY NON NON, ODD, EVEN STOP BIT 1BIT 1BIT, 2BIT BAUD RATE 38400 9600, 19200, 38400, 57600, 115200 DELIMITER CR+LF CR, LF, CR+LF EMISSION OFF ON, OFF CH OUT OFF ON, OFF BUZZER M OFF, L, M, H p.3-18 ECO OFF ON, OFF p.3-18 COLOR MARINE BLUE MARINE BLUE, GRASS GREEN ORANGE PEEL, STYLISH GRAY, SALMON PINK, NIGHTMARE LANGUAGE – JAPANESE, ENGLISH Section 3 SETUP BUTTON LOCK Default Value p.3-18 p.3-19 ZUV User’s Manual 3-...
- マニュアル
...BUTTON LOCK 3. BUZZER 4. DISPLAY 5. LANGUAGE 6. ALL CLEAR 7. VERSION Set the system environment. Setting value 8 BIT, 7 BIT NON, ODD, EVEN 1BIT, 2BIT 9600,19200,38400,57600,115200 CR,LF,CR+LF When [BUTTON LOCK] is selected: 1. EMISSION 1.OFF 2. CH OUT 2.ON When [BUZZER] is selected: 1.OFF 2.L 3.M 4.H When [DISPLAY] is selected: 1. ECO 2. COLOR When [ECO] is selected: 1.OFF 2.ON When [COLOR] is selected: 1. MARINE BLUE 2. GRASS GREEN 3. ORANGE PEEL When [LANGUAGE] is selected: 4. STYLISH GRAY 5....
- マニュアル
...Introduction How to Use This Manual Page Format Describes the settings. 9,600*, 19,200, or 38,400 None*, odd, or even 77 bits or 8 bits* 1sbit* or 2 bits None*, 02
, or 1B * ETX, 0A LF, 0D CR... - マニュアル
...The format of non-procedural commands are as follows: Example: A command to acquire a measured value MEASURE command * Each character is output as an ASCII code (except for FLOWDATA response). M E A S U R E O ...
- マニュアル
... is 5 times per minute or higher. Countermeasure Examples When switching an inductive load, connect an surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current C R Power supply Inductive load ...
- マニュアル
... command line I/F. Command frame has a Command Code area to control the R/W and Command Data area that is used with Command Code. Terminator that indicates the end of the frame is [LF]. RS-232C requires a start code [SOH], check data, and [...
- マニュアル
... " OMRON" to the ID Controller with controller number 2. Command Controller No. @ 0 2 T S FCS Test data Command code O M R O N 1 Terminator 4 * CR 2 5 2 2 Command code Test data FCS Terminator 3 Response Controller No. @ 0 3 58 RFID System Operation Manual 2 T S 2 O M R 5 O N 1 4 2 * ...
- マニュアル
...PARITY OFF OFF, ODD, EVEN p.104 p.104 STOP BIT 1 1, 2 p.104 BAUDRATE 38400 9600, 19200, 38400, 57600, 115200 p.104 NODE 0 0 to 16 DELMIT CR CR, LF, CR+LF p.104 p.104 WHITE BALANCE - - p.102 ALL CLEAR - - p.102 MEAS CLEAR - - p.103 LANGUAGE - ENGLISH, JAPANESE p.103 VERSION - - p.103 MODE SWITCH LOCK OFF LOCK OFF, LOCK ON p.107 KEY LOCK OFF LOCK OFF, LOCK ON p.107 TEACH IN LOCK OFF LOCK OFF, LOCK ON p.107 PASS NUMBER 0000 0~9999 p.107 OUTPUT (*8) EACH ALL, ...
- マニュアル
...Details Input Set the basic input format items. Output Set the basic output format items. None*/STX/ESC Select the symbol that indicates the beginning (header) of the command format. No symbol will be selected if [None] is selected. Suffix ...
- マニュアル
.... For a description of each command, refer to "List of Non-procedural Commands." •SYSGET/DATAGET/BANKGET command The returned value consists of left-aligned characters indicating the acquired value and a delimiter. Example: The returned value is -30 mm. - 3 0 ...
- マニュアル
...) are available for extending the installation distance between the Sensor and the Controller. Digital equalizer ZG-XEQ Cable for Sensor : 0.5 m (2 m) (flexible cable) ZG User’s Manual Digital equalizer ZG-XEQ Extension cable ZG-XC__...
- マニュアル
...The following values can be output when expressions are set. Item Description Message Judgment result The judgment result is output. (0:OK, -1:NG, -2: not measured) Judge (JG) Correlation The degree of match between the measurement image and model Correlation (...