全 50426 件が検索されました。(2321 - 2340件を表示)

  • マニュアル

    ...The default value for both and is 10. The AUTO Command can be canceled by entering CTRL+C. If an already existing line number is specified, an asterisk (*) is displayed immediately after the line number. If a new line number is input followed by a ...

  • マニュアル

    ...thesamemeaning. Anerrorinthewayinwhichaprogramiswritten.Syntaxerrorscaninclude `spelling'mistakes(i.e.,afunctioncodethatdoesnotexist),mistakesinspecifyingoperandswithinacceptableparameters(e.g.,specifyingread-onlybitsa$a destination),andmistakesinactualapPlicatjonofinstructions{e.9.,acalltoa subroutinethatdoesnotexist). ThearrangementinwhichUnitsinaSystemareconnected.Thistermrefersto theconceptualarrangementandwiringtogetherofallthedevicesneededto comprisetheSystem.InOMRONterminology,systemconfigurationisusedto describethearrangementandconnectionoftheUnitscomprisingaControlSys・ temthatincludesoneormorePCs, Anerrorgeneratedbythesystem,asopposedtooneresultingfromexecutionof aninstruCtiOndeSignedtogenerateanerrOr. Anerrormessagegeneratedbythesystem,asopposedtooneresultingfrom executionotaninstructiondeSignedtogenerateameSSage. Thecodecomprisinganasteriskandacarriagereturn(★...

  • マニュアル

    ... or more times per minute. Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes Power supply Inductive load ...

  • マニュアル

    ... one resulting from execution of an instruction designed to generate a message. terminal instruction An instruction placed on the right side of a ladder diagram that uses the final execution conditions of an instruction line. terminator The code comprising an asterisk and a carriage return (* ...

  • マニュアル

    ...(Find)Key.Thefunctionkeymenuatthebottomofthe screenwillchange,andamessageandaninputareawillapPear・ 17 ---------------------[End of Page 8827]--------------------- ChangingSFCSettings Secti◎n2・3 d)Enterthestep,transition,oractionnumberofthesheettofindandpress theEnterKey.Whenthesheetisfound,thesheetnumberwillappearin theinputarea.Atableofsheetnumberswillbedisplayedifmorethan onesheetisfound.Selectthesheetnumbertobetransferredfromthe tabIe. 3.Programtransferw川startwhentheEnterKeyispressed.Amessagewiil flashduringprogramtransfer.Theamountoftheprogramtransferredwillbe displayedasapercentage. PresstheEscKeytocanceltheprogramtransfer. ...

  • マニュアル

    ...CRindicatestheEnterKey. SFCpart Keysequence Comments Name SymboI Step F6sfθρnμ〃めθrCRor〃0ηamθCR StepnumbersCV500:0to511CVIOOO:Oto1023Thel/Onamemaybei叩utinsteadofthθstepnumber.DonotpresstheF6Key肖thgレOnameisi叩ut. 1 1 Transition 十 1buseatransitionnumber=F5佐…η5従わ刀no....

  • マニュアル

    ...-seriesPCprovideseparateareasfortimersandcounterssothattimer/ counternumbersareeasiertohandleLtisthuspossib│etoassignbothTOO1 (timer1)andCOOI(counter1). WhenSFCprogramminglsused,theFistScanFlagwillbeONduringthefirst executionofeachactbnprogram,ratherthaniirstexecutionoftheentireprogramasitistorC-seriesPCs. AlthoughtimersarealwaysresetformodechangeswithC-seriesPCs,thepresentvalueottimerscanbemaintainedformodechangeswiththeCV-seriesPCs byturningONtheIOMHoldBit. lDatalLnks SYSMACNETLinkSystemsThedataIinkareasforCV-seriesPCsmustallbecontinuous.Gapsbetween datalinkareasarenotallowedastheywereforC-seriesPCs. SYSMACUNKSystems ThedatalinkareasforbothC-seriesandCV-seriesPCsmustallbecontinuous, ThedatalinkareascanbeinanyorderanddonotnecessarilyhavetobeiRorder ofthenodeaddresses. 3 ---------------------[End of Page 9333]--------------------- ...

  • マニュアル

    ... execution of an instruction designed to generate an error. system error message An error message generated by the system, as opposed to one resulting from execution of an instruction designed to generate a message. terminator The code comprising an asterisk and a carriage return (* ...

  • マニュアル

    ...CVM1/CV-series Host Links The following C-mode commands are supported only by built-in Host Links for CPU Unit of version 2 (-V2) or later and cannot be used on other CVM1/CV-series Host Links. RL/WR: RH:WH: ...

  • マニュアル

    ... the baud rate, E is for even parity, 8 is the data length, 1 is the number of stop bits, N controls XON/XOFF flow control, RS controls the RTS signal, CS10 monitors transmissions, DS0 controls the handling of the DSR signal, and LF enables the LF-after-...

  • マニュアル

    ...-line-no.The start・〃nθ・no.andendlineno,canbelinenumbersthatdonotexist. lfonlystart-//ne-no.isspecified,onlythatlineisdisplayed. lfthestart-tine-no,issρecifiedfoliowedbyahyphen(一),theprogramlines aredisplayedstartingfromthespecifiedline. lfena「-tinθ−no.isspecifiedprecededbyahyphen(一),theprogramlinesare displayedstartingfromthefirstlinetothespecifiedline. lfboththestart・〃ηθ−no.andendIineno.areomitted,alltheprogramlines aredisplayed. TheLLエsTcommandoutputstheprogramline(s)totheprinterinsteadofthe display....

  • マニュアル

    ... execution of an instruction designed to generate an error. system error message An error message generated by the system, as opposed to one resulting from execution of an instruction designed to generate a message. terminator The code comprising an asterisk and a carriage return (* ...

  • マニュアル

    ....Thistermrefersto theconceptualarrangementandwiringtogetherofallthedevicesneededto comprisetheSystem.lnOMRONterminology,systemconfigurationisusedto describethearrangementandconnectioRoftheUnitscomprisingaControlSys' temthatincludesoneormorePCs, SystemDM AdedicatedportionoftheDMareathatisusedforspecialpurposesincontro1lingandmanagingthePC.1ncludestheProgramVersion,ParameterArea,ParameterBackupArea,UserProgramHeader,andErrorしogArea. systemerror Anerrorgeneratedbythesystem,asopposedtooneresultingfr◎mexecutionof aninstructiondesignedtogenerateanerr◎r・ SyStemerrOrmeSSage Anerrormessagegeneratedbythesystem,asopposedtooneresultingfrom executionofaninstructiondesignedtogenerateamessage・ terminaginst『ucti◎n AninstructionplacedontherightsideofaIadderdiagramthatusesthefinalexecutionconditionsofaninstructionline. te『minat◎r Thecodecornprisinganasteriskandacarriagereturn("...

  • マニュアル

    ...8 BS CAN ( 8 1001 9 HT EM ) 9 1010 A LF SUB * 1011 B VT ESC 1100 C FF FS 1101 D CR 1110 E S0 1111 F S1 1011 B 1100 C 1101 1110 D 1111 E F 0 @ P ` p ! 1 A Q a q " 2 B R b r s # 3 C S c s t $ 4 D T d t e u % 5 E U e u V f v & 6 F V f v W g w ' 7 G W g w H X h x ( 8 H X h x I Y i...

  • マニュアル

    ... for heat to build up. All inputs can thus be turned ON simultaneously for testing, provided that all inputs have been OFF for at least 2 hours. 151 Appendix B Specifications Analog Timer Unit (C200H-TM001) Item Specifications Oscillation Method ...

  • マニュアル

    ...). Use a surgeabsorbing diode with a voltage resistance of at least five times the circuit voltage. DC Relay DC RY AC Relay Surge-absorbing diode AC Solenoid, etc. SOL 10 Surge absorber (Example: Okaya Electric's ...

  • マニュアル

    ..., insert the surge protector in parallel with the load. If the supply voltage is 100 to 200 V, insert the surge protector between the contacts. Yes Inductive load Diode method Power supply Yes Inductive load ...

  • マニュアル

    ..., delimiter/terminator, etc. If the data is not received normally, however, any of these parts may be missing or corrupted. Be sure to allow for the possibility of missing or corrupted data when receiving data at the host. 2. In this example, the code for ...

  • マニュアル

    ... as shown below. Circuit Current Power supply Inductive load Varistor method Power supply No Yes Yes Yes Inductive load Diode method Power supply DC Yes Inductive load CR method AC Yes Characteristic Required element If the load is a relay or solenoid, there is a time lag between the moment the circuit is opened and the moment the load is reset. If the supply voltage is 24 or 48 V, insert the surge protector in parallel with the load. If the supply voltage is 100 to 200 V, insert the surge protector between the contacts. The capacitance of the ...

  • マニュアル

    ... be installed right next to relays and solenoids. Use surge-absorbing diodes with a dielectric strength of at least five times the circuit voltage. DC Relay AC Relay Surge-absorbing diode (Example: ERB44-06, by Fuji Electric) Surge absorber (Example: ...