全 50426 件が検索されました。(2381 - 2400件を表示)

  • マニュアル

    ...LF SUB * : J Z j z 1011 B VT ESC + ; K [ k { 1100 C FF FS , < L \ l | 1101 D CR GS Ć = M ] m } 1110 E S0 RS . > N ^ n ~ 1111 F S1 US / ? O _ o 63 Revision History A manual revision code appears as a suffix to the catalog number on the front cover of the manual. Cat. No. Z043–E1–01A Revision code The following table outlines the changes made to the manual during each revision. Revision code Date 1 June 1990 01A December 2004 Revised content Original production Warranty and liability information added to beginning of ...

  • マニュアル

    ... THEN FCSD$=”0”+FCSD$ . .......... FCS computed by software 1110 IF FCSD$<>FCSP$ THEN FCSCK$=”ERR” 1120 PRINT ”FCSD$=”FCSD$, ”FCSP$=”FCSP$, ”FCSCK$=”FCSCK$: . ... OK for correct FCS ERR for in correct FCS 1130 RETURN Note In this example, ...

  • マニュアル

    ... Terminal, specify the parameters shown below. The communications specifications of the Visual Controller 3Z4SP-C23 are to match those of the Keyboard Terminal prior to shipment. Baud rate 9600 bps Data length 8 bits Parity bit None Stop bit 2 bits Delimiter ...

  • マニュアル

    ... RS–232C port. Format PRINT# [...] Example PRINT# ”OMRON” Description Specifies a variable name or character string to be output to the RS–232C port. Format is written the same as in the PRINT command. Outputs data with the delimiter (...

  • マニュアル

    ...8 9 10 11 12 13 14 15 0 0 0 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0 0 1 0 1 0 1 2 DLE SPACE ! DC1 ” DC2 DC3 # $ DC4 NAK % & SYN , ETB ( CAN ) EM SUB * + ESC , FS – GS ⋅ RS / US 0 1 1 1 0 0 1 0 1 1 1 0 1 1 1 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 4 @ A B C D E F G H I J K L M N O 5 P Q R S...

  • マニュアル

    ...8 9 A B C D E F 0 0 0 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0 0 1 0 1 0 1 2 SPACE DLE DC1 ! DC2 ” DC3 # DC4 $ NAK % SYN & ETB , CAN ( EM ) SUB * ESC + FS , GS – ⋅ RS US / 0 1 1 1 0 0 1 0 1 1 1 0 1 1 1 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 4 @ A B C D E F G H I J K L M N O 5 P Q R S...

  • マニュアル

    ... Processing start address – Number of bytes to be processed (for read command), write data (for write command) Response Result of processing – End code – Read data (for read command) Indicates end of command or response. Note: ∗ indicates “2A”H of ASCII code, and ...

  • マニュアル

    ... address – Number of bytes to be processed (for read command), write data (for write command) Response Result of processing – End code – Read data (for read command) Terminator Indicates end of command or response. Note: ∗ indicates “2A”H of ASCII code, and ...

  • マニュアル

    ...P. Parity Sets the parity bit. None: No parity setting Even: Even parity setting Odd: Odd parity setting S. Stop bits Selects whether one or two stop bits are to be used. D. Delimiter Sets the delimiter. ...

  • マニュアル

    ... the delimiters used with OVL Versions 1.jj and 2.00. Relevant files are data files and programs transferred via RS-232C or between the CPU and a Memory Card. File I/O Delimiters used Version 2.00 Version 1.jj Input ...

  • マニュアル

    ...will be created under that filename and the data will be stored in that file. (The extension “.DAT” will be added automatically to the filename.) The data will be output in order, beginning with the lowest output number. Outputting Judgement Results Only O , ...

  • マニュアル

    ... / time B. Baud rate : status 1200 2400 4800 9600 19200 S. System L. Data length : 7 bit 8 bit P. Parity bit : None Even Odd S. Stop bit : 1 bit 2bit D. Delimiter : CR LF CR+LF F. Flow : None Xon / off RS / CS : [ 0 ] 100 ms T. Time-out Dialog box Used for setting data. E.End Comment line Shows procedure, etc. Save system data to memory card. X.Execute 38 C.Cancel Message box Displays confirmation messages or error messages. Menu Operations 4-3 Section 4-3 Menu Operations 4-3-1 Selecting Menus F350 menus are ...

  • マニュアル

    ...can subsequently be used as a shortcut for entering that character string. The following character strings are the default settings. F1 F2 F3 F4 F5 F6 F7 F8 F9 F10 10 AUTO LIST RUN CR CAMERA FILTERIN DISPLAY SMDATA RMDATA SQSET SMRUN Basic Operations Control Key Section 2-3 Combining the Control Key with other keys makes possible the operations shown in the following table. They can be used for creating and editing programs. Key Operation CTRL+A Performs the same function as HELP. It displays the last correctly input line and also displays the command and location when an...

  • マニュアル

    ... specified data is decremented from the overwrite count control area, and whether or not the data has exceeded the limits will be determined. Command Format M D S I X X X X X X ∗ CR Specify the decrement count in hexadecimal code. (00H, 01H, 02H,,..., FBH) Area start address specification range (jjj0H to jjj5H or jjj8H to jjjDH) Response Format M D 7 5 ∗ ...

  • マニュアル

    ...-a-day check when creating the system program. 2. Access for checking whether the battery is low is only enabled when the two bytes of data from address 0000H to 0001H are read. Use one of the following commands to check the battery status. (The ...

  • マニュアル

    ... settings. The default communications settings are as shown in the following table. These settings can normally be used. Item Setting Baud rate 38,400 bps Data length 8 (bits) Parity None Stop bits 1 (bit) Delimiter ...

  • マニュアル

    ... X Measured X coordinate Search Y Measured Y coordinate Reference RX Reference X coordinate Reference RY Reference Y coordinate Displacement DX Measured X coordinate – reference X coordinate Displacement DY Measured Y coordinate – reference Y coordinate Correlation ...

  • マニュアル

    ... position: RX X coordinate of registered model position Reference position: RY Y coordinate of registered model position Displacement: DX Difference between X coordinates for measurement and reference values Displacement: DY Difference between Y coordinates for measurement and reference values Correlation: ...

  • マニュアル

    ...Section 4-5 Connection Examples Communication Settings • V530-R150 → p. 140 Item Setting Baud rate 19200 bps Data length 8 bit Parity bits EVEN Stop bits 2 bit Header None Footer CR Mode Normal • Programmable Controller: Turn OFF the DIP switch of CQM1. Set DM6645 to [1001], DM6646 to [0904], DM6648 to [1000] and DM6649 to [0D00]. Match communication settings with the V530-R150. Refer to the operation manual for CQM1 for the ways to change the setting. Program Examples This is an example of a program in which a Programmable Controller (CQM1) receives the data which is read at ...

  • マニュアル

    ...Section 4-5 Connection Examples Communication Settings • V530-R150 → p. 161 Item Setting Baud rate 19200 bps Data length 8 bit Parity bits EVEN Stop bits 2 bit Header None Footer CR Mode Normal • Programmable Controller: Turn OFF the DIP switch of CQM1. Set DM6645 to [1001], DM6646 to [0904], DM6648 to [1000] and DM6649 to [0D00]. Match communication settings with the V530-R150. Refer to the operation manual for CQM1 for the ways to change the setting. Program Examples This is an example of a program in which a Programmable Controller (CQM1) receives the data which is read at ...