全 50426 件が検索されました。(2441 - 2460件を表示)
- マニュアル
... USB interface. Synchronization method Start-stop Transmission code ASCII (Binary format can be selected only when outputting measurement values set at [Setup] - [Support] - [Calculation] - [Data].) Communication speed USB2.0-compliant Data length - Parity - Stop bit - Delimiter ...
- マニュアル
.... Section 4 Creating Setting Files Using the 2DCR Configear ■ Open 9,600*, 19,200, or 38,400 None*, odd, or even * 77 bits or 8 bits 1sbit* or 2 bits None*, 02
, or 1B * ETX, 0A LF, 0D CR , or 0D0A ... - マニュアル
...-RX40_UM_E.book 70 ページ 2009年12月11日 金曜日 午前10時58分 (5) Interface settings This menu is used to specify conditions for PC connection. Settings Selections available New Line code CR...
- マニュアル
... the data retention time *1. High temperatures are those exceeding 125°C up to 250°C. • Resetting the data retention time
1.Reading data from the RF tag addresses 0010Hex to 0015Hex. Command : RDSTH100100006*[... - マニュアル
...The following values can be output when expressions are set. Item Description Message Judgment result The judgment result is output. (0:OK, -1:NG, -2: not measured) Judge (JG) Correlation The degree of match between the measurement image and model Correlation (...
- マニュアル
... USB interface. Synchronization method Start-stop Transmission code ASCII (Binary format can be selected only when outputting measurement values set at [Setup] - [Support] - [Calculation] - [Data].) Communication speed USB2.0-compliant Data length - Parity - Stop bit - Delimiter ...
- マニュアル
...Setting content Command 9600 bps (Factory default setting) Data length 8 bits (Factory default setting) Parity None (Factory default setting) Stop bit 1 bit (Factory default setting) Header None (Factory default setting) Footer ...
- マニュアル
... switches with ENTER key. 3 Selections available USB ID 0 to 9 IP Address 0 to 255. 0 to 255. 0 to 255. 0 to 255 Detailed Settings New Line Code SETTINGS AND MEASUREMENT Setting CR+LF, LF, CR USB ID 0 to 9 IP Address 0 to 255. 0 to 255. 0 to 255. 0 to 255 Subnet Mask 0 to 255. 0 to 255. 0 to 255. 0 to 255 Port Number 1024 to 65535 Gateway 0 to 255. 0 to 255. 0 to 255. 0 to 255 DNS Address 0 to 255. 0 to 255. 0 ...
- マニュアル
...[8] [OFF] Odd Even Adjust to the PC communication specifications. [1 ] 2 Xon/Xoff Flow control is performed with software. Data is sent according to the Xon/Xoff codes from external devices. ● ● ● Timeout [s] [...
- マニュアル
.... 1. 50 In the "Model parameter" area, select the search mode, then specify a value for each item for Search FZ3 Processing Items List Manual that mode. 2 Set value [factory default] Measurement Setting item Description [...
- マニュアル
...X Position X This is the X coordinate of the position −99999.9999 to 99999.9999 where the model was found. Y Position Y This is the Y coordinate of the position −99999.9999 to 99999.9999 where the model was found. ...
- マニュアル
..., they can be called up easily by simply switching the user. ZR-RX45 User’s Manual Setting Menus 95 (5) Interface settings This menu is used to specify conditions for PC connection. Setting Selections available Selections available New Line code ...
- マニュアル
...2: No judgement (not measured), 0: Judgement is OK, −1: Judgement is NG, −13: Teaching not performed error, −14: Figure not registered error, −15: Out of range error C Count This is the number of models found. 0 to 32 ...
- マニュアル
... mode 0 rotation With rotation 0 endAngle Upper limit of the rotation angle 180 startAngle Lower limit of the rotation angle -180 angleSkip Skipping angle 5 smartMode Smart mode 1 stability Stab.(CR) 12 accuracy Prec. 2 searchSpeed Stab.(SH) 3 referencePosX Reference X 0 referencePosY Reference Y 0 detectionPosX Detection point X 0 detectionPosY Detection point Y 0 subPixel Sub-pixel 0 candidateLevel Candidate Point Level 70 upperX Upper limit of measure X 99999.9999 lowerX Lower limit of measure X -99999.9999 upperY Upper limit of measure Y 99999.9999 lowerY Lower limit of measure Y -99999....
- マニュアル
.... 1. In the "Model parameter" area, select the search mode, then specify a value for each item for FZ4 Processing Items List Manual Search 59 that mode. 2 Measurement Setting item Set value [factory default] Description [...
- マニュアル
... length Sets the data length. 8 bits (default value), 7 bits Parity Sets the parity bit (error detection sign). None (default value), odd, even Stop bit Sets the stop bit. 1bit (default), 2bit Delimiter Sets the delimiter (data delimiter). ...
- マニュアル
...IP1: 1 to 233 IP2: 0 to 255 IP3: 0 to 255 IP4: 1 to 254 Subnet mask SUB1.SUB2.SUB3.SUB4 SUB1: 0 to 255 SUB2: 0 to 255 SUB3: 0 to 255 SUB4: 0 to 255 Delimiter CR, LF, CR+LF Analog output Voltage/Current output Sensor Head calibration Calibrates the Sensor Head. Refer to User's Manual. Calibrations conducted in an inappropriate environment may lead to failures in measurement. Timing reset Executes a timing reset. System information This provides four types of system information. Controller version Displays the version of the controller. Controller MAC address Displays the ...
- マニュアル
... as shown in the following table.Use the default settings under normal circumstances. Setting communication specifications p.195 Item Setting value Baud rate 38400 (bps) Data length 8 (bit) Parity None Stop bits 1 (bit) Delimiter ...
- マニュアル
... length Sets the data length. 8 bits (default value), 7 bits Parity Sets the parity bit (error detection sign). None (default value), odd, even Stop bit Sets the stop bit. 1bit (default), 2bit Delimiter Sets the delimiter (data delimiter). ...
- マニュアル
...f g h i j k l m n o Code A NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI Code B ` a b c d e f g h i j k l m n o Input p q r s t u v w x y z { | } ~ @D Code A DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US Code B p q r s t u v w x y z { | } ~ DEL Fiber Laser Marker MX-Z2000G series User’s Manual 2 - ...