全 50426 件が検索されました。(2401 - 2420件を表示)
- マニュアル
...Search X Measured X coordinate Search Y Measured Y coordinate Reference RX Reference X coordinate Reference RY Reference Y coordinate Displacement DX Measured X coordinate – reference X coordinate Displacement DY Measured Y coordinate – reference Y coordinate Correlation ...
- マニュアル
... communications System settings Camera settings Communications Serial Output Normal Display Host link OperationParallel settings Measurement control Switch menu Startup mode ↑↓ The Communications (Normal) window will be displayed. Communications(Normal) Flow control : None Delimiter : ...
- マニュアル
...Density deviation DV Density deviation within the measurement region Classification Measurement item Meaning Judge JG Judgement result Search position X X coordinate of position where model found Search position Y Y coordinate of position where model found Correlation ...
- マニュアル
.... This is a code to detect an error in data string. This expresses a calculation value of horizontal parity of character string between immediately after SOH and immediately before FCS in two ASCII characters. Terminator Shows the end of command with two characters, "*" ($2A) and ...
- マニュアル
... of data for a Tag is transmitted directly as ASCII or JIS 8-bit code. One transmitted character is equal to a 1 byte of data in the Tag. Character data can be read/written directly. Do not use any control codes, such as [SOH] or [...
- マニュアル
... default is “none.” • None • STX • ESC FCS Any of the following can be selected from the Console. The default is “OFF.” • OFF • ON Footer Any of the following can be selected from the Console. The default is “...
- マニュアル
... 66 Change Mode @MC page 67 Change Camera Mode @CC page 67 Read Version Information @VR page 68 Read System Data @SR page 68 Write System Data @SW page 70 Read Scene Data @CR page 71 Write Scene Data @CW page 77 Read Light Level Settings @LR page 78 Write Light Level Settings @LW page 79 Section 4-3 Trigger Inputs and Output Format 1:N (Multi-drop) Connections Function Command Page One Shot Reading @GL page 80 Polling @RD page 80 QR Code Teaching @MQ page 80 Data Matrix Teaching @MD page 81 Read Scene Number @MS page ...
- マニュアル
... cursor to the desired baud rate using the Up and Down Keys. 4. Press the ENT Key. The selections will be registered. System Baud rate : 38400bps 8bit Data Length : : None Parity : 1bit Stop bits : CR Delimiter : None Flow End Scn 0 System Baud rate : 38400bps 8bit Data Length : 2400bps : 4800bps None Parity : 9600bps 1bit Stop bits : 19200bps ...
- マニュアル
... control Setting 38400 (bps) 8 (bit) None 1 (bit) None (Xmodem protocol is used.) Item Baud rate Data length Parity bit Stop bits Delimiter Setting 38400 (bps) 8 (bit) None 1 (bit) CR Scn0 TOOL Check position Scn0 Test Scn1 Record NG Scn2 Backup Scene Z300 toScn3 PC Scn4 System PC to Z300 Scn5 Sys+Scn Scn6 Scn7 Section 3-4 Useful Functions 8. Select Execute. Scn0 TOOL Scn0 The data will be saved. OK? Execute 9. Cancel Select Transfer/Receive File from the Hyper Terminal menu on the computer. •Specify where the file is to be saved. •Set ...
- マニュアル
... computer Input a command. Execute a command. During command execution, the BUSY signal of the parallel I/O interface turns ON. Output reading data. Receive reading data. ‘Communications port OPEN status ‘One shot reading command transmission ‘Loading data (with Footer code ...
- マニュアル
... communications System settings Camera settings Communications Serial Output Normal Display Host link OperationParallel settings Measurement control Switch menu Startup mode ↑↓ The Communications (Normal) window will be displayed. Communications(Normal) Flow control : None Delimiter : ...
- マニュアル
...Density deviation DV Density deviation within the measurement region Classification Measurement item Meaning Judge JG Judgement result Search position X X coordinate of position where model found Search position Y Y coordinate of position where model found Correlation ...
- マニュアル
...Circuit Current AC DC Power supply Inductive load Varistor method Power supply Yes No Yes Yes Yes Inductive load Diode method Power supply Yes Inductive load CR method Characteristic Required element If the load is a relay or solenoid, there is a time lag between the moment the circuit is opened and the moment the load is reset. If the supply voltage is 24 or 48 V, insert the surge protector in parallel with the load. If the supply voltage is 100 to 200 V, insert the surge protector between the contacts. The capacitance of the capacitor must be 1 ...
- マニュアル
... as shown in the following table.Use the default settings under normal circumstances. Setting communication specifications p.194 Item Setting value Baud rate 38400 (bps) Data length 8 (bit) Parity None Stop bits 1 (bit) Delimiter ...
- マニュアル
...i y A LF SUB * : J Z j z B VT ESC + ; K [ k { C FF FS , < L ¥ l | D CR GS - = M ] m } E SO RS . > N ^ n ~ F SI US / ? O _ o DEL Appendix 0 Lower A-5 Appendix Setting list The setting list shows addresses for CompoWay/F communication and Modbus communication. Refer to the addresses of the protocol that you are using. The hexadecimal values in the Setting (monitor) value column are the setting ranges in CompoWay/F and Modbus, and the values in parentheses ( ) are the actual setting ranges. The monitor and setting values can ...
- マニュアル
... the ZEN included is more than 5 times per minute. Countermeasure Examples When switching an inductive load, connect an surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current Power supply Inductive load ...
- マニュアル
... as shown in the following table.Use the default settings under normal circumstances. Setting communication specifications p.196 Item Setting value Baud rate 38400 (bps) Data length 8 (bit) Parity None Stop bits 1 (bit) Delimiter ...
- マニュアル
... user. The MDL command is used exclusively for EEPROM DCs that allow 100,000 overwrite operations. Command Format @ Unit No. M D S/L × × × × × × × × × CR FCS Designate the updated number to be added in hexadecimal code (00H, 01H, 02H, ..., FFH). Start address number specification range (@@@0H to @@@5H or @@@8H to @@@DH) R/W Head number (1 for head 1, 2 for head 2, 3 for head 3, 4 for head 4) Mode specification S: Subtraction Set the number of overwriting operations (16,700,000 max.) Note: The number of ...
- マニュアル
... completed. Command processing abort and reset commands, however, can always be received. 36 Electromagnetic Inductive RFID System User's Manual SECTION 4 Commands Command Response Format Command Frames Data Command code Terminator * 2 n ...
- マニュアル
... to 255 OUTPUT TIME 0 0 to 255 p.69 p.68 THROUGH - - p.65 FREEZE - - p.65 I/O MON - - p.70 MODE COMPOWAY COMPOWAY,NORMAL DELMIT CR CR, LF, CR+LF p.66 p.66 ALL CLEAR - - MEAS CLEAR - - VERSION - - p.64 p.64 p.65 TRIG(*4) HEAD(*4) LINK I/O, LINK p.71 USE USE, NOT USE OUTPUT(*5) EACH ALL, EACH p.72 p.72 p.67 p.68 (*3)This menu is displayed only when Amplifier Units are gang-mounted. (*4)This setting does not display for the host device (the Amplifier ...