全 50426 件が検索されました。(2281 - 2300件を表示)
- マニュアル
... is additionally displayed in the "(1) Content" textbox with a display code based on the following control code table. Control code NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI Display code %x00% %x01% %x02% %x03% %x04% %x05% %x06% %x07% %x08% %x09% %x0A% %x0B% %x0C% %x0D% %x0E% %x0F% Control code DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US DEL Display code %x10% %x11% %x12% %x13% %x14% %x15% %x16% %x17% %x18% %x19% %x1A% %x1B% %x1C% %x1D% %x1E% %x1F% %x7F% Additional Information For Data Matrix, "05 ...
- マニュアル
...に従い、表示コードで追加表示されます。 制御コード NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 2 - 40 表示コード %x00% %x01% %x02% %x03% %x04% %x05% %x06% %x07% %x08% %x09% %x0A% %x0B% %x0C% %x0D% %x0E% %x0F% 制御コード DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US DEL 表示コード %x10% %x11% %x12% %x13% %x14% %x15% %x16% %x17% %x18% %x19% %x1A% %x1B% %...
- マニュアル
...f g h i j k l m n o Code A NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI Code B ` a b c d e f g h i j k l m n o 入力 p q r s t u v w x y z { | } ~ @D Code A DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US Code B p q r s t u v w x y z { | } ~ DEL ファイバレーザマー...
- マニュアル
...f g h i j k l m n o Code A NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI Code B ` a b c d e f g h i j k l m n o 入力 p q r s t u v w x y z { | } ~ @D Code A DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US Code B p q r s t u v w x y z { | } ~ DEL ファイバレーザマー...
- マニュアル
...ーズマニュアル (5)I/F設定パソコンと接続するための条件設定を行います。 設定項目 選択内容 行末文字 CR+LF・LF・CR 0∼9 TCP-IP設定 IPアドレス自動取得 使用しない・使用する IPアドレス 0∼255.0∼255.0∼255.0∼255(IPアドレス自動取得を使用しな...
- マニュアル
...・str拍gmemorytablgaddress NurneraRablgaddress NT20M,NT2000M 000toO31(3<▲igitBCD) 000to127(3・dig柁BCD) NT600M 000to255{3・digitBCD) 000to255(3巳digitBCD} DescriptionCopiesthecontentsofthecopysourcememorytabletothecopydestination memorytabie.Thememorytablecontentsarecopiedtoamemorytableofthe sametype=character-stringmemorytabletocharacter-stringmemorytabieor numeraltabletonumeraltable. 5・1・7LampandTouchSwitchDispSay(BitSpecificati◎n), Format {ESCIKmOsmO2mllm12m2im22m3fm32【...
- マニュアル
... NT20S. The NT20S returns the number of the displayed screen using the Screen Number Response Command (refer to 6-2 Screen Number Response). Memory Tables Section 6-3 Screen Number Response Format [ESC] Y m1 m2 m3 [...
- マニュアル
... are described below. Lamp and Touch Switch Display (Bit Specification) Format [ESC] K m01 m02 m11 m12 m21 m22 m31 m32 1B 4B * * * * * * * * * * * * * * * * m131 m132 [CR] * * * * 0D m41 m42 * * * * ... m0,…m13: Specification of lamps and touch switches (2-digit hexadecimal) The relationship between the lamp and touch switch number and an expression of m0 to m13 in bits is given in the following table. mx1 Bit mx2 7 6 5 4 3 2 1 0 m0 07 06 05 04 03 02 01 00 m1 15 14 13 12 11 10 09 08 m2 23 22 21 20 19...
- マニュアル
....). The following ten-keys (system keys) can be assigned to the input terminals. Ten-keys 1 2 3 4 5 6 7 8 9 0 A B C D E F CR . HOME ¯ ¬ ® MENU Reference: When a screen switchover key for each screen is also assigned to the same input terminal, it acts as the screen switchover key. S Screen switchover function With the screen number assigned to the input terminal, it can function as the screen switchover key similar to the touch switch. However, with “0” specified to the screen number, it functions as the screen switchover ...
- マニュアル
... explanations in this section, parameters are denoted in lower case characters. When specifying a command, write those parts denoted in upper case without modification, and write the numeric values for parameters (BCD or hexadecimal) as ASCII character strings. Parts in square brackets, such as [ESC] and [...
- マニュアル
... PT memory that can be written to by the host. ID [ENO] 05 30 [ESC] 30 1B W Address 57 Write data D11 D12 D13 D14 Dn1 Dn2 Dn3 Dn4 [CR] 0D ID : ”00” (30 Hex, 30 Hex) fixed W : ”W” (57 Hex) fixed This indicates the write mode. 225 Section 5-2 Outline of Communications Address : Address of PT memory at write destination (4 BCD digits) Note, however, that the first word of addresses used only by lamps is ”A” (41 Hex). D11, D12, D13, D14 to Dn1, Dn2, Dn3, Dn4: Write data (4 hexadecimal digits) n words...
- マニュアル
... display Temp. Alarm 11:01 Screen 1 7 8 9 4 5 6 Menu Touch switch SV PV Fixed display-text Graph display String Display Data input (numeral input) 1 2 3 SP 0 CR Numeral display 3 What Is Support Tool? Section 1-1 Product Configuration The NT-series Support Tool for Windows (Ver. 4.) consists of the following software and data. Support Tool Specifications Model number NT-ZJCAT1-EV4 For IBM PC/AT or compatible, media: CD-ROM Keyboard tenkey library Color pallette symbols (Library of parts for filling with color models) System Installer (to replace PT ...
- マニュアル
...case characters. When specifying a command, write those parts denoted in upper case without modification, for those parts denoted in lower case, write the numeric values (BCD or hexadecimal) or character string for parameters as ASCII character strings. Parts in square brackets, such as [ESC] and [...
- マニュアル
... values from testing, and take into consideration that the capacitance suppresses spark discharge when the contacts are separated and the resistance limits the current that flows into the load when the circuit is closed again. DC Yes Inductive load ...
- マニュアル
...case characters. When specifying a command, write those parts denoted in upper case without modification, for those parts denoted in lower case, write the numeric values (BCD or hexadecimal) or character string for parameters as ASCII character strings. Parts in square brackets, such as [ESC] and [...
- マニュアル
...DNV Norway Det Norske Veritas RINA Italy Registro Italiano Navale BV France Bureau Veritas GL Germany Germanischer Lloyd ABS USA American Bureau of Shipping KR South Korea Korean Register of Shipping CR...
- マニュアル
...XW2Z-S002 Omron product Cable length 2m, 9 pin⇔9 pin 39 3-3 Communications procedures 3-3-1 Memory Link Commands Command/response formats are as mentioned below. • Read/write/change notify command ESC • *D SUM ...
- マニュアル
... given in uppercase letters as is and replace lowercase letters with ASCII text strings to specify the numeric values of the parameters (BCD or hexadecimal) or the text strings for parameters. Any text given in square brackets [ ], however, represents one control code, such as ESC or ...
- マニュアル
...Stop bit: Set the same as for the communication setting's Stop Bits of the PT. Transmission speed: Set the same as for the communication setting's Comm. Speed of the PT. Sumcheck: ON (YES) Transmission control procedure: Form1 (without ...
- マニュアル
... bits Stop bits Parity End code Start code Unit number Modem connection 14 Setting 19,200 bps 8 1 Enabled, odd Setting Computer link 19,200 bps 8 1 Enabled, odd CR No STX 1 No connection Section 2-1 FP-X Series 2-1-1 Connecting to an FP-X-series Tool Port Connection Configuration between PLC and PT Connect the PT to the tool port on the FP-X-series PLC as shown below. Power supply PT Communications Format Setting System register number 410 412 413 414 Item Tool port unit number Modem connection Data length Parity ...