全 53645 件が検索されました。(5821 - 5840件を表示)

  • カタログ

    ...) Type Semiconductor laser Wavelength: 655 nm Laser class Class 2 (JIS C6802 2014) Marking area 90 × 90 mm 160 × 160 mm Working distance 170 ± 10 mm 220 ± 10 mm Scan speed 1 to 12,000 mm/s Marking resolution 2 μm Text 4 μm Type: English alphabet (upper/lower case letters) / numbers / symbols / hiragana / katakana / kanji (JIS level 1, level 2) / other languages (UNICODE (Basic Multilingual Panel)) Printable fonts: • TrueType font • Stroke font (original / original2 / OCR-A /OCR-B / SEMI / LM font) Details of marking Setting Cable Bar code CODE39/NW-7/ITF/CODE128/JAN GS1 Databar ...

  • カタログ

    ...ード*2 150ns∼450ns (3パターン) 半導体レーザ 波長: 655nm クラス2 (JIS C6802 / IEC60825-1) 160×160mm 160×160mm 90×90mm 220±10mm 220±10mm 170±10mm 1∼12,000mm/s 4μm 4μm 2μm 英大小文字 / 数字 / 記号 / ひらがな / カタカナ / 漢字 (JIS第1、 第2水準) /その他言語 (UNICODE (基本多言語面) ) オリジナル / オリジナル2 / OCR-A / OCR-B / SEMI / LMフォ...

  • カタログ

    ...Orientation Now Inspection, reading the 2D code Marking Positioning Cost and labor for the design, implementation and execution were high. Before All processes are consolidated in one single step. Design, implementation, and execution are greatly simplified. Now Camera(...

  • カタログ

    ...用 カメラアタッチメント形MX-9150 ❶位置補正・2次元コード読み取り・文字検査・各種検査デジタルCCDカメラ形FZ-SC/FZ-S 30万画素 カラー/モノクロ 画像処理システム形FH-L551 形FH-2052 形FH-5052 形FH-5552 MX-Z2050H用 MX-Z2055H用 カメラアタッチメント形MX-9151 レ...

  • カタログ

    ...Digital setting: 0.01 Hz, Analog setting: Maximum frequency × 1/1000 Voltage/Frequency characteristics V/f characteristics (constant torque, reduced torque) Sensorless vector control, V/f control with speed feedback Overload current rating of inverter Normal-load rating (ND): 150%/60 ...

  • カタログ

    ... for your applications. The size of the Check Box, Slider, and Radio Button objects can also be changed. You can greatly improve the usability of your machine by enlarging these objects in size. ■Custom keypads ■Resizing object Changing the keypad size Creating user'...

  • カタログ

    .../IPTM is the trademarks of ODVA. Other company names and product names in this document are the trademarks or registered trademarks of their respective companies. The product photographs and figures that are used in this catalog may vary somewhat from the actual products. Microsoft product screen shot(...

  • カタログ

    ... OFF for only a short time for a hot-start, the capacitor will not sufficiently discharge and the inrush current given in the table may be exceeded by up to twice the given value. An inrush current of approximately 4 A may occur and continue for 1 ...

  • カタログ

    ...SD memory card, 2GB HMC-SD292 SDHC memory card, 4GB HMC-SD492 SDHC memory card, 16GB HMC-SD1A2 *1. There are restrictions on the combination of CPU Unit version and memory card. Refer to NJ/NX-series CPU Unit Software User'...

  • カタログ

    ....omron.com Authorized Distributor: Regional Headquarters OMRON EUROPE B.V. Wegalaan 67-69, 2132 JD Hoofddorp The Netherlands Tel: (31) 2356-81-300 Fax: (31) 2356-81-388 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U....

  • カタログ

    ... RRP+R SCARA PRR+R 3-AXES Multi-axis setup and tuning Multi axis tuning wizard Multi - drive window Several 1S servo drives can be tuned simultaneously in a short amount MotorR Adjusting, monitoring Motor1 parameters of the robot’...

  • カタログ

    ...) Database connection: Logs real-time data from production lines directly into SQL Databases. This enables preventive maintenance and quality traceability. One Software One integrated development environment software Fully conforms with IEC 61131-3 standards PLCopen function blocks for motion control Packed with Omron’...

  • カタログ

    ...IT system Easy SCADA/HMI/MES/ERP Simple connection to host system A gateway computer is required to connect a traditional PLC to the host system. The user must register variables, allocate memory to them, and convert complex data. Omron'...

  • カタログ

    ... Series NC Integrated Controller Machine Automation Controller NJ Series Integrated NC and PLC functionality for advanced processing machines 2 Machine Automation Controller NJ Series - NC Integrated Controller NC Integrated Controller brings further of multi-purpose processing machines With changes in consumer’...

  • カタログ

    ...制御軸数 モーション軸最大数 16 *1 CNC軸最大数 16 *1 1系統あたりの同期軸数 4 系統数 4 最小通信周期 500µs ソフトウェア 統合開発環境 Sysmac Studio: • ラダー図、ストラクチャードテキスト(ST)、インラインST • IEC 61131-3規格準拠 • PLCopen®準拠モーション/安全...

  • カタログ

    ...IOG IOG I3+ I4+ IOV IOV IOG IOG Current output + Current output − IOG B8 A8 B8 37 NX-AD/DA Version Information Connected to a CPU Unit Refer to the user's manual for the CPU Unit details on the CPU Units to which NX Units can be connected. NX Unit Model Corresponding unit versions/versions Unit version CPU Unit Sysmac Studio Ver.1.0 Ver.1.13 Ver.1.17 NX-AD@@@@ NX-DA@@@@ Note: Some Units do not have all of the versions given in the above table. If a Unit does not have the specified version, support ...

  • カタログ

    .... The settings that are backed up are saved in memory in the Communications Coupler Unit. The settings that are backed up are not saved in the Communications Interface Units. 7 NX-CIF Version Information Connecting with CPU Units Refer to the user'...

  • カタログ

    ...UDP 123 SNMP agent UDP 161 SNMP trap UDP 162 Remarks Fixed values You can change the port number in the Unit Settings on the Sysmac Studio. NX-CSG Configuration Unit Refer to the user's manuals for information on the NX Units that can be connected to the NX-series Communication Control Unit. Safety Control Units Unit Model Safety CPU Unit NX-SL5500, NX-SL5700 Safety Input Unit NX-SIH400, NX-SID800 Safety Output Unit NX-SOH200, NX-SOD400 I/O Units Model Unit 2-point Units Digital Input Unit −−− Digital Output Unit NX-OC2633 NX-OC2733 Digital Mixed...

  • カタログ

    ...and adjusts the closing time to prevent overfilling or underfilling caused by flow rate fluctuations. Inspection without slowing down conveyor speed or causing false positive During inline inspection, variations in conveyor speed prevent capturing an image so that it fits into the camera’...

  • カタログ

    ...) Model Remarks NX-EC0122 1/1 NX-EC0132 Line receiver input NX-EC0142 NX-EC0212 24-V voltage input 2/2 2 (PNP) NX-EC0222 * Refer to the I/O Refreshing Methods in the USER'S MANUAL (Cat. No. W524) for the communications cycles for each model. Position Interface: SSI Input Units Specification Product name Number of channels SSI Input Unit Input/Output form Maximum data length Encoder power supply Type of external connections Model 1 EIA standard RS-422-A 32 bits 24 VDC, 0.3 A/CH Screwless push-in terminal block (12 terminals) NX-ECS112 2...