全 53645 件が検索されました。(5841 - 5860件を表示)
- カタログ
..._15 Combine flexibility in Remote I/O configuration with the speed and determinism of EtherCAT. • The EtherCAT Coupler Unit is the link between the EtherCAT Machine Control network and the NX-series I/O Units. With I/O Units ranging from basic I/O'...
- カタログ
...NX-ECT101 System Configuration An example of a system configuration for an NX-Series EtherCAT Slave Unit is shown below. The following figure shows an example when an NX-series NX102 CPU Unit is used for the NX-series CPU Unit. Refer to the user’...
- カタログ
....omron.com Authorized Distributor: Regional Headquarters OMRON EUROPE B.V. Wegalaan 67-69, 2132 JD Hoofddorp The Netherlands Tel: (31) 2356-81-300 Fax: (31) 2356-81-388 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U....
- カタログ
... I/O control and safety control can be integrated by connecting Units for safety. • The IP address can be found on the label on the Unit, without using software. • Slave configuration by Sysmac Studio can be done centrally via the controller, or on-the-spot using the Coupler'...
- カタログ
...OK OK OK OK OK --- --- --- --- --- Mail send/receive --- --- --- --- --- --- OK --- --- --- Web functions --- --- --- --- --- --- OK --- --- --- Automatic adjustment of PLC/Controller’s internal clock OK OK OK OK OK --- OK --- OK OK OK *1 OK *1 OK *1 OK *1 OK *1 OK *1 OK OK OK OK Response to PING command OK OK OK OK OK OK OK OK OK OK SNMP/SNMP trap OK OK OK OK OK OK --- --- OK OK CIDR function for IP addresses OK OK OK OK OK OK --- --- OK OK DHCP client --- OK --- --- --- --- --- --- --- --- Online connection via EtherNet/IP using CXOne --- --- --- --- --- --- OK --- OK OK Online connection via EtherNet/IP ...
- カタログ
...NX-series High-speed Analog Input Unit NX-series High-speed Analog Input Unit NX-HAD@@@ CSM_NX-HAD____DS_E_DITA_7_1 Simultaneous sampling of 4 channels with sampling times down to 5 µs • NX-series High-speed Analog Input Unit • Multi-range inputs: Voltage and current • Highest resolution: 1/64,000 NX-HAD@@@ Features • • • • • • • Continuously samples analog input signals from 4 channels every 5 µ...
- カタログ
... model, NXTC, which has 4 channels per unit. Approx. 40% *1 When using standard control less width NX-HTC 30 mm Save more space by using together with XW2K ultra-compact interface wiring system Save more in-panel space with the industry’...
- カタログ
...が必 要 非接触温度センサによる温 度 制 御や 装置機構の温度モニタリングができます。 非 接 触 温 度 セン サ E S 1- N ・測定温度 - 50 ~ 500 ℃、- 50 ~ 1,000 ℃ ・再現性± 0.5 ℃、応 答 速 度 0.14 秒( 95 %)と高 精 度、高 速 測 定 。 ・専用ソフトウェア 形 ES1-TOOLS( WEB より無 償ダウンロー...
- カタログ
...-circuit Not supported. detection * This model does not support the input filter. If the Unit is susceptible to noise, take countermeasures such as separating or shielding the Unit and signal lines from the noise source. Refer to NX-series Digital I/O Unit User’...
- カタログ
... IO-Link Master Unit and the IO-Link devices. This enables partial troubleshooting for NJ/NX-series Controllers and NY-series Industrial PCs. * This function is supported with the unit version 1.1 or later. Version Information Connecting with CPU Units Refer to the user'...
- カタログ
.../8 ms max. for cold start at room temperature At 200 VAC: 40 A *2/8 ms max. for cold start at room temperature At 24 VDC: 30 A/2 ms max. for cold start at room temperature 7 A *3/3 s max. for cold start at room temperature Output capacity *4 Total: 90 W max. Total: 70 W max. Output terminal (service supply) Not provided. RUN Output Contact configuration: SPST-NO Switch capacity: 250 VAC, 2 A (resistive load) 120 VAC, 0.5 A (inductive load), 24 VDC, 2A (resistive load) Replacement notification function Not provided. Insulation ...
- カタログ
... Units. I/O power supply is also required to drive the built-in I/O output circuit. However, only the supply to the NX Unit is described in this section. For the I/O power supply to the built-in I/O, refer to the hardware user’...
- カタログ
...-Run refreshing • Synchronous I/O refreshing • Task period prioritized refreshing 5 VDC ± 10% -5.0 to 5.0 mV/V Model Load Cell Input Unit NX-RS1201 * Refer to the I/O Refreshing in the NX-series Load Cell Input Unit User’...
- カタログ
.../IP™ is a trademark of ODVA. Other company names and product names in this document are the trademarks or registered trademarks of their respective companies. The product photographs and figures that are used in this catalog may vary somewhat from the actual products. Microsoft product screen shot(...
- カタログ
... required for production system design Automatic Programming Create a truth table using input, output, and stop conditions of safety devices to automatically create a safety program for a simple machine. * Programs created by Automatic Programming will not guarantee functional safety. Refer to the User'...
- カタログ
.../IP™ is a trademark of ODVA. Other company names and product names in this document are the trademarks or registered trademarks of their respective companies. The product photographs and figures that are used in this catalog may vary somewhat from the actual products. Microsoft product screen shot(...
- カタログ
... have been certified for safety standards, refer to your OMRON website. Features • Meets EN ISO 13849-1 (PLe/Category 4) and IEC 61508 (SIL3) • Safety I/O can be freely placed and combined on the NX bus master and mixed with standard I/O • Omron’...
- カタログ
... possible combinations of versions of NX-series Safety Control Units, CPU Units, Communications Coupler Units, and Sysmac Studio. Available functions that are related to safety control vary depending on the versions of the units and Sysmac Studio. Refer to the NX-series Safety Control Unit User'...
- カタログ
... possible combinations of versions of NX-series Safety Control Units, CPU Units, Communication Control Units, and Sysmac Studio. Available functions that are related to safety control vary depending on the versions of the units and Sysmac Studio. Refer to the NX-series Safety Control Unit User'...
- カタログ
...ESI files End Cover NX Units * The connection method for the Sysmac Studio depends on the model of the CPU Unit or Industrial PC. Note: To check whether NX Units can be connected to your CPU Unit or Communications Coupler Unit, refer to the user'...