全 7847 件が検索されました。(5121 - 5140件を表示)
- マニュアル
...・●●■●●■●■●●■●●●●■●●●●●●●◆●●●●●●・● BasicOperatingPrinciples QpPerationa1Flow SystemConfiguration ControlSystemPrinciples SECTION2 BeforeOperation……・…・・……………・…・・ 2-1Nomenclature,Switches,andIndicatOrs 2-2W垣ng 2-3WiringPreca頭ons SECTION3 TrialMotorOperation 3-1 3_2 3・-3 3-4 3-5 3-6 ...
- マニュアル
...HX/HG/HE, C500, C1000H, C2000H WF FM AREA WRITE Not Valid Valid Valid C1000H, C2000H WC TC PV WRITE Not Valid Valid Valid All: C120, C200H/HS/ HX/HG/HE, C500, C1000H, C2000H W# SV CHANGE 1 Not Valid Valid Valid All: C120, C200H/HS/ HX/HG/HE, C500, C1000H, C2000H ...
- マニュアル
...ON execution condition for a WAIT following an AND for the input (i.e., an input for the programmed bit). The time required to service a Master Remote I/O Unit depends on the number of Masters in the system. The time between servicing any one Master, ...
- マニュアル
...-coveringdiameter t3mm d5 Outer・coveringdiameter 3.Omm D1 lnnersheathdiameter 9.5mm D2 Outersheathdiameter(cabledia.) 12.5mm 3 ---------------------[End of Page 7801]--------------------- Plastic tiealFiber《7ableforLTndoor乙Tse(遵]P盛り Section1-4 OpticalConnectorOutsideMeasurements ▼ 5(Sidevi・...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 1-6 Maximum Distance Between ID Sensor Unit and R/W Head . . . . . . . . . . . . . . . . . . . . . . . 9 1-7 Maximum Distance Between ID Sensor Unit and R/...
- マニュアル
... 20521 SURGXFWV PHDQV ´ZRUGµ DQG LV DEEUHYLDWHG ´:Gµ LQ GRFXPHQWDWLRQ 7KH DEEUHYLDWLRQ ´3&µ PHDQV 3URJUDPPDEOH &RQWUROOHU DQG LV QRW XVHG DV DQ DEEUHYLDWLRQ IRU DQ\ WKLQJ HOVH 9LVXDO $LGV 7KH IROORZLQJ KHDGLQJV DSSHDU LQ WKH OHIW FROXPQ RI WKH PDQXDO WR KHOS \RX ORFDWH GLIIHUHQW ...
- マニュアル
...Expansion: The change in the protrusion between the core and ferrule tip compared to the initial value. value Electrical Characteristics Item Specification mm2 Cross sectional area of power supply wire’s conductor 0.75 Maximum conductor resistance 26.1 ...
- マニュアル
...・ ity.BesuretoreadthissectionifthesystemconsistsofmultiplenetWorks. SectionsdescribestheDiagnosticUtility,whichisusedtocheckoperationwhentheSYSMAC NETSystemjsinstalledandtotroubleshootthesystemwhenerrotsoccur. Sθction6describestheprocedureforexecutinglooptests.Refertothissectionwhenexecutingacommunicationstest,suchastheseperformedaftersettingupSYSMACNET communicationsonanIBMPC/ATorcompatiblecomputer. Section7describestheNodeConfigurationUtility,whichperformsvarioussettingsrelatedto NSUs(NetWorkServiceUnits)andlocalbridgesmountedinSYSMACNETSys・ tems.MakesurethatNSUsandlocalbrldgesaresetcorrectlybyreferringtothis sectionwhiiesettingthedevices. Section8describesproceduresforoperatingtheversiondisplayutility,thestatusdisplayutility,andthepacketpartitioningutility. SθctiongdescribesaprogramusedtotestcommunicationswithothernodesusingtheSYSMACNETdatagramservice. PART3:PROGRAMMINGThesecondpartdescribesprogramdevelopmentusingFINScommunica・ tionsanddatagramcommunications,includingprotocoisandinte㎡aces. Sampleprogramsareprovided, Section10describesthedatagramservice.Usethedatagramservicewhencommunicating withnodesthatdonotsupporttheRNSprotocol,suchasC-seriesPCs. △...
- マニュアル
...6:Ch2,12Voutput,ON/OFF 7:Ch2,-12Voutput,ON/OFF 8:Ch2,5Voutput,ON/OFF ThesVoutputcanhandleuptoabout300mAperchannel.The12Vand-12 Voutputgivesatotalofabout100mAperchaRnel.Normally,onlypin4for theframegroundshouldbeshorted,whileothersopen(OFF), ---------------------[End of Page 8248]--------------------- HardwareDescn'ption Secki◎n1 1・7 C◎rmectljn9量heNe量...
- マニュアル
...耐nd・一.f「ash臼whonthgtok飢{8clr側lat{ngal卯glh6100P,Thoinlθn⑲hyoflighldθcroa8981flhθr6}3abOPθr了OL-.. NCDlnd已ator{f6d) 瓢=;!e拍ct撫h6n亀hg眺a͡b叩. BCDild泌ator{16d)一 Bad{boρCarrlerD身tgC書,L口w}ton{hgrθ18abackboρrOC6ρtbn8k抑a1. 3 ● ---------------------[End of Page 8311]--------------------- sstemCot Itrations Sectlon14 Th6followlnOchartdescribeshowtointerprettheNCOandBCDindlcators、 BackPanol ThebackpanetottheLlnθSgrverUnitisusedtoconngcttheOptlcalFibθr CablθsandthePowθrsuPptyTwek}ndsolOptlcal日bθrCablemaybeus8d: 6tandardHC・PCF{hardcor6pla6tioCtadfiber}cable,orAGF{allglasstibec) quartZcrystatCablefOrnetWo「ks拍a1『6qolr③distancθsupte3kmbetWoon repea{etS.Ifuslnglheqva(tZCrystalcab!θ,lheLlnθServerUnitmustb8mo・ diRedbyOMRONtaclorypetsonnel.TitθtollowiRgfigureshowstheback pan6ioteheLineServer, ORX,OYX CoqnectiOfi{or叫」8rtzcry6{ぬl cabiθ・feceivear"」U8ftsmi¶ Sし...
- マニュアル
... form
= TIME$, TIME$ returns an eight character string in the form: hh:mm:ss. If is not a valid string, an error message will be displayed. USR Function Purpose: To call a user-written assembly language program. Format: USR [ ]( )[,... - マニュアル
... used as bypass resistors. If, as in the following example diagram, the load current is 4 mA, then: Output transistor current (7 mA) = Load current (4 mA) + Bypass current (3 mA). The output circuit of the Position Control Unit is provided with 1.6 kΩ (1/2 ...
- マニュアル
... be placed in the same duct at the point of connection to the equipment, be sure to screen them with a grounded metal plate. Metal (iron) plate 200 mm min. 1 2 3 Grounding (at a ground resistance of less than 100 ...
- マニュアル
...(sentences and phrases) 60 max. Message input (switch-selectable) MIC IN Microphone input: unbalanced dynamic microphone (600 Ω) LINE IN Tape input: Input impedance: 50 kΩ, unbalanced; Maximum input voltage: 3.3 V SPEAKER OUT Built-in amplifier output: 0.14 ...
- マニュアル
...Power supply connector 2 Supplies backup power to a SYSMAC LINK Unit. P/S2 L1 100240 VAC Power supply terminals Backup AC power is supplied through these terminals. L2/N LG Ground Connect LG to a separate 100 ...
- マニュアル
... power supplies, the CPU (as well as the Programming Console) will not operate unless power is supplied the I/O Unit. The following illustration shows the proper way to connect a power supply to the PC. Although the power consumption for each Unit is lower than 20 ...
- マニュアル
... commands are set in the DM area as shown below. Refer to Appendix I for the extended ASCII table. DM0000 5 7 5 4 “WT” Write command header DM0001 4 1 3 1 “AI” ASCII code, R/W Head 1 DM0002 3 0 3 0 “00” DM0003 3 0 3 6 “06” DM0004 0 0 0 0 DM0005 2 A 0 0 “* ” DM0200 5 2 4 4 “RD” Read command header DM0201 4 1 3 1 “AI” ASCII code, R/...
- マニュアル
...(destinationnode) ←Firstwordofparameter 33 ---------------------[End of Page 8441]--------------------- RoutinTables Section3-4 Schematically,theprocedureworksasfollows: Program SYSMACC・series ∼ SEND(90) mOO LROI DMOOO {ContentsofMOO} − sySMAcNet − (Resp◎nse) SYSMACC-series 3-3 DataFE◎...
- マニュアル
.... Cutthecabletotherequlredlength. Usearazorbladetocutawaythesheath:25mmforRS-422cable;40 mmforRS-232Ccable. Usescissorstocutawaytheexposedbraiding. Usewirestripperstoremovetheinsulationfromthelast5mmofall Wlres. Wrapinsulatingtapeoverthetopandendofthethecutsheath. 1 25(RS-422)_●40(RS-232C) 1 【 一5-− Electrician's tape Soldering Observethefollowingwhensolderingthepreparedwiresontotheconnectors. 13 ---------------------[End of Page 8497]--------------------- ...
- マニュアル
... form
= TIME$, TIME$ returns an eight character string in the form: hh:mm:ss. If is not a valid string, an error message will be displayed. USR Function Purpose: To call a user-written assembly language program. Format: USR [ ]( )[,...