全 281 件が検索されました。(81 - 100件を表示)

  • マニュアル

    ...据温度单位的设定值显示C或F。 输入类型 0.0 hb1 Segment n Format (Only at Slope Setting) 紧密安装(mm) 前面板的元件名称 ·°C / °F:温度单位 Proportional Band (Cooling) M ct1 连接(端子适用性因机器型号而异。 ) 单独安装(mm)     * 请勿拆下接线板。 否则,会导致故障或误动作。 *调试工具端口配...

  • マニュアル

    ... for a • : Protection indicator 0% output. Lit when Setting Change Protect is ON (disables the • OUT2: Control output 2 indicator • No.1 display Transfer output B(+) E5EC One linear current output Names of Parts on Front Panel • °...

  • マニュアル

    ...* 如果前面板端口盖丢失或损坏,请另行订购。 根据运行环境,防水密封圈可能会劣化、收缩或变硬,因此请定期进行更换。 ·°C / °F:温度单位 供电电压 连接(端子适用性因机器型号而异。 ) 单独安装(mm) + 0.8 0 尺寸(mm) 92 接线 在客户的应用中,欧姆龙不负责...

  • マニュアル

    ... number of units - Waterproofing is impossible with side-by-side installation. When waterproofing is required, fit watertight packing on the backside of front panel. 92 +0.8 0 120 min. 91 96  • °C / °F...

  • マニュアル

    ... mistakenly connected while input type is not set for it. To clear the s.err display, correct the wiring and cycle the power supply. Setting The setting data for the E5EN-HAA2HBF is shown here as an example. Initial Setting Level Input Type • °...

  • マニュアル

    ... connected.) Refer to the instruction manual provided with the USB-Serial Conversion Cable for details on connection methods. • No.1 display • No.2 display Operation indicators Process value or set data type Set point, set data read-out value or changed input value • °...

  • マニュアル

    ...) Scaling Lower Limit (in-l) Decimal Point (dp) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-5-3 °C/°F Selection (d-u) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-5-4 SP Upper Limit (sl-h) SP Lower Limit (sl-l) . . . . . . . . . . . . . . . 7-5-5 PID/OnOff (cntl) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-5-6 Heating Control Period (cp) Cooling Control Period (c-cp). . . . . . 7-5-7 Direct/Reverse Operation (oreU) . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-5-8 Alarm 1 Type (alt1) Alarm 2 Type (alt2) Alarm 3 Type (alt3) . 7-5-9 Control Output 1 Allocation (out1) . . . . . . . . . . . . . . . . . . . . . . . . . 7-5-10 Control Output 2 Allocation (out2) . . . . . . . . . . . . . . . . . . . . . . . . . 7-5-11 Auxiliary Output 1 Allocation (sub1) . . . . . . . . . . . . . . . . . . . . . . . 7-5-12 Auxiliary Output 2 ...

  • マニュアル

    ...X SP X X SP X SP X SP Y 0 * Alarm values 1 to 7: Set the deviation from the SP (set point) in the alarm value (X). Alarm 8: Set the absolute value from 0°C/°F in the alarm value (Y). * The default is 2 (upper-limit alarm). 1-12 Section 2 Preparations 2.1 Installation .............................................................................. 2-2 ■ External Dimensions (Unit: mm) ................................ 2-2 ● E5CSV ................................................................ 2-2 ● E5CS-U............................................................... 2-2 ■ Panel Cutout Dimensions (Unit: mm)......................... 2-2 ● E5CSV and E5CS-U ........................................... 2-2 ■ Mounting.................................................................... 2-3 ● E5CSV ................................................................ 2-3 ● E5CS-U............................................................... 2-3 ● Mounting to the ...

  • マニュアル

    ... hysteresis ON Lower-limit alarm Alarm hysteresis ON OFF OFF Alarm value Alarm value • Alarm hysteresis is set independently for each alarm in the Alarm Hysteresis 1 to Alarm Hysteresis 3 parameters (initial setting level). • The default is 0.2 (°...

  • マニュアル

    ... to display d-u (Temperature Unit). Initial Setting Level d-u c 2 4 d-u c 4-4-1 Temperature Unit * Press the U or D Key to select °C. The default is c (°C). c: °C, f: °F Temperature Unit The temperature unit is not displayed by the E5DC and E5DC-B. E5@C Digital Temperature Controllers User’s Manual (H174) 4-4 Selecting the Temperature Unit • Either °C or °F can be selected as the temperature unit. • Set the temperature unit in the Temperature Unit (d-u) parameter of the Initial Setting Level. The default is ...

  • マニュアル

    ...Press the M Key several times in the Initial Setting Level to display d-u (Temperature Unit). Initial Setting Level d-u c 2 4 - 20 Press the U or D Key to select °C. The default is c (°C). c: °C, f: °F Temperature Unit d-u c E5@C-T Digital Temperature Controllers User’s Manual (H185) 4 Basic Operation Selecting PID Control or ON/OFF Control (Not Supported for Position-proportional Models.) Two control methods are supported: 2-PID control and ON/OFF control. Switching between 2-PID control and ON/OFF control is executed by means ...

  • マニュアル

    ...63% of the SP change width PV Standby time = Integral time (I) Thermac Simulator Operation Manual (H190) Temp. rise time 6 times the temperature rise time 4-1 Phase Changes during Log Data Collection Settling width: SP ±1°...

  • マニュアル

    ...Operating Procedure 1 Press the M Key several times in the Initial Setting Level to display d-u (Temperature Unit). Initial Setting Level d-u c Press the U or D Key to select °C. The default is c (°C). c: °...

  • マニュアル

    ...7-3 Input Function...................................................................................................................... 7-11 7-3-1 7-3-2 7-3-3 7-3-4 7-3-5 7-3-6 7-3-7 7-4 Input Type Settings ................................................................................................................... 7-11 Temperature Unit (°...

  • マニュアル

    ... enabled after the power supply is reset. An example of a case where the instance ID is 01 hex is described below. Data Attribute ID Parameter name Description 64 hex Sensor 1 (0000 to 270F hex) (0 to 999.9 (unit: °...

  • マニュアル

    ...7-8 Input Function...................................................................................................................... 7-11 7-3-1 7-3-2 7-3-3 7-3-4 7-3-5 7-3-6 7-3-7 7-3-8 Input Type Settings ................................................................................................................... 7-11 Temperature Unit (°...

  • マニュアル

    ...1 Press the M Key several times in the Initial Setting Level to display d-u (Temperature Unit). Initial Setting Level d-u c 2 Press the U or D Key to select °C. The default is c (°C). c: °C, f: °F 4 - 14 Temperature Unit d-u c E5D-H Digital Temperature Controllers User’s Manual (H239) 4 Basic Operation 4-5 Two control methods are supported: 2-PID control and ON/OFF control. Switching between 2-PID control and ON/OFF control is executed by means of the PID ON/OFF parameter in the initial ...

  • マニュアル

    ...可能 計測パラメータ表示選択 off、on 表示点灯時間 0∼99 63.dsp 0 電圧誤結線検出 off、on 64.v-e on c、f 65.d-u c -50.0∼50.0 t.ad 0.0 簡易温度設定 温度単位 温度補正値 -w:積算回生電力量、var.d:積算進み無効電力量、 var.g:積算遅れ無効電力量、var.a:...

  • マニュアル

    ... power consumption 61.rtt rtim Measurement parameter display selection off, on 62.d.sl Display lighting time Incorrect voltage wiring detection Simple Temperature unit temperature Temperature correction value setting 0 to 99 off, on ...

  • マニュアル

    ...off、on 09. bz on キー操作のブザー音の有無を設定 64.v-e 65.d-u on c 10.co2 0.387 単位:kg-CO2/kWh off、on c、f 0.000∼99.999 電圧誤結線検出簡易温度 温度単位設定温度補正値 -50.0∼50.0 t.ad 0.0 料金換算設定 0.000∼99.999 11.chg 10.000 (レート設定、料金単位設定)...