全 281 件が検索されました。(181 - 200件を表示)

  • マニュアル

    ...一999∼9999(TC)-99.9∼999.9(Pt> 8 絶対値上限警報 '一●「'L ゴ6℃/芋一999∼9999(TC)-99,9∼999.9(Pt) 9 絶対値下限警報 「'一●■9-'o 亡O▲C/・F 一999∼9999(TC)-99.9∼999.9(Pt) (注)工場出荷時は警報1、2とも上限警報"2"に設定しています。 EsEF-AM 16 (注)X、Yの値を負に設定することによ...

  • マニュアル

    ...100 in-l 0 dp 0 d-u c sl-h 1300 sl-l -200 onof s-hc stnd *6 25 No alarm function Decimal point (only when setting analog input) °C/°F selection °C= c °F= f (C stands for Celsius, F for Fahrenheit) Hold down for at least 3 seconds (No.1display flushes, then the control stops.) *6 *6 Hold down for at least 1 second Set point lower limit In ON/OFF control = onof In 2-PID control = pid *6 *6 Standard control = stnd Heating and cooling control = h-c (Select standard control or heating and cooling ...

  • マニュアル

    ... as 198.8 °C after input shift if the input shift value is set to –1.2 °C. run run When control stop = stop 0 on off 25 Adjustment Level 0 onof pid DO NOT USE • °C / °F : temperature unit The temperature unit is displayed when the displayed value is a temperature. When this parameter is set to “°C”, “C” is displayed, and when set to “°F”, “F” is displayed. This flashes while ST (Self-Tuning) is activated. • : Protection indicator Lit when Setting Change Protect is ON (disables the Up and Down Keys). • MANU: Manual output indicator Lit when ...

  • マニュアル

    ... input shift if the input shift value is set to –1.2 °C. run run When control stop = stop 0 on off - B + Adjustment Level 0 onof pid 25 Transfer output + mA • °C / °F : temperature unit The temperature unit is displayed when the displayed value is a temperature. When this parameter is set to “°C”, “C” is displayed, and when set to “°F”, “F” is displayed. This flashes while ST (Self-Tuning) is activated. • : Protection indicator Lit when Setting Change Protect is ON (disables the Up and Down Keys). • MANU: Manual output indicator Lit when the Auto/Manual Mode ...

  • マニュアル

    ...(℃) 。 /0 to 320( F) 0 to 165(℃) 。 /0 to 500( F) 0 to 260(℃) Input K *7 *7 Scaling lower limit (only when setting analog input) *7 Decimal point (only when setting analog input) °C/°F selection *7 In ON/OFF control = In 2-PID control = *7 Use the following ranges for scaling: –1999 to 9999, –199.9 to 999.9 c-cp *7 No alarm function 1 Deviation upper/lower limit ON OFF 2 Deviation upper limit ON OFF 3 *1 *1 5 Deviation upper/lower limit standby sequence ON ON OFF 6 Deviation upper limit standby sequence ...

  • マニュアル

    ... when it's OFF. For a current output, lit except for a 0% output. *5 −199.9 to 999.9, Vary Depending on "L", "H" value W PLII Thermocouple Initial Setting Level DO NOT USE RS-485 communications • °C /°F...

  • マニュアル

    ...,4和5要提供不同的报警类型,可以设定上限与下限。 这些用字母 L和H指示。 · 默认值是“2” 第一显示 B 7 • °C/°F:温度单位 PV/SP 连接的传感器与 0 输入类型不同时, s.err 25 0 按住至少3秒钟 *6 (第一显示闪烁, 然后控制停止) 控制周期(加热) 20 (单位:...

  • マニュアル

    ... Manual Basic Type (Cat. No. H156) for details of control range. *2: Error shown only for "Process value / Set point". Not shown for other status. hys Hysteresis 1.0 (Heating) *6 ins Temperature Input 0.0 Shift (Unit: °...

  • マニュアル

    ... as the setting range. setting accuracy range Influence of conductor resistance Thermocouple: ±0.1°C/Ω or ±0.2°F/Ω max. Platinum resistance thermometer: ±1.0°C/Ω or ±1.8°F/Ω max. per line Input shift –99.9 to 99.9°...

  • マニュアル

    ... limit value After shift Before shift Lower limit value 0 About the temperature unit Input shift lower limit value Input (%FS) 100 To switch the temperature unit from “_C” to “_F” for temperature unit, switch the setting of the _...

  • マニュアル

    ...After shift Before shift Lower limit value 0 About the temperature unit 3--4 Input shift lower limit value Input (%FS) 100 To switch the temperature unit from “_C” to “_F” for temperature unit, switch the setting of the _...

  • マニュアル

    ...After shift Before shift Lower limit value 0 About the temperature unit 3--4 Input shift lower limit value Input (%FS) 100 To switch the temperature unit from “_C” to “_F” for temperature unit, switch the setting of the _...

  • マニュアル

    ... setting is “2: K1 (thermocouple).” • For details on input types and setting ranges, see page 5-31. E5AK 3.2 Setting Input Specifications J Temperature input F Temperature unit • To switch the temperature unit from “_C” to“_F” when input is temperature, switch the “_...

  • マニュアル

    ... setting is “2: K1 (thermocouple).” • For details on input types and setting ranges, see page 5-31. E5EK 3.2 Setting Input Specifications J Temperature input F Temperature unit • To switch the temperature unit from “_C” to“_F” when input is temperature, switch the “_...

  • マニュアル

    ... 5Ć31. Ă• For details on input types and setting ranges, see page 5Ć31. 3–4 E5CK 3.2 Setting Input Specifications JTemperature input F Temperature unit Ă• To switch the temperature unit from C" toF" when input is temperĆ ature, switch the ...

  • マニュアル

    ... is “2: K (thermocouple).” • For details on input types and setting ranges, see page 5-25. E5EK---DRT 3.2 Setting Input Specifications J Temperature input F Temperature unit • To switch the temperature unit from “_C” to“_F” when input is temperature, switch the “_...

  • マニュアル

    ... Input type . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-3 Selecting °C/°F . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-3-1 Temperature unit. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-4 Selecting PID Control or ON/OFF Control . . . . . . . . . . . . . . . . . . . . . . . . . . 3-5 Setting Output Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-5-1 Control period. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-5-2 Direct/reverse operation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-6 Setting the SP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-6-1 Changing the SP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-7 Executing ON/OFF Control . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-7-1 ON/OFF Control. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-7-2 Setup . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-8 Determining PID Constants (AT, ST, manual setup) . . . . . . . . . . . . . . . . . . . 3-8-1 AT (auto-tuning). . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-8-2 ST (self-tuning). . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-8-3 ST start conditions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-8-4 ST stable range . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-8-...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-4 3.3 Selecting _C/_F . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-5 Temperature unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-5 3.4 Selecting PID Control or ON/OFF Control . . . . . . . . . . . . . . . . . . . 3.5 Setting Output Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-6 3-7 Control period . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Direct/reverse operation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-7 3-7 E5GN 3.6 Setting the SP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-9 Changing the SP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-9 3.7 Executing ON/OFF Control . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-10 ON/OFF control . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Setup . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-10 3-11 3.8 Determining PID Constants (AT, ST, manual setup) . . . . . . . . . . . 3-12 AT (auto-tuning) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ST (self-tuning) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Manual setup . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-12 3-13 3-15 3.9 Alarm Output . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3-...

  • マニュアル

    ... sensor. Two input type specifications are supported, “platinum resistance thermometer” and “thermocouple and infrared temperature sensor.” 3--4 E5AN/EN/CN/GN 3.1 Variable Area (setup range) List Variable Address type Item Set (monitor) Value C3 0004 _...

  • マニュアル

    ... point is expressed as 16-bit signed binary data (two’s complement for negative values) in the corresponding word allocated in the Master Unit mounted to the PC. The unit used depends on the position of the decimal point in the E5ZE. The default values are 1°...