全 7847 件が検索されました。(5261 - 5280件を表示)

  • マニュアル

    ... used as a voltage output or an open collector output. This is only for short-term protection, however, so be sure to correct the problem quickly. • The following OMRON power supplies are recommended: Input voltage 100 V 200 V Capacity 25 ...

  • マニュアル

    ...The Handheld ID Controller is used to control ID systems such as those shown below. The first is a V600 (short-distance) system; the next, a V620 (long-distance) system. 2 Section 1–2 Configuration V600 Series (Short-distance) Read/Write (R/...

  • マニュアル

    ...ID Controller V600-P01; Monitor Unit V600-P01 Monitor Unit Read/Write Head Read/Write Head Data Carrier Pallet, etc. (when V600-CA1A-V is used) Pallet, etc. (when V600-CA2A-V is used) Read/Write Head (R/...

  • マニュアル

    ... used, be sure to connect it to the Camera 1 connector. 2. For the display terminal, you can substitute a TV which has a video input terminal complying with the EIA RS-170 standard (composite video signal with amplitude of 1.0 V p-p/75 ...

  • マニュアル

    ..., Y and Z directions) Insulation resistance 20 MW min. using a 500 VDC megger (see note) Breakdown voltage 1500 VAC (for 1 minute) (see note) Interface Video output In accordance with RS-170 Composite video signal, Amplitude 1.0 Vp-p/75 ...

  • マニュアル

    ...5 85 55 U 117 75 u 22 16 54 36 6 86 56 V 118 76 v 23 17 55 37 7 87 57 W 119 77 w 24 18 56 38 8 88 58 X 120 78 x 25 19 57 39 9 89 59 Y 121 79 y 26 1A 58 3A : 90 5A Z 122 7A z 27 1B 59 3B ; 91 5B [ 123 7B { 28 1C 60 3C < 92 5C \ 124 7C | 29 1D 61 3D = 93 5D ] 125 7D } 30 1E 62 3E > 94 5E ^ 126 7E ~ 31 1F 63 3F ? 95 5F _ 127...

  • マニュアル

    ...FG Pin no. Abbreviation RDA 9 SDA RDB 5 SDB SDA 6 RDA SDB 1 RDB SG 3 SG The termination resistance must have a minimum resistance of 100 W. 220 W 220 W SW601 SW602 6.8 V Shielded cable The termination resistance (220 ...

  • マニュアル

    ...Connection Diagram The following example provides information on how the RS-422 Intelligent Signal Processor is to be connected to the host computer. Host computer RS-422 Terminator Processor Abbreviation The terminator must have a minimum resistance of 100 ...

  • マニュアル

    ... checking operating status and facilitating system maintenance. • Records up to 30 errors which may occur during operation for the quick investigation into causes of system abnormalities. • Testing communications with a Data Carrier (DC) can be performed off-line. This facilitates installation of the Read/Write (R/...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Wiring the R/W Head . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . DIP Switch Setting . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 4 Communications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-1 4-2 4-3 4-4 4-5 Movement of Data Carrier and Command Status . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Memory Map of Data Carrier . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Command Format . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Types of Commands and Responses . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Example Communication Programs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 5 Testing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-1 5-2 5-3 5-4 5-5 Test Run . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Lists . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Troubleshooting . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Maintenance and Inspection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Systems Check . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 1 2 3 4 5 6 8 11 12 16 25 27 28 33 36 41 55 59 60 61 62 63 63 Appendices A B C D Standard Models . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Codes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Auto Read/...

  • マニュアル

    ...Shock resistance 20G (196 m/s2) Ambient operating temperature 0%C to 50%C Operating humidity 35% to 85% RH (no condensation) Operating environment No corrosive gases Storage temperature –25%C to 65%C Ground Ground resistance: 100 ...

  • マニュアル

    ...plane display Message box Moving the Cursor 1, 2, 3... S. Scn D. Disp 1. Left/Right Movement The following example shows left/right movement within the main menu display. C.Camera B. Bin W. Wind O. Condi M. Meas Y. Sys T. Tool 5 Section 1-2 Basic Console Operation 2. Up/Down Movement The following example shows up/down movement within the scene menu box display. 0. Scene 0: 1. Scene 1: 2. Scene 2: 14. Scene 14: 15. Scene 15: Note Use the direction keys to move the cursor in any of the four directions. Scrolling in ...

  • マニュアル

    ...Displays data on the display. Text display control Command 167 WRITE# Writes data to a sequential file. File control Command 168 WSCROLL Scrolls the window memory. Special graphic display control Command 168 V ...

  • マニュアル

    ... voltage Power consumption E5AJ E5BJ E5EJ E5CJ Input CT input Control output 24 V AC/DC, 50 or 60 Hz 10 VA (at 100 VAC) to 14 VA (at 10 VA (at 24 VAC) 240 VAC) 6 W (at 24 VDC) 10 VA (at 100 VAC) to 12 VA (at 240 VAC) 10 VA (at 100 VAC) to 14 VA (at 240 VAC) 10 VA (at 100 VAC) to 12 VA (at 240 VAC) Thermocouples (K, J, T, L, U, and N) and platinum resistance thermometers (JPt100 and Pt100) Dedicated CT (E54-CT1 or E54-CT3) E5AJ/E5BJ/E5EJ...

  • マニュアル

    ...Basic Screen After the Initial Screen operation has been completed, the following screen will be displayed. This is called the Basic Screen. It serves as the basis for menu operations, and can execute various functions. S.Son D.Disp C.Camera B.Bin ...

  • マニュアル

    .... . . . . . . . . . . . . 91 Section 7-1 Errors 7-1 Errors Errors at Startup Symptom “BUS ERROR” is displayed. “CPU HALT” is displayed. “CPU CHECK ERROR” is displayed. “RAM R/W CHECK ERROR” is displayed. “ROM SUM CHECK ERROR” is displayed. “SUB-CPU ROM ERROR” is displayed. “SUB-CPU RAM ERROR” is displayed. “SUB-CPU NOT READY” is displayed. “SUB-CPU INCORRECT” is displayed. “SUB-CPU ERROR(????)” is displayed. The application program cannot be started at the startup,, instead,, the OVL system y starts t t and d the th promptt is i displayed. di l d The OVL program cannot be ...

  • マニュアル

    ...[”command or function name”] The wildcard characters (?, :) can be used in the command name. The ? wildcard represents a single character and the asterisk wildcard represents any number of characters. For example, the following command would display help messages for all commands beginning with the character ...

  • マニュアル

    ...Hardware error Faulty switch setting External input error Not used Description Required action CPU error due to excessive noise. The switch is set halfway between the settings. The input state is unstable due to excessive noise. The R/...

  • マニュアル

    ... is treated as an ASCII (or JIS 8) code or hexadecimal code is specified in a command. ASCII (JIS 8 Code) One character of ASCII or JIS 8 code data occupies 1 byte (1 address) of the Data Carrier memory. Example of Specifying ASCII Code ...

  • マニュアル

    ... small for the object being measured, use the Camera with a normal CCTV lens and light. → p. 14 Measurement object Distance 20-mm lens: 61 to 71 mm 50-mm lens: 66 to 76 mm Fixed Field of Vision (H × W) 20-mm lens: 20 × 20 mm 50-mm lens: 50 × 50 mm Note Since the field of vision and focal point vary depending on the lens, adjust the setting distance whenever the lens or Camera is replaced. 13 Section 2-6 CCTV Lens Mounting the Camera The specified camera distance is only an approximation. Mount...