全 7847 件が検索されました。(5341 - 5360件を表示)
- マニュアル
...A/D resolution Photo MOS relay scanning system; all channels isolated 10 ch 16-bit Measurement Voltage ranges Temperature Humidity (*1) Measurement Voltage accuracy Thermo(*2) (*3) couple Thermocouples: K, J, E, T, R, S, B, N, ...
- マニュアル
...-voltage input signals) Item 18 Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples K, J, E, T, R, S, B, N, ...
- マニュアル
...Measurement Voltage ranges Temperature 20, 50, 100, 200, 500 mV; 1, 2, 5, 10, 20, 50 V; 1-5 V F.S. Humidity (*1) Measurement Voltage accuracy Thermocouple Type (*2) (*3) Thermocouples: K, J, E, T, R, S, B, N, ...
- マニュアル
...shorted within all channels. Item Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples K, J, E, T, R, S, B, N, ...
- マニュアル
...-CA5D01-V ID Controller ID Sensor Units CS1W-V680C11 CJ1W-V680C11 V68 0C1 RUN1 ERC ERP ERH T/R NOR M/ER R TES T ON HEA D1 V700-A40-W M Cable * Always use the specified Cable to connect a V680-H01-V2 Antenna. The V680-H01-V2 Antenna cannot be connected without using the specified Cable. Antennas with Built-in Amplifier V680-H01-V2 * When V680-H01-V2 is connected with V680-CA1D/-CA2D, V680-D1KP66T cannot be used. RF Tags V680-D1KP58HTN 12 RFID System User's Manual V680-D1KP66T Section 2 Specifications and Performance Section ...
- マニュアル
... output. (0 to 9999.999) Min. pitch (PL) Maximum pitch The maximum detected pitch is output. (0 to 9999.999) Max. pitch (PH) Average width The average detected edge width is output. (0 to 9999.999) Average width (...
- マニュアル
... correction is returned. For details, see "Parameter List (p.39)." 22 About Communication Commands ZFX-C Serial Communication Command Reference Acquiring/Changing Passwords < PASSWORD command > Acquiring the password This command acquires the currently set password. < Command format > P A S S ...
- マニュアル
..._ 0R R _0R_ S 0S _0S_ T 0T _0T_ 0U U _0U_ V 0V _0V_ V400-R1CF/R1CS User’s Manual 89 Section 4 Setting Method Menu sheet W Command 0W _0W_ 0X X _0X_ Y 0Y _0Y_ Z 0Z Section 4 Menu Sheet/Command List _0Z_ $A a _$A_ b $B _$B_ $C c _$C_ d $D _$D_ e $E _$E_ $F f _$F_ g $G _$G_ 90 V400-R1CF/R1CS User’s Manual Section 4 Setting Method Menu sheet h Command $H _$H_ $I i _$I_ j $J _$J_ k $K Section 4 Menu Sheet/Command List _$...
- マニュアル
... DC Current consumption 200 mA max. Ambient operating temperature 0 to 50 °C Ambient operating humidity 25% to 85% Ambient storage temperature −15 to 60 °C (with no icing or condensation) Size (mm) 30 × 58.2 × 98 mm (...
- マニュアル
...-voltage input signals) Item Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50, 100, 200, 500V/F.S.; 1-5V Thermocouples K, J, E, T, R, S, B, N, ...
- マニュアル
...Share name 152 Set value [Factory default] Description This is the name to be recognized by the controller as a network drive. Only 1 unit can be connected.For FZ3-L35 /FZ3-3 /FZ3-7 S,T,U,V,W,X,Y,Z , the shared name is displayed in the \Network folder. For FZ3-9 /FZ3-H9 , the drive letters, such as E:, F:, G:, and H:, are displayed. Setting the System Operation Environment FZ3 User's Manual 4. 5. Shared folder - User name - Password - Specify the shared folder name. Specify the name of the folder that has been created ...
- マニュアル
...Number of Edge Pins N Number of detected edges Average pitch P Average pitch of detected edges Max. pitch PH Maximum pitch of detected edges Min. pitch PL Minimum pitch of detected edges Average width ...
- マニュアル
... Width 0 to 99999.9999 Width amount This is the difference between the ref- 0 to 99999.9999 erence width and the measured edge width. Reference width This is the reference width when the model was registered. JG Judgement ...
- マニュアル
... for low-voltage input signals) Item Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples K, J, E, T, R, S, B, N, ...
- マニュアル
... Input Cables ZR-RX45 User’s Manual Item Description Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples K, J, E, T, R, S, B, N, W (WRe 5-26) Resistance temperature detector PT100, JPT100, PT1000 (IEC751) A/D resolution 16-bit (Effective resolution: About 1/40,000 of the +/- range) Filter Off, 2, 5, 10, 20, 40 Filter operation is on a moving average basis. The average value of the set sampling count is used. If the sample interval exceeds 30 seconds, ...
- マニュアル
...Description Power supply voltage 24 VDC (21.6 to 26.4 V) Output current 0.65 A or higher when no Strobe Controller is connected 1.3 A or higher when a Strobe Controller is connected Recommended Power Supplies S8VS-01524@ (15 ...
- マニュアル
...TransformXY T Try U UnitData U UnitData$ U UnitData2 U UnitInfo U UnitItemIdent$ U UnitJudge U UnitNo U UnitTitle$ V val V varpop V varpush W wait W Wait X xor Statement As command to deal with minimum unit, a statement can't have more than 245 characters. If a statement have more than 245 characters, there will be wrong. And program will suspend. Statement has following three types. ● ● ● Executable statement that make a descriptive record of command treatment and function description. Unexecutable statement that make a descriptive record of annotation and so on that not deal with. Label that ...
- マニュアル
...Number of Edge Pins N Number of detected edges Average pitch P Average pitch of detected edges Max. pitch PH Maximum pitch of detected edges Min. pitch PL Minimum pitch of detected edges Average width ...
- マニュアル
... a power supply with an overcurrent detector, because this sensor uses DC-DC converter for its power supply circuit and inrush current may activate the protective circuit for a power supply with an overcurrent detector. Recommended power supply: S8VS-06024 (Omron, DC24 V 2.5 A 60 ...
- マニュアル
... currently displayed windows can be aligned to the top of the window. When a window protrudes outside the screen and can no longer be displayed, this option allows you to redisplay the window in the screen. Operation Procedure 1. Select [Option(O)]-[Alignment of Windows(...