全 7847 件が検索されました。(5301 - 5320件を表示)
- マニュアル
... Labels for Laser Products The Z500 is designed to be built into the finished system unit. Refer to the following technical standard for installation. 21CFR1040.10 and 1040.11 FDA Labels Class III B Caution logo type DANGER PEAK POWER 15000 µ...
- マニュアル
...Operation Manual 187 Peak/bottom measurement width 99 V Peak-peak Hold 84 VERGET 179 Personal computer 136 Version 152 Position compensation 64 Vertical setting 118, 121 PROFILE 175 Profile display 34 Profile Monitor 33, 121 ...
- マニュアル
... into the finished system unit. Refer to the following technical standard for installation. 21CFR1040.10 and 1040.11 12 PRECAUTIONS FDA Labels for Laser Products Class II Caution logo type Class II Caution logo type CAUTION PEAK POWER 1000 µ...
- マニュアル
...R Real-time zero, 94 U Using outputs in calculations, 93 Recording data, 115 Recording NG data, 122 V Reflecting surface, 51 VERGET, 172 Relative coordinate mode, 94 Version, 144 Removing noise, 62 Reproducing recorded images, 116 ...
- マニュアル
...V530-R160 V530-R160 Branching Link Adapter V530-R160 V530-R160 Notes: When using B500-AL001, Please set the terminator to "ON", and terminate to the line of final stations as follows; V530-R160 - Connect 200 Ω (1/2 ...
- マニュアル
..., always connect it to camera connector 0. Strobe specifications Shutter trigger polarity STGOUT0 or STGOUT1 signal when the flash is synchronized to the OFF-to-ON transition of the strobe trigger signal. Positive The “shutter trigger width” setting determines the pulse width ...
- マニュアル
...a b o p 0 1 # $ SPC CD QR c d q r 2 3 % DEL E F GH I J S T U VWX e f g h i j s t u v w x 4 5 6 7 8 9 ( ) ^ ` BS INS K Y k y . L MN Z l m n z - - ! ¨ 1. These characters can be input. Inserts a space. Deletes 1character to the right of the I cursor. Deletes 1character to the left of the I cursor. Switches between insert (default)/overwrite. Moves the I cursor to the left. Moves the I cursor to ...
- マニュアル
... + R ($12) Left Key CTRL + S ($13) Up Key CTRL + E ($05) Right Key CTRL + D ($04) Down Key CTRL + X ($18) SHIFT + Left Keys CTRL + F ($06) SHIFT + Up Keys CTRL + W ($17) SHIFT + Right Keys CTRL + H ($08) SHIFT + Down Keys CTRL + Z ($1A) F1 Key CTRL + C ($03) F2 Key CTRL + V ($16) F3 Key CTRL + B ($02) F4 Key CTRL + N ($0E) F5 Key CTRL + J ($0A) F6 Key CTRL + K ($0B) F7 Key CTRL + L ($0C) F8 Key CTRL + O ($0F) F9 Key CTRL + P ($10) --- (See note.) CTRL + Q ($11) Note Changes the ...
- マニュアル
...a b o p 0 1 # $ SPC CD QR c d q r 2 3 % DEL E F GH I J S T U VWX e f g h i j s t u v w x 4 5 6 7 8 9 ( ) ^ ` BS INS 1. K Y k y . L MN Z l m n z - - ! These characters can be input. Inserts a space. Deletes 1character to the right of the I cursor. Deletes 1character to the left of the I cursor. Switches between insert (default)/overwrite. Moves the I cursor to the left. Moves the I cursor to ...
- マニュアル
...Bit Clear Clears the specified bits of the specified area in the Data Carrier. Masks the specified bits in the specified area of the Data Carrier and writes data to the bits that are not masked. Writes the data read from a Data Carrier by one R/...
- マニュアル
... case of short-circuit), or – a secondary fuse or other such secondary circuit protective device used to limit the available current shall be rated at not more than a value 4.2 amperes (for the power supply voltage of 24VDC) Recommended power supply: S82K (15 ...
- マニュアル
... body. This product is designed to be built into the finished system unit. Refer to the following technical standard for installation. 21CFR1040.10 and 1040.11 FDA Labels for Laser Products Class III B DANGER logo type DANGER PEAK POWER 15000 µ...
- マニュアル
...k l m A B C D E F G H I J K L M n o p q r s t u v w x y z N O P Q R S T U V W X Y Z 0 1 2 3 4 5 6 7 8 9 -1 0 1 2 3 4 5 6 7 8 9 -1 (Most significant digit) IX ● Revision History The revision code of this manual is given at the end of the catalog number at the bottom left of the back cover. The following table outlines the changes made ...
- マニュアル
...CR method AC DC Yes Yes Characteristic Required element The capacitance of the capacitor must be 1 to 0.5 m F per contact current of 1 A and resistance of the resistor must be 0.5 to 1 W per contact voltage of 1 V. These values, howIf the supply voltage is 24 ever, vary with the load and the characteristics of the relay. or 48 V, insert the surge Decide these values from protector in parallel with the load. If the supply volt- experiments, and take into age is 100 to 200 V, insert consideration that the capacitance ...
- マニュアル
...Edit Rung Comments Select Objects Insert (I) Rung (M) Contact (input bit)/ Coil (output bit) Horizontal (H) Vertical (V) Ladder rung diagram Electrical circuit diagram 50% 100% 150% 200% Help (H) Go Online/Offline (...
- マニュアル
...Min. switched current/voltage 10 mA/10 V Power supply - user select 110/230 V AC (50-60 Hz) and 24 V AC/DC +10%−15% (110-V setting also allows use at 100 V ±10%) Power consumption <9 VA 6 W Relay outputs 2 × independent volt free N/O safety contacts 1 × volt free N/C auxiliary contact NB - Aux must not be used for safety circuit Fuse externally, 5 A max. (quick acting) for AC 2.5 A max. (quick acting) for DC Utilization category AC - 15; 4 A/250 V AC DC - 13; 2 A/...
- マニュアル
... body. This product is designed to be built into the finished system unit. Refer to the following technical standard for installation. 21CFR1040.10 and 1040.11 FDA Labels for Laser Products Class III B DANGER logo type DANGER PEAK POWER 15000 µ...
- マニュアル
...1 2 SW SETTING DAT BUSY TEST IN RUN ERR/ALM INH PRPHL COMM BKUP MCPWR BUSY TEST HEAD1 HEAD1 HEAD2 HEAD2 OUT HEAD2 HEAD2 R/W Head R/W Head DC DC Workpiece (moving body) NT-AL001 Converter Workpiece (moving body) 3 Section 1-3 Operation Overview 1-3 Operation Overview RS-422A NT-AL001 Converter RS-232C or ID Controller SYSMAC CJ1G-CPU44 PROGRAMMABLE CONTROLLER OPEN RUN ERR/ALM INH PRPHL COMM BKUP IN OUT 0 1 2 3 4 0 1 2 5 6 7 8 9 3 4 5 V600C12 RUN ERC ERP ERH HEAD1 HEAD2...
- マニュアル
...Mounting method Power consumption APPENDICES Encoder input Inputs External inputs H8PS- BP H8PS- BFP 24 VDC 85% to 110% of rated supply voltage Flush mounting Surface mounting, Flush mounting track mounting Approx. 4.5 ...
- マニュアル
... write data, a command error will occur. • Data Write Example If “V670” is specified as the write data for 4 bytes of memory beginning with the address 10h, the data is written to the Tag memory SECTION 4 as shown in the diagram. Command ...