全 50423 件が検索されました。(501 - 520件を表示)
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
...) Displays the details of the Execution Log. In the Details parameter, information items are separated from each other by a tab. The number of information items in the Details parameter is variable. The contents differ according to the category. When it is output, ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
...CP2E CPU Unit Hardware User’s Manual(W613) 5 Installation and Wiring z Countermeasure Examples • When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Current Circuit AC Inductive load ...
- マニュアル
... power is turned ON Set. 00 Hex When power is turned ON : FF hex 2-3-5 End Code None (Received Bytes) Received Bytes (no end code) 256 bytes 256 bytes When power is turned ON CR, LF Set End Code 2-3-6 Received Bytes (setting) When power is turned ON 1 byte : 255 bytes 2-3-7 Set End Code (setting) 00 Hex Delay 0 ms 00 Hex When power is turned ON : FF Hex 2-3-8 0 (×10 ms) When power is turned ON : 9999 (×10 ms) 2-5 Modbus-RTU Easy Master Settings 2-...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...
- マニュアル
...times Capacitor Relay Approx. 2 to 3 times Approx. 20 to 50 times Resistance load 1 • Absorption Element Example Absorption element Effectiveness 16 Diode Diode + Zener diode Varistor CR ❍ ❍ ∆ ✕ Normal current As an absorption element, the diode is the most effective at suppressing the counter-electromotive force. The release time for the solenoid or electromagnetic valve will, however, increase. Be sure to check the circuit before use. To shorten the time, connect a Zener diode and a regular diode in series. The release time will be shortened at the same rate that the Zener voltage (Vz) of the Zener diode ...
- マニュアル
... No. 01h 0 1 Test data Command code 1 Data 1 0 1 Data 2 2 3 Data 3 4 5 FCS Data 4 6 7 8 0 CR 8 0Dh Response SOH Node No. Response code 01h 0 0 1 0 Test data Data 1 1 Data 2 2 3 Data 3 4 5 FCS Data 4 6 7 8 0 ...
- マニュアル
...Circuit Current AC DC Power supply Inductive load Varistor method Power supply Yes No Yes Yes Yes Inductive load Diode method Power supply Yes Inductive load CR method Characteristic Required element If the load is a relay or solenoid, there is a time lag between the moment the circuit is opened and the moment the load is reset. If the supply voltage is 24 or 48 V, insert the surge protector in parallel with the load. If the supply voltage is 100 to 200 V, insert the surge protector between the contacts. The capacitance of the capacitor must be 1 ...
- マニュアル
...C D E F 0 1 2 3 4 5 6 7 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US SPACE ! ‘‘ # $ % & ‘ ( ) * + , . / 0 1 2 3 4 5 6 7 8 9 : ; < = > ? @ A B C D E F G H I J K L M N O P Q R S T U V W X Y Z [ ¥ ] ^ _ ` a b c d e f g h i j k l m n o p q r s...
- マニュアル
....3-36 cycle.) VERSION - (Displays the Sensor Controller version.) LENGTH 8BIT 8BIT, 7BIT PARITY NON NON, ODD, EVEN STOP 1BIT 1BIT, 2BIT BAUDRAT 38400 9600, 19200, 38400, 57600, 115200 DELIMIT CR CR, LF, ...
- マニュアル
...cycle.) VERSION - (Displays the Multi-Controller version.) - LENGTH 8BIT 8BIT, 7BIT - PARITY NONE NONE, ODD, EVEN - STOP 1BIT 1BIT, 2BIT - BAUDRAT 38400 9600, 19200, 38400, 57600, 115200 - DELIMIT CR CR...
- マニュアル
...- (Data Storage Unit system clock) p.3-36 HOUR LENGTH 8BIT 8BIT, 7BIT p.4-5 PARITY NONE NONE, ODD, EVEN STOP 1BIT 1BIT, 2BIT BAUDRAT 38400 9600A19200A38400A57600 A115200 DELIMIT CR CR, LF, CR+LF MODE COMPWAY COMPWAY, NORMAL p.4-5 NODE 0 0 to 16 p.4-5 FORMAT - - p.3-37 FILE No. (current start No.) 0 to 999 p.3-37 KEYLOCK OFF OFF, ON p.3-37 LANGUAG Japanese Japanese, English p.3-38 Section 3 SETUP INFO p.3-35 *1: When [IMAGE] - [SOURCE] - [IMGSAVE] is ON *2: When [IMAGE] - [SOURCE] - [IMGSAVE] is ...
- マニュアル
... No. 01h 0 1 Test data Command code 1 Data 1 0 1 Data 2 2 3 Data 3 4 5 FCS Data 4 6 7 8 0 CR 8 0Dh Response SOH Node No. Response code 01h 0 0 1 0 Test data Data 1 1 Data 2 2 3 Data 3 4 5 FCS Data 4 6 7 8 0 ...
- マニュアル
...The format of non-procedural commands are as follows: Example: A command to acquire a measured value MEASURE command * Each character is output as an ASCII code (except for FLOWDATA response). M E A S U R E O ...
- マニュアル
...-XC_A: within 10 m (including Sensor Head cable. Extension Cable cannot be daisy-chained.) - Extension Cable: ZS-XC_B(R): within 22 m (including Sensor Head. Up to two Extension Cables can be daisy-chained.) - Extension cable for a long distance ZS-XC_ _...