全 50423 件が検索されました。(521 - 540件を表示)

  • マニュアル

    ... Antenna’s interrogation zone, “--” will be displayed. The measurement result is also output from the USB port. Monitor display Bar indicator 1 Output from the USB Port The distance level and Antenna channel are output from the USB port. DL 06 1 0 * [...

  • マニュアル

    ... the data retention time *1. High temperatures are those exceeding 125°C up to 250°C. • Resetting the data retention time 1.Reading data from the RF tag addresses 0010Hex to 0015Hex. Command : RDSTH100100006*[...

  • マニュアル

    ... the data retention time *1. High temperatures are those exceeding 125°C up to 250°C. • Resetting the data retention time 1.Reading data from the RF tag addresses 0010Hex to 0015Hex. Command : RDSTH100100006*[...

  • マニュアル

    ..., 19200, 38400 (default value: 38400) LEN (data length) 7, 8 (default value: 8) S.BIT (stop bit) 1, 2 (default value: 1) PRTY (parity) NONE (none), ODD (odd), EVEN (even) (default value: NONE) HD.FT ST.ET (STX+ETX), ...

  • マニュアル

    ...4 E “N” V600 Commands W T A 1 byte 1 0 Command code ASCII Processing setting area number setting 0 1 0 O M R O N CR Write data Start address Terminator V680 Commands W T S T A 1 0 ASCII Processing Command code Communications setting area number specification 0 1 0 O M R O N Write data Start address ...

  • マニュアル

    ...Value Settings Option/Range Pages SYSTEM COMM PORT DATA BIT 8BIT 8BIT, 7BIT PARITY NON NON, ODD, EVEN STOP BIT 1BIT 1BIT, 2BIT BAUD RATE 38400 9600A19200A38400A57600 A115200 DELIMITER CR+LF CR, LF, CR+LF PASSWORD ON/OFF OFF (Displayed only when password is set to ON) BUZZER ON OFF, ON p.3-21 LANGUAGE - JAPANESE, ENGLISH p.3-21 LIGHT OFF TIME TIME INPUT p.3-21 LOG DATA OFF OFF, ON p.3-21 SYSTEM DATA - (Initializes controller settings.) p.3-22 HEAD DATA - VERSION - (Displays controller version.) p.3-22 EMISSION button OFF ON, OFF CH button...

  • マニュアル

    ...The wav Exclusive extension cables are available for extending the installation distance between the Sensor Head and the Controlle. Can be extended a maximum of 27 m. Cable for Sensor: 0.5 m, 2 m (flexible cable) Extension cable (*1) ZG2-XC__...

  • マニュアル

    ...-[SYSTEM]-[COM] Setting value Setting range RS-232C LENGTH 8BIT, 7BIT (default value: 8BIT) PARITY NONE, ODD, EVEN (default value: NONE) STOP 1BIT, 2BIT (default value: 1BIT) BAUDRAT 9600, 19200, 38400, 57600, 115200 (default value: 38400) DELIMIT ...

  • マニュアル

    ...Node No.1 is tested with the data 12345678. SECTION 3 Communications Test • 1:1 Protocol Command Test data Command code 1 Data 1 0 1 Data 2 2 3 Data 3 4 5 CR Data 4 6 7 8 0Dh Response Test data Response code 0 0 Data 1 1 Data 2 2 3 Data 3 4 5 ...

  • マニュアル

    ...Amplifier Unit Host A test is preformed for the Amplifier Unit using the data 12345678. Command Test data Command code 1 Data 1 0 1 Data 2 2 3 Data 3 4 5 CR Data 4 6 7 8 0Dh Response Test data Response code 0 0 Data 1 1 Data 2 2 3 Data 3 4 5 ...

  • マニュアル

    ... the File Format The output CSV file format can be changed according to the external device. Item Symbol Field separator None, comma (default), tab, space, or semicolon Decimal symbol None, point (default), or comma Record separator None, comma, tab, space, or ...

  • マニュアル

    ...X Position X This is the X coordinate of the position −99999.9999 to 99999.9999 where the model was found. Y Position Y This is the Y coordinate of the position −99999.9999 to 99999.9999 where the model was found. ...

  • マニュアル

    ...Setting content Command 9600 bps (Factory default setting) Data length 8 bits (Factory default setting) Parity None (Factory default setting) Stop bit 1 bit (Factory default setting) Header None (Factory default setting) Footer ...

  • マニュアル

    .... Section 4 Creating Setting Files Using the 2DCR Configear ■ Open 9,600*, 19,200, or 38,400 None*, odd, or even * 77 bits or 8 bits 1sbit* or 2 bits None*, 02 , or 1B * ETX, 0A LF, 0D CR , or 0D0A ...

  • マニュアル

    ... 99,999.9999 ST 108 Data name Reference angle This is the angle when the model was registered. Adjusting the Images That Were Taken -180 to 180 FQ2-S/CH User’s Manual Expression text string Data name CR...

  • マニュアル

    ...EtherNet/IP: p.101 PLC link: p.131 PROFINET: p.156 No-protocol (TCP), No-protocol (UDP): p.182 Note • Endian Little endian data is output. • Code Conversion The converted codes are outputted for the following character codes. Character code ...

  • マニュアル

    ...Host Amplifier Unit Node No.1 is tested with the data 12345678. • 1:1 Protocol Command Test data Command code 1 Data 1 0 1 Data 2 2 3 Data 3 4 5 CR Data 4 6 7 8 0Dh Response Test data Response code 0 0 Data 1 1 Data 2 2 3 Data 3 4 5 ...

  • マニュアル

    ...Amplifier Unit Host A test is preformed for the Amplifier Unit using the data 12345678. Command Test data Command code 1 Data 1 0 1 Data 2 2 3 Data 3 4 5 CR Data 4 6 7 8 0Dh Response Test data Response code 0 0 Data 1 1 Data 2 2 3 Data 3 4 5 ...

  • マニュアル

    ...Bank copy [BK.COPY] Save [SAVE] Initialization [INIT] ASCII[ASCII]*/Binary[BINARY] − 1 / 2 / 3 / 4 /5* − 0 / 1 / 2 / 3 / 4 / 5 / 6* − Off* /On − None [NO]*/Comma [COMMA]/ Tab [TAB]/Space [SPACE]/ CR[CR...

  • マニュアル

    ... length Sets the data length. 8 bits (default value), 7 bits Parity Sets the parity bit (error detection sign). None (default value), odd, even Stop bit Sets the stop bit. 1bit (default), 2bit Delimiter Sets the delimiter (data delimiter). ...