全 50423 件が検索されました。(541 - 560件を表示)
- マニュアル
... Failure due to Sulphurization or Chlorination 24 CASE 13 Corrosion 26 CASE 14 Contact Failure due to the Penetration and Adherence of Foreign Substances (Such as Dust and Insects) 28 CASE 15 Burn Damage 30 CASE 16 ...
- マニュアル
... Failure due to Sulphurization or Chlorination 24 CASE 13 Corrosion 26 CASE 14 Contact Failure due to the Penetration and Adherence of Foreign Substances (Such as Dust and Insects) 28 CASE 15 Burn Damage 30 CASE 16 ...
- マニュアル
... (TCP) communications use serial commands stated in this manual. For example, “Read” commands are described in Appendix H — Read Cycle. The following describes the output format of serial (RS-232C, TCP) communications.
Read strings - マニュアル
... the number of wires, so use common return circuits. Use thick wires with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use countermeasures, such as ...
- マニュアル
... Cycle Character notatiion 1 2 Hex notatiion 31 32 Read result 3 4 5 33 34 35 Autofocus Multicode Reader MicroHAWK V320-F/V330-F/V420-F/V430-F Series User Manual for Communication Settings (Z407-E1) CR...
- マニュアル
... the figure on the right varies depending on your environment. * For details on the command, refer to 9.2.2. Command Settings. Response Format Read data 1 2 3 4 5 6 7 8 9 0 A B C D E CR LF Footer 25 8. Initializing the System 8. Initializing the System This document assumes that each device uses the factory default settings. If you change their settings from the defaults, you may not be able to perform various setting procedures as described. 8.1. Initializing the Controller To initialize the controller, initialize the CPU Unit. Before initialization, ...
- マニュアル
...8 bits (default) Stop bit 1 bit 1 bit (default) Parity None None (default) Baud rate 9,600 bps (default) 9,600 bps Protocol macro transmission Full-duplex --- Header --- None (default) Footer --- <CR+LF> (default) Host port protocol --- Point-to-point (default) (connection) port method * SCU Unit: Serial Communications Unit Precautions for Correct Use It is assumed that the CJ1W-SCU22 Serial Communications Unit is used with the unit number is 0 and the communications (connection) port Port 2. If using other conditions to connect the Unit, refer to Section 9. Program and create a program by modifying the control...
- マニュアル
...f g h i j k l m n o Code A NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI Code B ` a b c d e f g h i j k l m n o Input p q r s t u v w x y z { | } ~ @D Code A DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US Code B p q r s t u v w x y z { | } ~ DEL Fiber Laser Marker MX-Z2000H-V1 series User’s Manual (...
- マニュアル
... in the Watch Tab Page, as shown in the figure on the right. Response Format Read data * The receive data in the figure on the right varies depending 1 2 3 4 5 6 7 8 9 0 A B C D E CR LF on your environment. Footer * For details on the command, refer to 9.2.2. Command Settings. 27 8. Initializing the System 8. Initializing the System This document assumes that each device uses the factory default settings. If you change their settings from the defaults, you may not be able to perform various setting procedures ...
- マニュアル
... bits (default) Stop bit 1 bit 1 bit (default) Parity None None (default) Baud rate 9,600 bps (default) 9,600 bps Protocol macro transmission method Full-duplex --- Header --- None (default) Footer --- <...
- マニュアル
...ASCII code. Send and Receive Messages Send message 3C '<' 20 '' 3E '>' 00 31 32 33 34 35 36 0D 0A '1' '2' '3' '4' '5' '6' [CR] [LF] (Normal processing) Receive message 1 (Error processing) No response message will be returned in error processing. 44 9. Software Part 9.3. Error Judgment Processing This section describes error judgment processing by the software part. 9.3.1. Error Judgment by the Software Part This software part performs error judgment processing for the following four types of errors (1) to (4). Refer to 9.7. Error Code List for information on error ...
- マニュアル
... (TCP) communications use serial commands stated in this manual. For example, “Read” commands are described in Chapter 5 Read Cycle. The following describes the output format of serial (RS-232C, TCP) communications.
Read strings - マニュアル
... Guide December 2022 5.9.2.TCP/IP and Serial Output String TCP/IP or Serial output messages provide the ability to transmit inspection results like a barcode or measurement to another device. In this example we will send the Decode1 tool string followed by ...
- マニュアル
...0 Enter Key N/A N/A N/A Tab Key N/A N/A N/A Miscellaneous Options Transmit Code ID Character 45 2Dh None Preamble Value 99, 105 63h, 69h 7013 <CR>
Postamble 1 Value 98, 104 62h, 68h Postamble 2 Value 100, 106 64h, 6Ah Scan Data Transmission Format 235 EBh FN1 Substitution Values 103, 109 67h, 6Dh 7013 <... - マニュアル
... bit 8 bit (default) Stop Bits 1 bit 1 bit (default) Parity No None (Default) Baud Rate 115,200bps 115,200Bps (default) Protocol macro transmission Full Duplex - Header - None (default) Footer - <CR+LF> method * SCU Unit: Serial Communications Unit Precautions for Correct Use It is assumed that the serial communication unit used is "CJ1W-SCU22", the unit number is "0", the communication (connection) port is "port 2" and these have been set ahead of time.When connecting under conditions other than this, refer to Section 9 “Program" and change the control data of the assigned Relay Area and PMCR ...
- マニュアル
... is.) 33 ● Sent/Received Message Send Message 54 'T’ 52 'R' 49 'I' 47 'G' 47 'G' 45 'E' 52 'R' (Normal processing: measurement data 369 171 -1,LOT123456 DATE05/2012,123456<CR>
) Receive Message 33 ‘3’ 4F ‘O’ 45 ‘E’ 34 ‘4’ 36 ‘6’ 54 ‘T’ 30 ‘0’ 35 ‘5’ 39 ‘9’ 31 ‘1’ 35 ‘5’ 36 ‘6’ 20 ‘’ 32 ‘2’ 2F ‘/’ 0D ... - マニュアル
...Class C Supports IRT communication that realizes reliable synchronization. Not Supported The functions below are defined in Class A. Function Overview Cyclic Data Exchange Real-time data communication between the IO controller and IO devices at determined cycles. Set by IO data ...
- マニュアル
...) 1: Judgment result OK -1: Judgment result NG -10: Error (image format mismatch) -11: Error (unregistered model) -12: Error (insufficient memory) -20: Error (other errors) Count C No. of models detected If none detected, 0 Mean correlation ...
- マニュアル
...output(Message) icon on the Main window of the Vision Sensor to open its setting screen. 2 Open “Output setting” tab to confirm the settings are as figure shown in right. Output : Serial (Ethernet) Delimiter string:\20 (Space) Terminate string:\r (...
- マニュアル
... (TCP) communications use serial commands stated in this manual. For example, “Read” commands are described in Chapter 5 Read Cycle. The following describes the output format of serial (RS-232C, TCP) communications.
Read strings