全 50423 件が検索されました。(481 - 500件を表示)

  • マニュアル

    ....) is being sent as an attached file in TXT format, the data is stored with the following procedure. 1. The word data is converted to ASCII. 2. The word data is delimited by hard tabs ([HT]: 09). 3. A return and line feed ([...

  • マニュアル

    ...1011 B 1100 C 1101 D 1110 E 1111 F 0000 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0001 1 DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US 0010 2 Space ! ” # $ % & ’ ( ) * + , . / 0011 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 0100 4 @ A B C D E F G H I J K L M N O 0101 5 P Q R S T U V W X Y Z [ \ ] ^ _ 0110 6 a b c d e f g...

  • マニュアル

    ...i y 0A lf sub * : J Z j z 0B vt esc + ; K [ k { 0C ff fs , < L \ l | 0D cr gs = M ] m } 0E so rs . > N ^ n ~ 0F si us / ? O _ o del 241 International System of Units 242 Appendix E Revision History A manual revision code appears as a suffix to the catalog number on the front cover of the manual. Cat. No. W440-E1-04 Revision code The following table outlines the changes made to the manual during each revision. Page numbers refer to the previous version. Revision code 01 02 Date November 2004 November 2005...

  • マニュアル

    ...&0 0x0000 to 0x00FF &0 to &2 End code EndCode INT &0 Receive data size RecvDataSize INT &0 ■ Start Code Start code specified Start code not used ■ End Code End code specified CR+LF specified for end code End code not specified 0x0000 to 0x0OFF &0 to &256 Description 1 (ON): FB started. 0 (OFF): FB not started. Specify the Unit and the serial port. Q Serial Communication Board(SCB) Unit selection #BBBB Serial port No. &1: Port 1 &2: Port 2 Q Serial Communication Unit(SCU) Unit selection SCU Unit No. (&0 to &15) Serial port No. &1: ...

  • マニュアル

    .../Parallel Structure 13 Illegal Axis Declaration 14 Position Specification Error 15 Speed Specification Error 16 Time Specification Error 98 Detailed description Number of blocks of programming exceeded 800. ----Number of characters in one block exceeded 128 including ...

  • マニュアル

    ...23 01 01 X10 [0-63] 789 789 456 X1 0 1 2 3 4 5 6 7 OUT 8 9 10 11 12 13 14 15 MS NS WORD NODE ADR CRT1 CR X10 [0-63] T1-AD AD04 04 ANALOG TERMINA L 456 78 78 456 23 WORD NODE ADR CRT1 CR T1-OD OD1616 1 REMOTE TERMIN AL 23 MS NS 9 01 01 23 0 1 2 3 4 5 6 7 OUT X1 9 01 23 456 X10 [0-63] 789 789 456 CRT1 ...

  • マニュアル

    ...2 outputs CRT1-DA02 I/O capacity 4 inputs Model CRT1-VAD04S 2 outputs CRT1-VDA02S 4 inputs CRT1-VAD04ML 2 outputs CRT1-VDA02ML X1 X10 63] [0- 04 AD T1- AL CR MIN N TER RO G ALO OM AN Features I/O range: 0 to 5 V, 1 to 5 V, 0 to 10 V, −10 to 10 V, 0 to 20 mA, 4 to 20 mA Units with Connectors Type Analog I/O Slave Units with e-CON Connectors Analog I/O Slave Units with MIL Connectors 24 Appearance Features I/O range: 0 to 5 V, ...

  • マニュアル

    ... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...

  • マニュアル

    ...CP1E CPU Unit Hardware User’s Manual(W479) 5 Installation and Wiring  Countermeasure Examples • When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Current Circuit AC Inductive load ...

  • マニュアル

    ... power is turned ON Set. 00 Hex When power is turned ON : FF hex 2-3-5 End Code None (Received Bytes) Received Bytes (no end code) 256 bytes 256 bytes When power is turned ON CR, LF Set End Code 2-3-6 Received Bytes (setting) When power is turned ON 1 byte : 255 bytes 2-3-7 Set End Code (setting) 00 Hex Delay 0 ms 00 Hex When power is turned ON : FF Hex 2-3-8 0 (×10 ms) When power is turned ON : 9999 (×10 ms) 2-5 Modbus-RTU Easy Master Settings 2-...

  • マニュアル

    ...-485 port or the Serial Option Board port. (The output port is specified with bits 8 to 11 of C.) • The following send-message frame format can be set in the PLC Setup. 1) Start code: None or 00 to FF hex. 2) End code: None, ...

  • マニュアル

    ... 6 7 OUT 8 9 10 11 12 13 14 15 MS NS WORD NODE ADR X10 [0-63] 23 9 01 CRT1-AD04 ANALOG TERMI NAL 456 78 78 456 CRT1 CR T1-OD16-1 REMOTE TERMI NAL 23 MS NS 23 23 23 0 1 2 3 4 5 6 7 OUT X1 9 01 456 01 X10 [0-63] 789 789 456 CRT1 ...

  • マニュアル

    ...01 01 X10 [0-63] 456 789 789 456 0 1 2 3 4 5 6 7 OUT 8 9 10 11 12 13 14 15 X1 MS NS WORD NODE ADR CRT1 CR 23 9 01 CRT1 CR X10 [0-63] T1-AD AD04 04 ANALOG TERMINA L 456 78 78 456 T1-OD OD1616 1 REMOTE TERMIN AL 23 MS NS 23 23 0 1 2 3 4 5 6 7 OUT X1 9 01 23 456 01 X10 [0-63] 789 789 456 CRT1 ...

  • マニュアル

    ... user, or when a Serial Communications Unit is connected to devices that only receive or send data, such as bar code readers, or printers. Execute data transmission Text 1-3-4 No-protocol Mode ST 1 SerialSend Serial Communications Unit ...

  • マニュアル

    .... Using a contact protection circuit can also cause a delay in the resetting time (shut-off time). Contact protection circuit examples are listed in the following table. Current Circuit Power supply 7-20 C R Inductive load ...

  • マニュアル

    ... Manual (W524) 4 Installation and Wiring DC Relays AC Relays + DC RY Diode for absorbing surge AC RY Surge absorber − Solenoids 4-4 Wiring Precautions SOL Surge absorber (Example: Okaya Electric Industries ...

  • マニュアル

    ...6-4 NJ/NX-series Database Connection CPU Units User’s Manual (W527) 6 How to Use Operation Logs [Serial number][Date][Time][Millisecond][Category][Log code][Log name][Result][DB Connection name][Serial ID][Details]<...

  • マニュアル

    ... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...

  • マニュアル

    ... the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • If noise causes malfunctions, use countermeasures, such as ...

  • マニュアル

    ... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...