全 50423 件が検索されました。(461 - 480件を表示)

  • マニュアル

    ...). Use a surgeabsorbing diode with a voltage resistance of at least five times the circuit voltage. DC Relay DC RY AC Relay Surge-absorbing diode AC Solenoid, etc. SOL 10 Surge absorber (Example: Okaya Electric's ...

  • マニュアル

    ... the current will be converted into Joule heat by the resistance of the inductive load. This time lag, between the moment the circuit is opened and the moment the load is reset, caused by this method is longer than that caused by the ...

  • マニュアル

    ... to 07 08 to 15 Function Node number (Host Link) 00 to 31 (BCD) Start code enable (RS-232C) 0: Disable; 1: Set End code enable (RS-232C) 0: Disable (number of bytes received) 1: Set (specified end code) 2: ...

  • マニュアル

    ... non-procedure mode start code enable cedure 0: Disabled (default); 1: Enabled 12 to 15 Non-pro- Port B non-procedure mode end code enable cedure 0: Disable (Specify the number of receive data items) (default) 1: Enable (Specify the end code) 2: ...

  • マニュアル

    ...Section 4-1 Overview 4-1 Overview The following operations are covered in this section. Operation Command/function Opening a communications port OPEN command Sending data PRINT command (The LPRINT command executes device: LPRT.) Receiving data ...

  • マニュアル

    ... transmission method Asynchronous Baud rate 9,600 bps Start bit 1 bit Stop bit 1 bit Parity Even Character code ASCII 7 bits Data format 8 characters (P or A) (+ or –) (0 to 9) x 5 digits (CR) Serial Data P or A, Start bit 0 to 9 + or – Data ...

  • マニュアル

    ...256 01 1 to to FF 256 Value (Hex) No-protocol Mode end code setting 0 None (Specify the amount of data being received) 1 Yes (Specify the end code) 2 End code is set to CR+LF Value (Hex) No-protocol Mode start code setting 0 None 1 Yes Address 166@@@@ RS-232C port Value (Hex) 0000 0001 to 0007 Maximum Unit No. in NT Link Mode No. 0 No. 1 to No. 7 Address 195@@@@ Value (Hex) Scheduled interrupt time units 0000 10 ms 1.0 ms 0001 Note These settings are not supported for CS1D Duplex-CPU ...

  • マニュアル

    ...1011 B 1100 C 1101 D 1110 E 1111 F 0000 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0001 1 DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US 0010 2 Space ! ” # $ % & ’ ( ) * + , . / 0011 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 0100 4 @ A B C D E F G H I J K L M N O 0101 5 P Q R S T U V W X Y Z [ \ ] ^ _ 0110 6 a b c d e f g...

  • マニュアル

    ... the port parameters as follows: • Port 1 Parameters Data length: 8 bits Parity: None Stop bits: 1 Header code: Disabled Delimiter code: Enabled Flow control: Enabled Baud rate: 9,600 bps Delimiter code ...

  • マニュアル

    ... that the current will be converted into Joule heat by the resistance of the inductive load. This time lag, between the moment the circuit is opened and the moment the load is reset, caused by this method is longer than that caused by the ...

  • マニュアル

    ... firmly. Also, be sure that the coaxial cable is locked before use. Attaching Connectors to Coaxial Cable Assemble the connector parts as shown below. Contact clip Body Sleeve Ferule Contact Approx. 24.3 mm A hand crimp tool (...

  • マニュアル

    ...(Any other setting disables the start code, causes a non-fatal error, and turns ON AR 1302.) 12 to 15 End code selection for no-protocol communications 0 (Hex): Disables end code; 1 (Hex): Enables end code in DM 6649; 2 (Hex): Sets end code of ...

  • マニュアル

    ... characters Data Format Byte +0 P (See note 1.) Note +1 +2 +3 +4 +5 Data on the number of rotations Sign (+ or -) Whole numbers (5 digits of decimal numbers) +6 +7 CR 1. “P" of ASCII code. It is 50 Hex in hexadecimal. 2. The range of No. of rotations that can be received by the unit is between +65535 to -65535. 3. For details of the data on the number of multi-turns received from a servo driver, please check the manual of the servo driver in use. 4. Please set the unit function setting "high-speed ...

  • マニュアル

    ... locked securely before starting operation. 2-1-4 Attaching Connectors to the Coaxial Cable The following diagram shows the parts that make up the BNC connector. Body Sleeve Contact crimp Ferrule Contact Approx. 24.3 mm A hand crimp tool (...

  • マニュアル

    ...Transfer direction Method Max. amount of data Data transmission Execution of TXD(236)/ 256 bytes (PLC → External device) TXDU(256) in the program* Frame format Start code End code Yes: 00 to FF Yes: 00 to FF or ...

  • マニュアル

    ...AC DC C Power supply R Inductive load Varistor method Power supply Yes No Yes Yes Yes Inductive load Diode method Power supply Yes Inductive load CR method Characteristic Required element If the load is a relay or solenoid, there is a time lag between the moment the circuit is opened and the moment the load is reset. If the supply voltage is 24 or 48 V, insert the surge protector in parallel with the load. If the supply voltage is 100 to 200 V, insert the surge protector between the contacts. The capacitance of the capacitor must be 1 ...

  • マニュアル

    ...750 2 1 ,8 0 0 3 5 9 ,00 0 4 8 5 ,00 0 5 9 0 ,00 0 6 1 0 8 ,0 0 0 7 1 2 5 ,0 0 0 CV Cr ossing +CV −CV +CV −CV +CV −CV +CV −CV +CV −CV +CV −CV +CV −CV c rossing crossing c rossing crossing c rossing crossing c rossing crossing c rossing crossing c rossing crossing c rossing crossing Out1 Soft2 Soft3 R S R R S S S R R R S This example shows the Comparison Mode applied to a Circular Counter. 74 Section ...

  • マニュアル

    ... system × 2 m • Total cable length ≤ 20 m • Length of a single cable ≤ 4 m (for a 1:1 connection) 15 devices max. including the GP-IB Interface Unit GP-IB device address Delimiters 0 to 30 Select from the following: ...

  • マニュアル

    ...× 4 Rotary: 1V/250r/min × 10 Linear: 1V/100mm/s 7 Motor rotation speed × 8 Rotary: 1V/125r/min × 100 Linear: 1V/10mm/s 8R Reserved 9R Reserved AR Reserved BR Reserved CR Reserved DR Reserved ER Reserved Reserved 1 Analog monitor 2 2 Reserved --- 0 3 Reserved --- 0 S Reserved 0 Reserved 1R Reserved constant 0-F Enable ● --- Motor rotation speed Rotary: 1V/1000r/min, Linear: 1V/1000mm/s R Support tool initial value 0002H 2 0 F Pn004 Lower limit 2 Advanced function selection switch 3 0 Unit 2 --- 0000H 1210H --- 0200H ∆ 0 0 ∆...

  • マニュアル

    ...1011 B 1100 C 1101 D 1110 E 1111 F 0000 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0001 1 DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US 0010 2 Space ! ” # $ % & ’ ( ) * + , . / 0011 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 0100 4 @ A B C D E F G H I J K L M N O 0101 5 P Q R S T U V W X Y Z [ \ ] ^ _ 0110 6 a b c d e f g...