全 50423 件が検索されました。(561 - 580件を表示)

  • マニュアル

    ...> 20 3E Code Reader V440-F C-Mount Code Reader Communication Manual (Z453-E1) In Read Cycle Character notatiion 1 Hex notatiion 31 2 32 Read result 3 4 5 33 34 35 CR LF 0D 0A 3-31 3 3-2-3 Communication Settings (Serial (TCP)) Serial Trigger Character (Delimited) 3-2 Controlling Operation and Data Output with Serial (TCP) Additional Information 3 Controlling Operation and Data Output with Ethernet 3-2-4 Setting the Data to Output after a Read The code reader can be configured so that after a Read is executed, its read results are ...

  • マニュアル

    ... is saved when trigger is detected. 👉👉 The external input signal from the camera is “input 0". Please see your camera’s manual for external input signals. 👉👉 For TCP command external input, following command is send to this application. Command trigger n(...

  • マニュアル

    ...,match length,wild card character,sequence on No-Read,sequence on mismatch, placeholder character> 1 1 to 3000 Wild Card Character Usage: Definition: Serial Cmd: Default: Options: Example: With Wild Card Character defined as the default asterisk, defining ...

  • マニュアル

    ...> 20 3E Code Reader In Read Cycle Character notatiion Hex notatiion V460-H Industrial Handheld DPM Reader Communication Manual (Z462-E1) 1 31 2 32 Read result 3 4 5 33 34 35 CR LF 0D 0A 2-33 2 2-2-3 Communication Settings (Serial (TCP)) Serial Trigger Character (Delimited) External device 2-2 Controlling Operation and Data Output with Serial (TCP) Change the Command that Executes Read 2 Controlling Operation and Data Output with Ethernet 2-2-4 Setting the Data to Output after a Read The code reader can be configured so that after a Read ...

  • マニュアル

    ...--- Data bit length 8 bits 8 bits (default) Stop bit 1 bit 1 bit (default) Parity None None (default) Baud rate 115,200 bps 115,200 bps (default) Header --- None (default) Footer --- <CR+LF> (default) Host port protocol --- Point-to-point (default) (connection) port Precautions for Correct Use It is assumed that the NX-CIF210 Serial Communications Unit is used with the unit number 0 and the communications (connection) port Port 2. If using other conditions to connect the Unit, refer to Appendix 2. Ladder Program and create a program by modifying the control data in the CIO Area ...

  • マニュアル

    ...-XC_A: within 10 m (including Sensor Head cable. Extension Cable cannot be daisy-chained.) - Extension Cable: ZS-XC_B(R): within 22 m (including Sensor Head. Up to two Extension Cables can be daisy-chained.) - Extension cable for a long distance ZS-XC_ _...

  • マニュアル

    ...The format of non-procedural commands are as follows: Example: A command to acquire a measured value MEASURE command * Each character is output as an ASCII code (except for FLOWDATA response). M E A S U R E O ...

  • マニュアル

    ..., lighting, and match string, and to call Quickset functions such as Quick Photometry and Quick Focus that actively set up imaging. Serial Command Syntax 1. All Serial Commands start with an ! followed by the command name. All commands must be followed by a carriage return (...

  • マニュアル

    ... as Start/Stop Specifies the command character used to end a Read Cycle. This character must be different from the Start Character. 3  Example: Serial Trigger Command • Read string: 12345, Format Output: Space, Preamble: None, Postamble: \r\n Transmit: S Response: 12345<...

  • マニュアル

    ... in the Watch Tab Page, as shown in the figure on the right. Response Format Read data * The receive data in the figure on the right varies depending 1 2 3 4 5 6 7 8 9 0 A 02 C D E CR LF on your environment. Footer 23 8. Initializing the System 8. Initializing the System This document assumes that each device uses the factory default settings. If you change their settings from the defaults, you may not be able to perform various setting procedures as described. 8.1. Initializing the Controller To initialize the controller, initialize ...

  • マニュアル

    ... in the Watch Tab Page, as shown in the figure on the right. Response Format Read data * The receive data in the figure on the right varies depending 1 2 3 4 5 6 7 8 9 0 A 02 C D E CR LF on your environment. Footer 25 8. Initializing the System 8. Initializing the System This document assumes that each device uses the factory default settings. If you change their settings from the defaults, you may not be able to perform various setting procedures as described. 8.1. Controller To return the controller to its default ...

  • マニュアル

    ...ensures compatibility and efficient communications between different manufacturers and devices. CPU Unit --- A CPU Unit is the central part of a Controller that processes inputs from sensors and actuators, and outputs control signals based on a program. It manages the entire system. ...

  • マニュアル

    ...Host Amplifier Unit A test is preformed for the Amplifier Unit using the data 12345678. Command Test data Command code 1 0 Data 1 1 Data 2 2 3 Data 3 4 5 CR Data 4 6 7 8 0Dh Response If the response test data matches the command, the host device and Amplifier Unit are connected correctly. Test data Response code 0 0 Data 1 1 Data 2 2 3 Data 3 4 V640 SERIES AMPLIFIER UNITS ETHERNET TYPE USER'S MANUAL (Z497) 5 ...

  • マニュアル

    .... 17 Terminology Terminology Term Abbreviation Description CPU Unit --- A CPU Unit is the central part of a Controller that processes inputs from sensors and actuators, and outputs control signals based on a program. It manages the entire system. ...

  • マニュアル

    ... the header. Normally choose RS-232 or RS-485. Choose format 1/format 4. Set the time-out period. Set value for this example Non-procedural 8bit Even 1bit 9600 Yes Regular/RS232C Form1(without CR,LF) 30(300msec) 2-2 RS-232C Serial Communications Connecting to Mitsubishi Electric PLCs Communications cable The suited cable is different according to the combination of component. Please produce the cable of the following connecting wires when connecting with a Mitsubishi Electric Standard PLC FX series. G9SP-series RS-232C Serial Communications Board Connector D-Sub male 9-pin Mitsubishi Electric FX series...

  • マニュアル

    ...いでください。 ・ センサヘッドとセンサコントローラ間のケーブルの延長には、別売りの長距離延長ケーブル形 ZG2-XC□□CR(全長3m、8m、15m、25mを用意しています。 全長には、 センサヘッドのコード部分含まず)を使用します。 延長ケーブルの種類によ...

  • マニュアル

    ... laser beams or electric arc-welding machines) 2. Power Supply and Wiring ・ Reverse connection of power supply is not allowed. Connection to AC power supply is also not allowed. ・ Open-collector outputs should not be short-circuited. ・ Use the Extension Cable ZG2-XC□□...

  • マニュアル

    ... Head and Sensor Controller. The total length differs according to the Extension cable. Extension Cable ZS-XC □A : max. total length 10 m (including Sensors) Extension Cable ZS-XC □B(R) : max. total length 22 m (including Sensors) Extension Cable ZS-XC □...

  • マニュアル

    ... Head and Sensor Controller. The total length differs according to the Extension cable. Extension Cable ZS-XC □A : max. total length 10 m (including Sensors) Extension Cable ZS-XC □B(R) : max. total length 22 m (including Sensors) Extension Cable ZS-XC □...

  • マニュアル

    ...語) 形 ZS-XEQ スマートセンサデジタルイコライザ 取扱説明書 ■定格/性能 2. 配線について・ 本製品は形ZS-XC□□CR、形ZS-XC02D専用品です。 形ZS-XC□□CR、形ZS-XC02Dに接続して使用してください。 ・ 形ZS-XC□□CR、形ZS-XC02D以外に接続すると動作しません。 また、故障の原因...