全 1430 件が検索されました。(421 - 440件を表示)
- マニュアル
... default PF Setting parameter is for shifting the digit. Operation Menu Initial Setting Level Input type Platinum resistance thermometer Input Setting Pt100 JPt100 Thermocouple K Temperature inputs J T Analog input type ...
- マニュアル
.... (b) More than one disconnect switch may be required to de-energize the equipment before servicing. (c) Signal inputs are SELV, limited energy. (d) Caution: To reduce the risk of fire or electric shock, do not interconnect the outputs of different Class 2 circuits. (...
- マニュアル
.... (b) More than one disconnect switch may be required to de-energize the equipment before servicing. (c) Signal inputs are SELV, limited energy. (d) Caution: To reduce the risk of fire or electric shock, do not interconnect the outputs of different Class 2 circuits. (...
- マニュアル
...Altitude Recommended fuse Weight Degree of protection Installation environment Memory protection +1.0 0 Waterproofing is impossible with side-by-side installation. When waterproofing is required, fit watertight packing on the backside of front panel. ...
- マニュアル
... power before starting actual control operations to ensure the correct temperature display. (11) When using adaptive control, turn ON power for the load at the same time as or before supplying power to the Digital Controller. (12) During tuning, ensure that the power for the load (...
- マニュアル
... power before starting actual control operations to ensure the correct temperature display. (11) When using adaptive control, turn ON power for the load at the same time as or before supplying power to the Digital Controller. (12) During tuning, ensure that the power for the load (...
- マニュアル
...X 0 0 0 *1: Upper and lower limits can be set for parameters 1, 4 and 5 to provide for different types of alarm. These are indicated by the letter "L" and "H". • The default alarm type is "2" T E L U N R S B C/W PL II K J T Pt100 4 to 20 mA 0 to 20 mA 1 to 5 V 0 to 5 V 0 to 10 V Setting 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22...
- マニュアル
...ᅝ㺙⾡㉏IIˈ∵ᶧㄝ㑻 2(IEC61010-1) 䴲থݙᄬ ˄ݭ᭄˖1,000,000ˈ⦃๗⏽ᑺ25°C˅ ⦄എ䜡㒓ッᄤ ˄䰘ᏺP2CF-08P2CF-11˅ 䴲䄺䕧ߎൟ⫼ᦦᑻ˄8䩜˅˖ P2CF-08ǃP2CF-08-EP3G-08 䄺䕧ߎൟ⫼ᦦᑻ˄11䩜˅˖ P2CF-11ǃP2CF-11-EP3GA-11 *1 㽕ᓔਃAT˄㞾ࡼ䇗㡖˅ˈ䇋ৠᯊᣝԣϞ䇗䬂ঞ ϟ䇗䬂2⾦ҹϞⳈࠄ⏽ᑺᰒ⼎ᓔྟᰒ⼎DŽ *2 ҙ䄺ᓣϟᰒ⼎DŽ ᔧ䄺ᓣ䗝ᢽᓔ݇䆒㕂...
- マニュアル
... hidden protection key. The E5CS does not have one. ● Protection switch • The protection switch can be turned ON to disable the Up/Down Keys and prevent setting mistakes. • The temperature indication switching key, however, will operate even when the protection switch is ON (i....
- マニュアル
...着取り付け Informazioni precauzionali Potrebbero verificarsi lesioni di lieve entità prodotte da scosse elettriche. Non toccare i terminali mentre è presente l'alimentazione. MANUALE DI ISTRUZIONI Grazie per aver acquistato un prodotto OMRON. Questo manuale descrive le funzioni, le prestazioni ...
- マニュアル
.... Terminal Unit Solderless terminal size M3 In the pack: • E5DC Main Unit Terminal Unit (only provided with the E5DC-□□□□SM-□□□ type) • Instruction manual Sold Separately • Adapter (Y92F-53) • USB-Serial Conversion Cable(E58-CIFQ2) • Conversion Cable (E58-CIFQ2-...
- マニュアル
... key together for at least 1 second to switch Run/Reset. Operation Menu Initial Setting Level Input Type Input type Platinum resistance thermometer Input Setting Pt100 JPt100 Thermocouple K Temperature inputs J T ...
- マニュアル
...个适配器 (Y92F-51): ·前面板设置工具端口盖 (Y92S-P7): 另售件 ·端子盖(E53-COV24) ·USB串行转换电缆(E58-CIFQ2) ·转换电缆(E58-CIFQ2-E) 连接(端子适用性因机器型号而异。 ) 单独安装(mm) 紧密安装(mm) 继电器 250 VAC,5 A (阻性负载) 电压 (用于驱动SSR) 12 VDC,40 mA 1.0 (48 x 台数- 2.5) + 0 紧...
- マニュアル
... the D key together for at least 1 second to switch Run/Reset. Operation Menu Initial Setting Level Input Type Input type Platinum resistance thermometer Input Pt100 JPt100 Thermocouple K Temperature inputs J T ...
- マニュアル
...): • Two adapters (Y92F-51): • Terminal cover (Provided only for models with E5EC-□□□□ 5□.): • Front-panel Setup Tool port cover (Y92S-P7): Sold Separately • Terminal cover: (Model: E53-COV24) • USB-Serial Conversion Cable (E58-CIFQ2) • Conversion Cable (E58-CIFQ2-...
- マニュアル
...□的型号附带): ·前面板设置工具端口盖 (Y92S-P7): 另售件 ·端子盖(型号:E53-COV24) ·USB串行转换电缆(E58-CIFQ2) ·转换电缆(E58-CIFQ2-E) 并排安装(mm) 并排安装无法确保防水性能。 当有防水要求时,请在前面板的后侧安装防水密封圈。 负载:最大500 Ω ∗2 控制输出 RX 45 + 00.6 92 + ...
- マニュアル
... alarm. These are indicated by the letter "L" and "H". • The default alarm type is "2" Analog input type ON OFF RSP absolute value lower limit X ON OFF ON OFF (23) (24) T E L U N R S B C/W PL II K J T Pt100 4 to 20 mA 0 to 20 mA 1 to 5 V 0 to 5 V 0 to 10 V Power supply voltage 100 to 240 VAC, 50/60 Hz or 24 VAC, 50/60 Hz / 24 VDC Operating voltage range 85 to 110% of the rated voltage Power consumption...
- マニュアル
...) -50.00 to 200.00(°C) / -50.00 to 200.00(°F) -50.00 to 200.00(°C) / -50.00 to 200.00(°F) Input type Input Platinum resistance thermometer Pt100 JPt100 K Thermocouple J T E L U N R S B Platinum resistance thermometer Current input Voltage input Pt100 24 4 to 20mA 0 to 20mA 1 to 5V 0 to 5V 25 26 27 28 0 to 10V 29 in-t 5 *6 in-h *6 in-l 100 0 dp *6 0 d-u *6 c sl-h 1300.0 sl-l -200.0 cntl...
- マニュアル
... on the side and bottom of the Digital Controller. Use these ports to connect a personal computer to the Digital Controller when using the Setup Tool. The E58-CIFQ2 USB-Serial Conversion Cable is required to connect to the side-panel port. The E58-CIFQ2-...
- マニュアル
...Specifications Control method Ambient temperature Ambient humidity Storage temperature Altitude Recommended fuse Weight Degree of protection Installation environment 3.4 3.4 8 35.4 35.5 Fig.3 E5L+PTF14A E5L+PTF14A-...