全 559 件が検索されました。(261 - 280件を表示)
- マニュアル
... status of the MECHATROLINK-II. For details, refer to MECHATROLINK-II Status LED Indicator on page 6-4. Rotary Switches Sets the node address. For details, refer to Servo Drive Display and Settings on page 6-3. Forward and Reverse Motor Rotation Reverse (...
- マニュアル
... travels back and forth between the two ends of the green arc. An optional beacon will illuminate green during this operation. 25% 50% 75% 100% Left Right State of Charge Side Light Disc Side Light Disc 0 to 90 ...
- マニュアル
... current SOC. A small white arc travels back and forth between the two ends of the green arc. Beacon blinks green (red if E-Stopped). 25% Left Side 50% 75% Right Side 100% State of Charge 0 to 90 cw 0 to 270 ccw 25% 0 to 180 ...
- マニュアル
..., the AMR scans its path for potential obstacles. It will remain stopped until its path is clear. 4-15-10 Charging 25% 50% 75% 100% Left Right State of Charge Side Light Disc Side Light Disc 0 to 90 cw...
- マニュアル
...An optional beacon will illuminate green during this operation. 25% 50% 75% HD-1500 Platform User's Manual (I645) 100% 4-41 4 Operation Left Right State of Charge Side Light Disc Side Light Disc 0 to 90 ...
- マニュアル
...RUN MING RESET CLIM SG COM AGND AGND Connector plug: MR-25RF (HONDA TSUSHIN KOGYO CO., LTD.) Connector cover: MR-25LK2 (HONDA TSUSHIN KOGYO CO., LTD.) 11 6. Product Specifications [R88A-CPWR0R3P] Symbol GND +...
- マニュアル
... Pulse input When you select position control (pulse train command) mode, input command pulses from the following pulse inputs. Select them according to the specifications of the host controller, then install wiring and set parameters. Host controller Host controller Maximum input frequency of ...
- マニュアル
...や散乱光の目又は皮膚への被ばくを避けること 半導体レーザ Yb:Fiber レーザ最大出力:1mW 最大出力:40W パルス幅:CW 最大ピークパワー:30kW 波長:655nm パルス幅:1-500ns 波長:1062nm クラス4レーザ製品 JIS C 6802: 2014 7 8 Semiconductor laser Yb : Fiber laser Maximum output : 1mW Maximum output : 40W Maximum peak power : 30kW Pulse duration : ...
- マニュアル
...are hazardous when the beam is stared into deliberately". Item Specification MX-Z2000H Remarks MX-Z2050H MX-Z2055H Wavelength 655 nm Visible laser Laser medium Semiconductor laser - Maximum output 1 mW - Laser oscillation type ...
- マニュアル
...Origin Shift.) H Origin Shift • Sets any angle to 0° according to the mechanical origin when the trigger turns ON in RUN mode. (Refer to 3-6-4 Origin Compensation and Origin Shift.) H Backlash Compensation • Sets a difference between the detection angles in ...
- マニュアル
... be controlled between 20 Hz and 1 MHz. • Basic I/O can be used for origin signal and other I/O, and pulse inputs can be used for encoder inputs, for Servomotors/Servo Drivers • For stepping motors, combination with basic I/O and pulse (...
- マニュアル
...Relative mode: 0000 0000 to FFFF FFFF Absolute mode: 8000 0000 to 7FFF FFFF Indicates whether or not the vir- OFF: Pulse output stopped tual pulse output has started. ON: Pulse being output Bit 08 Indicates the direction of virtual OFF: ...
- マニュアル
... 3.1 to Version 3.2 Previous version (unit version 3.1) Unit version 3.2 or later Not in previous version When PULS(886) is used in electronic cam mode (ring), the pulse output can be set to pass through 0 in the ...
- マニュアル
... 3.1 to Version 3.2 Previous version (unit version 3.1) Unit version 3.2 or later Not in previous version When PULS(886) is used in electronic cam mode (ring), the pulse output can be set to pass through 0 in the ...
- マニュアル
...Compensation of the tool edge path according to the tool radius Tool offset Compensation of tool center point path according to the tool length M code output and reset Outputs M codes, and interlocks with sequence control program using reset. Spindle axis ...
- マニュアル
...-6 Reservation Auxiliary Functions ................................................................................................... 3-7 M00 Program Stop ................................................................................................................................... 3-8 M01 Optional Stop.................................................................................................................................... 3-9 M02, M30 End of Program ..................................................................................................................... 3-10 Spindle Axis .................................................................................................................................. 3-11 Spindle Axis Rotation Function (S function) ........................................................................................... 3-12 M03 Spindle ...
- マニュアル
... spindle started by M code. 3 - 43 3-7-3 Soft Control Panel (Velocity Override) Button - 3 Features of CNC Operator Spindle Button The spindle operation is available as a manual operation function. Function name START STOP ORIENTATION ...
- マニュアル
... output in the CPM2A. In this case, do not use a direction signal and not wire anything. Note 2. In pulse + direction mode, allocation for the direction output is different between the CPM2A and CP1E. Note 3. As the CP1E does not have a ...
- マニュアル
...D3 #0000 D4 #27C0 D5 #0009 D6 #0064 D7 #0000 Number of output pulses: 600,000 pulses Starting frequency: 100 Hz (3) Ladder Program Specifies Pulse output 0 Specifies Pulse + direction output method, CW...
- マニュアル
...、未配線としてください。 注 2. CPM2A と CP1E のパルス+方向モードでは、方向時の接点割付が異なっています。 注 3. CP1E は CW/CCW モードを搭載していないため、「パルス+方向」モードを使用するシステムに変更ください。 出力接点 CPM2A CP1E-N タイプ *1 CP1E 単相...