全 414 件が検索されました。(161 - 180件を表示)
- マニュアル
...The Setting Tool can be used to allocate the peak value, bottom value, top value, valley value, rate of change, comparator results, Status Flags, etc. Node address setting No setting required. Baud rate setting No setting required. 156 Poll, Bitstrobe, and ...
- マニュアル
... ROOT • FDIV Instructions Floating-point Math Instructions Double-precision Floating-point Instructions 180 • MCMP • BCMP2 • • • • Instructions • • • • • • • • • • • • RAD DEG SIN COS TAN ASIN ACOS ATAN SQRT EXP LOG PWR • • • • FIXD FIXLD DBL DBLL SYSMAC CP1L/CP1E Introduction Manual Mnemonic • • • • • • • • • • • • • • • • • Table Data Processing Instructions Data Control Instructions lnstructions Basic I/O Unit Instructions Classification • MSG • SCH • SCTRL Clock Instructions • SEC • HMS Debugging Instructions • TRSM Failure Diagnosis • FPD Instructions Other Instructions • • • • CCS CCL FRMCV TOCV Block Programming Instructions • • • • • • • • • • • • • • • • • • • • • BPRG BEND BPPS BPRS EXIT EXIT NOT IF IF NOT ELSE IEND WAIT WAIT NOT TIMW TIMWX CNTW CNTWX TMHW TMHWX LOOP LEND LEND ...
- マニュアル
... the Connection Tab. Automatic connections are set by default. To specify the connections, use the following procedures. 1. Select User Setup. Possible connections are ready for selection. 2. Select the connections. Up to two connections can be selected. Note Both ...
- マニュアル
... Unit Hardware User’s Manual Appendices Basic Output Units CJ1W-OC201 Contact Output Unit (Independent Relays, 8 Points) Name 8-point Contact Output Unit with Terminal Block (Independent Relays) Model CJ1W-OC201 Max. Switching Capacity 2 A 250 VAC (...
- マニュアル
...C 0001 hex S 0000 to 0900 (BCD) 0 ° to 90° --- R 0000 to 9999 (BCD) 9999 (BCD) 0.0000 to 0.9999 1.0000 • Cosine Function (C=0001) When C is 0001, APR(069) calculates the COS(S) and writes the result to R. The range for S is 0000 to 0900 BCD (0.0° to 90.0°) and the range for R is 0000 to 9999 BCD (0.0000 to 0.9999). The remainder of the result beyond the fourth decimal place is eliminated. Note The actual result for SIN(90°) and ...
- マニュアル
...Slave Detailed Status ............................................................................................................... 3-61 Remote I/O Master Communications 4-1-1 4-1-2 4-1-3 4-1-4 4-2 Software Switches 1 ................................................................................................................... 3-9 Software Switches 2 (n + 1CH) ................................................................................................ 3-18 Master ...
- マニュアル
...) = ERROR& Return EndIf If ANGLE# > 180 Then RADIAN# = (ANGLE# - 360) / 180 * PI# Elseif ANGLE# <= -180 Then ANGLE# = RADIAN# = (ANGLE# + 360) / 180 * PI# Else RADIAN# = ANGLE# / 180 * PI# EndIf RBT_X0# = FOV_ORIGN_X# RBT_X1# = FOV_ORIGN_X# + ...
- マニュアル
... inspection item 0 Function List The following functions can be used in calculations. 68 Function Description SIN Finds the sine. The result is a value between −1 and 1. The angle in the expression is in degrees. SIN(angle) ...
- マニュアル
... for inspection item 0 Mathematical operator Area of label 0 for inspection item 0 328 Calculations and Judgments Using Inspection Item Data FQ2-S/CH User’s Manual Function List The following functions can be used in calculations. Function Description ...
- マニュアル
...Current Error UB Output Over Current Error UL Muting Lamp Status TO7 Muting Lamp Status TO3 Global Safety Input Status CIS Global Safety Output Status COS Input Power Error UB Output Power Error UL Safety Inputs Safety Input Status Bit 10 Safety Input Status I10 Bit 9 Safety Input Status I9 Bit 8 Safety Input Status I8 Bit 7 Safety Input Status I7 Bit 6 Safety Input Status I6 Bit 5 Safety Input Status I5 Bit 4 Safety Input Status I4 The target variable and its size must be Assembly and Size values listed in the Bit 3 Safety Input...
- マニュアル
...Default (Assembly instance number) Safety input assembly 1 (Instance No. 20C) None IN OUT Standard Connections: The default values for each type of connection are given below. Connection Poll IN OUT Bit strobe IN OUT ...
- マニュアル
... Tab. The default setting is Auto Connection. Use the following procedure to specify a connection. 1. Select the User Setup Option. Settings will be enabled for connections. 2. Select the connections to use. Up to two connections can be set. Note ...
- マニュアル
...The NE1A-series Controller simultaneously functions as the Safety Master and a Standard Slave. As a Standard Slave, the NE1A-series Controller enables standard I/O communications for a maximum of two connections with up to 16 bytes per connection. Four protocols (i.e., Poll, Bitstrobe, ...
- マニュアル
...parameters that have been set related to safety functions have been verified. A logical communications path used to communicate between devices. connection type The connection types are as follows depending on the communications method. DeviceNet Standard Communications • Poll connection • Bit-strobe connection • ...
- マニュアル
... for IN and OUT) With multi-cast inputs, however, communications is possible for a maximum of 15 Safety Masters. • Connection type: Single-Cast, Multi-Cast Standard I/O Standard Slave Function communications • Maximum number of connections: 2 • Connection type: Poll, Bit-strobe, ...
- カタログ
...Performs addition, subtraction, multiplication, division, and power operations. REMAINDER % Finds the remainder in division operations. OR/XOR/AND/NOT |, ., &, ! Performs logical OR, XOR, AND, and NOT operations. ABSOLUTE ABS Finds the absolute value. SINE, COSINE, ASINE, ACOSINE SIN, ...
- カタログ
...、&、! 論理和/排他的論理和/論理積/ビット反転をします。 絶対値 ABS 絶対値を求めます。 正弦/余弦/逆正弦/逆余弦 SIN、COS、ASIN、ACOS 正弦/余弦/逆正弦/逆余弦を求めます。 正接/逆正接 TAN、ATAN 正接/逆正接を求めます。 平方根/指数/自然対数 SQR、EXP、LOG 平方根/指数/自然対...
- カタログ
...Performs addition, subtraction, multiplication, division, and power operations. REMAINDER % Finds the remainder in division operations. OR/XOR/AND/NOT |, ., &, ! Performs logical OR, XOR, AND, and NOT operations. ABSOLUTE ABS Finds the absolute value. SINE, COSINE, ASINE, ACOSINE SIN, ...
- カタログ
...、&、! 論理和/排他的論理和/論理積/ビット反転をします。 絶対値 ABS 絶対値を求めます。 正弦/余弦/逆正弦/逆余弦 SIN、COS、ASIN、ACOS 正弦/余弦/逆正弦/逆余弦を求めます。 正接/逆正接 TAN、ATAN 正接/逆正接を求めます。 平方根/指数/自然対数 SQR、EXP、LOG 平方根/指数/自然対...
- カタログ
...50 x 50 mm flat plate Ultrasonic oscillation frequency Approx. 40 kHz Directional angle Half-value angle: 25° Response time Operate time: 0.25 s; release time: 0.5 s Control output Contact output: SPDT 3 A at 220 VAC, ...