全 414 件が検索されました。(141 - 160件を表示)
- マニュアル
.../3) Purpose: To round off a numeric value at the decimal point and convert it into an integer Format: CINT(
) Example: A = CINT(B#) Purpose: To return the cosine of the numeric value given by the argument Format: ... - マニュアル
...ALM ADJ Connector for resolver Insert the connector so that the cable will be pointing downward. Connector Pin Wiring Cam Positioner Unit 1 2 3 4 5 6 7 8 Sin(+) Sin(−) Cos(+) Cos(−) OUT(+) OUT(−) ----Connector case Resolver Sin(+) Sin(−) FG ...
- マニュアル
... to 0900 (0°≤ ≤ 90°). Description When the execution condition is OFF, APR(69) is not executed. When the execution condition is ON, the operation of APR(69) depends on the control word C. If C is #0000 or #0001, APR(69) computes sin() or ...
- マニュアル
... for LRC (longitudinal parity), CRC-CCITT (XMODEM), CRC-16 (MODBUS), and SUM (1-byte or 2-byte). This allows you to eliminate the programming previously required to calculate error check codes. Special Operations Calculations are possible for exponential function (ex), square root (√), trigonometric functions (TAN, SIN, and ...
- マニュアル
...be necessary to directly input settings such as the connection type and data size. (Always select the connection type that is supported by the Slave.) The following connection types are allowed in DeviceNet communications. Connection type poll bit strobe change of state (...
- マニュアル
... them to the SYSMAC-CPT, an error will occur. Timer Instructions TTIM Serial Communications Instructions PMCR and STUP Network Communications Instructions SEND, RECV, and CMND Floating-point Instructions FIX, FIXL, FLT, FLTL, +F, –F, *F, /F, DEG, RAD, SIN, ...
- マニュアル
... T1 Optical Fiber Twist-relief Cable device Pull line Winch The pulling tension (T) on the cable can be calculated from the tension reading (T1) at the pulley and the angle (θ) at the pulley. T= T1 θ 2 ...
- マニュアル
... characters Max. 6 characters Max. 16 characters (Unusable characters: None) Fixed for each function block item Max. 16 characters (Unusable characters: None) 0: Analog, 1: Contact Analog 0: Default, 1: Unit, 2: Integer Contact 0: OFF, 1: ON, 2: ...
- マニュアル
... be used whenever the size relationship can be expressed in the conditional statement. The operators that can be used in the conditional statement and calculation expressions are as follows: Symbol + * / ABS(x) ACOS(x) ASIN(x) ATAN(x) ...
- マニュアル
... is either in BIN 16 bit or BIN 32 bit. 180 Section 7-14 Improved Instructions In 32 Bit [D]: Calculation result (rightmost 4 digits) [D+1]: Calculation result (leftmost 4 digits) In 16 Bit [D]: Calculation result (4 digits) SIN/...
- マニュアル
... commands through serial connection Inter-network communications Other funcRemote programtions ming/monitoring Configurator operations through serial connection Memory Card backup function Master Unit error log function Communications cycle time setting Message monitoring timer ...
- マニュアル
... DM Area words. Specifications Section 1-3 Item Supported connections (communications) Remote I/O Slave allocation method master communications Fixed allocations User-set allocations Specifications • Remote I/O communications (master and slave): Master/slave connection (poll, bit-strobe, ...
- マニュアル
... nodes capable of simultaneous communications as explicit servers Data length for explicit messages Response monitoring time for explicit messages (for clients) Retries for explicit messages Note Minimum System Requirements Specifications • Bit Strobe • Polling • Cyclic • Change of State (...
- マニュアル
... Setting master remote I/O communications connections. • Setting slave remote I/O communications connections. • Enabling or disabling device data checks through remote I/O communications (checks on slave vendor, device type, and product code data). • Setting an explicit message monitor timer list. • Setting a ...
- マニュアル
...SINE SIN/ @SIN 460 Calculates the sine of a 32-bit floating-point number (in radians) and places the result in the specified result words. OK OK OK OK OK OK OK OK COSINE COS/ @COS 461 Calculates the cosine of a 32-bit floating-point number (in radians) and places the result in the specified result words. OK OK OK OK OK OK OK OK TANGENT TAN/ @TAN 462 Calculates the tangent of a 32-bit floating-point number (in radians) and places the result in the specified result words. OK OK OK OK OK OK OK OK FloatingFLOATING ...
- マニュアル
...Section 3-1 Common Slave Specifications 3-1 Common Slave Specifications 3-1-1 Communications Specifications Item Communications protocol Supported connections (communications) Connection forms Specifications DeviceNet Remote I/O: Master-Slave connection (Poll/Bit-Strobe/...
- マニュアル
...2nd Term 3rd Term AND (Logical AND) & #MW- = #MW- 1st Term & #MW-; 2nd Term 3rd Term Functions NOT (Reverse) ! Absolute value ABS Sine SIN Cosine Tangent ARC Sine COS TAN ASIN ARC Cosine ACOS ARC Tangent ATAN Square root SQR Normal logarithm EXP Natural logarithm LOG Decimal point Variable R/W B W L F @ --- No No Write Yes Yes Yes No No LONGMINLONGMAX Yes Integer Read Yes Yes Yes No Yes LONGMINLONGMAX Yes Integer Read Yes Yes Yes No Yes --- No No Write No Yes Yes No No LONGMINLONGMAX Yes Integer Read No Yes Yes No Yes LONGMINLONGMAX Yes...
- マニュアル
...: LOG10 argument EXP (argument) (See note 1.) REAL, LREAL REAL, LREAL a: = EXP (b) (*natural exponential of variable b stored in variable a*) Sine: SIN argument a: = SIN (b) (*sine of variable b stored in variable a*) Cosine: ...
- マニュアル
...code 0372h 200Eh 200Eh The following operand has exceeded the range. • Q (MOVEC, MOVETRAV, MOVELINK, CAMBOX) 0379h Correct the applicable operands. 200Fh 200Fh The following operands have exceeded the range. • K (CAM, CAMBOX) • B (MOVELINK, CAMBOX, CONNECT, SYNC, ADDAX) • TORQUE • SIN, ...
- マニュアル
... and select Parameter – Edit – General, and then select the Smart Slave to be set. Node Address Settings and I/O Allocation Section 2-2 2. Click the Advanced Setup Button, click the Connection Tab, and select User Setup. Select Use Poll Connection and Use ...