全 559 件が検索されました。(101 - 120件を表示)

  • マニュアル

    ...Expansion connector Control I/O connector Safety connector Encoder connector External encoder connector ■ Control I/O connector ● Pulse input Input the command pulse of for position control. SS2 series Terminal No. Symbol Name 22 +...

  • マニュアル

    ...AVOID EYE OR SKIN EXPOSURE TO DIRECT OR SCATTERED RADIATION Yb:Fiber レーザ半導体レーザ最大出力:40W 最大出力:1mW 最大ピークパワー:30kW パルス幅:CW パルス幅:1-500ns 波長:655nm 波長:1062nm クラス4レーザ製品 JIS C 6802: 2014 ■放射範囲 Yb : Fiber laser Semiconductor laser Maximum output : 40W Maximum output : 1mW Maximum peak power : 30kW Pulse duration : ...

  • マニュアル

    ...29m 57m φ17m φ31m φ60m Specification Remarks MX-Z2000H-V1 MX-Z2050H-V1 MX-Z2055H-V1 Wavelength 655 nm Visible laser Laser medium Semiconductor laser - Maximum output 1 mW - Laser oscillation type CW (continuous wave) - Class - 2 Controller.....1 Marker head.....1 System key.....2 Marker head control cable.....1 Marker head power supply cable.....1 The JIS (Japanese), EN (English), and EN (German/French) laser warning labels are affixed on the marker head. GB (simplified) and IEC (traditional) warning labels are also included. Affix the appropriate label according to the regulations and standards in the country/region the product ...

  • マニュアル

    ...Compensation of the tool edge path according to the tool radius Tool offset Compensation of tool center point path according to the tool length M code output and reset Outputs M codes, and interlocks with sequence control program using reset. Spindle axis ...

  • マニュアル

    ...-6 Reservation Auxiliary Functions ................................................................................................... 3-7 M00 Program Stop ................................................................................................................................... 3-8 M01 Optional Stop.................................................................................................................................... 3-9 M02, M30 End of Program ..................................................................................................................... 3-10 Spindle Axis .................................................................................................................................. 3-11 Spindle Axis Rotation Function (S function) ........................................................................................... 3-12 M03 Spindle ...

  • マニュアル

    ... spindle started by M code. 3 - 43 3-7-3 Soft Control Panel (Velocity Override) Button - 3 Features of CNC Operator Spindle Button The spindle operation is available as a manual operation function. Function name START STOP ORIENTATION ...

  • マニュアル

    ... output in the CPM2A. In this case, do not use a direction signal and not wire anything. Note 2. In pulse + direction mode, allocation for the direction output is different between the CPM2A and CP1E. Note 3. As the CP1E does not have a ...

  • マニュアル

    ...: 100 kHz Increment/decrement pulse: 100 kHz Pulse + direction: 100 kHz Phase difference: 50 kHz Increment pulse: 100 kHz (3) Using pulse outputs The CP2E has been enhanced to a maximum of 4 axes. The CP2E pulse output method does not support ...

  • マニュアル

    ...D3 #0000 D4 #27C0 D5 #0009 D6 #0064 D7 #0000 Number of output pulses: 600,000 pulses Starting frequency: 100 Hz (3) Ladder Program Specifies Pulse output 0 Specifies Pulse + direction output method, CW...

  • マニュアル

    ...LREAL LREAL LREAL LREAL UINT LREAL LREAL LREAL LREAL LREAL 設定値 150 220 500 10 62.5 MC_Group000 MC_Axis000 MC_Axis001 MC_Axis002 MC_Axis003 CW 0 0 0 0 表示 80 -379 325 150 100 240 種類 A A A A A B B B B B B B B B B C A A A A A A ロボット 1 の原点位置は以下のように設定します。 35 Delta3/Delta3R の設定値が完了した...

  • マニュアル

    ...、未配線としてください。 注 2. CPM2A と CP1E のパルス+方向モードでは、方向時の接点割付が異なっています。 注 3. CP1E は CW/CCW モードを搭載していないため、「パルス+方向」モードを使用するシステムに変更ください。 出力接点 CPM2A CP1E-N タイプ *1 CP1E 単相...

  • マニュアル

    ...ス:10kHz ③パルス出力を使用する場合 CP2E のパルス出力点数は最大 4 軸に強化されています。 CP2E のパルス出力方式は、CW/CCW に対応していません。 また S 字加減速カーブの指定はできません。 接点機能割付出力出力接点 100.00 100.01 100.02 100.03 CP1L CP1L-L10□...

  • マニュアル

    ...1 1 原点検出方法 0 原点検出方法 1 原点検出方法 2 値(Hex) パルス出力 0 原点サーチ方向指定 0 1 CW 方向 CCW 方向 付録-11 アドレス 259 □□□□ 258 □□□□ (CJ1M CPUユニット 内蔵入出力機能搭載タイプのみ) 値(Hex) パルス出力 0 原点サーチ / 原点復帰起動速度 00000000 ∼ 000186A0 ...

  • マニュアル

    ...可能。 ・ ユニット内の EEP-ROM に保存。 ・ サポートツール SYSMAC NCT により読み出し、パソコンのハードディスクなどに保存。 CW,CCW 限界入力信号原点近傍入力信号原点入力信号原点ラインドライバ(エンコーダ Z 相)入力信号即停止入力信号位置決め完...

  • マニュアル

    ...パルス周波数 原点サーチ減速比率 2000Hz/4ms 原点サーチ加速比率 2000Hz/4ms 原点サーチ近傍速度 1000Hz CCW 付 CW 原点サーチ方式 付録 設定 CW 原点サーチ方向指定 説明 CW方向に原点サーチを実行します。 原点検出方法指定 方法0 原点近傍入力信号の「OFF→...

  • マニュアル

    ...) CPU65 (-EIP) CPU66 (-EIP) CPU 13/33 CPU 14/34 CPU 15/35 最大 4 点 (パルス I/O ブロック 1 台あたり 2 点) 出力方式:CW/CCW、パルス+方向(配線およびラダー命令により選択) 出力周波数:1pps ∼ 100kpps (1pps 単位で指定) 出力モード:連続モード(速度制御用) 、単独モード(位置制御用) 出力...

  • マニュアル

    ...転開始時 : 100,000pps 名称 1 初期値 設定値の範囲 原点サーチ機能使用 使用しない 使用しない 1-1 CW CW 反映タイミング電源 ON 時 使用する原点サーチ方向指定 運転開始時 CCW 1-2 原点検出方法指定 方法 0 方法 0 運転開始時 方法 1 方法 2 1-3...

  • マニュアル

    ....01 が OFF → ON となったとき、INI 命令により、パルス出力を停止します。 0.00 @SPED #0000 パルス出力 #0100 パルス+方向出力 CW方向 連続モード D100 01F4 D101 0 目標周波数 500Hz D100 0.01 @INI #0000 パルス出力0 #0003 パルス出力停止 0 2 - 310 (使用していません) CP シリーズ CP1E/CP2E ...

  • マニュアル

    ...PTP(ABS) PTP(INC) 直線補間 (ABS) 直線補間 (INC) 円弧補間(通過点指定/ABS) 円弧補間(通過点指定/INC) 円弧補間(中心点指定/CW/ABS) 円弧補間(中心点指定/CW/INC) 円弧補間(中心点指定/CCW/ABS) 円弧補間(中心点指定/CCW/INC) 円弧補間(半径指定/...

  • マニュアル

    ...タ回転方向を切り替えることができます。 設定値の説明設定値 0 1 説明正転側指令時に、モータ回転方向は CW となります。 正転側指令時に、モータ回転方向は CCW となります。 • モータの回転方向は、負荷側の軸から見て時計回りが ...