全 2903 件が検索されました。(781 - 800件を表示)
- マニュアル
...-R before replacing the End Cap. Function End Cap Description Black 24 V Active (factory default setting) White 0 V Active External Test Input Selection - Do not remove the insulating rubber attached to the End Cap. Failure to do ...
- マニュアル
... Code A (factory default setting) Black Scan Code B White Scan code Selection *In the Wired Synchronization, F3SG-PG can prevent mutual interference in up to 3 sets. • Do not remove the insulating rubber attached to the End Cap. Failure to do ...
- マニュアル
...undetected, resulting in serious injury. Make sure to install the F3SG-PG at the safety distance from the hazardous part of the machine. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
...screws Fig. 5 • Tightening screws with a torque that considerably exceeds the recommended torque may cause failure. 10 F3SG-SR-K Quick Installation Manual Wiring Mounting Operation check ■Proper Mounting (Proper Mounting Orientation) Mount the emitter and receiver ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SG-SR at the safety distance from the hazardous part of the machine. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SG-SR at the safety distance from the hazardous part of the machine. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
... Code A (factory default setting) Black Scan Code B White Scan code Selection *In the Wired Synchronization, F3SG-SR can prevent mutual interference in up to 3 sets. • Do not remove the insulating rubber attached to the End Cap. Failure to do ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SJ at the safe distance from the hazardous part of the equipment. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
...-01TS series user's manual. 5-1. Mutual Interference Prevention ■Series Connection Series connection can prevent mutual interference when multiple sensors are used. Up to 3 sets, 240 beams, can be connected. The emission of series-connected F3SJ-A-01TS is time-divided, ...
- マニュアル
... include it to calculation of safety distance. Otherwise safety distance may be reduced, resulting in serious injury. The muting and override functions disable the safety functions of the device. You must ensure safety using other method when these functions are operating. Install muting sensors ...
- マニュアル
...-TS series user's manual. 5-1. Mutual Interference Prevention ■Series Connection Series connection can prevent mutual interference when multiple sensors are used. Up to 3 sets, 240 beams, can be connected. The emission of series-connected F3SJ-A-TS is time-divided, ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SJ at the safe distance from the hazardous part of the equipment. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
...F3SJ-A series user's manual. 5-1. Mutual Interference Prevention ■Series Connection Series connection can prevent mutual interference when multiple sensors are used. Up to 4 sets, 400 beams, can be connected. The emission of series-connected F3SJ-A is time-divided, ...
- マニュアル
... a hazardous area. Install protective cover(s) or fence(s). To prevent personnel approach to dangerous part of the machine through an area disabled by the fixed blanking function, you must install a protective structure to cover the whole disabled area. Failure to do ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SJ at the safe distance from the hazardous part of the equipment. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
... to F3SJAM series user's manual. 5-1. Mutual Interference Prevention ■Series Connection Series connection can prevent mutual interference when multiple sensors are used. Up to 4 sets, 400 beams, can be connected. The emission of series-connected F3SJ-AM is time-divided, ...
- マニュアル
... between two F3SJ-Bs in series connection: 7 m max. No Connection Mutual interference is prevented in up to 3 sets, using interference light avoidance algorithm. If 4 or more sets of F3SJ-E/B are installed and are not connected to each other, arrange them ...
- マニュアル
... two F3SJ-B-01Ts in series connection: 7 m max. No Connection Mutual interference is prevented in up to 3 sets, using interference light avoidance algorithm. If 4 or more sets of F3SJ-B-01T are installed and are not connected to each other, arrange them ...
- マニュアル
... two F3SJ-B-01TSs in series connection: 7 m max. No Connection Mutual interference is prevented in up to 3 sets, using interference light avoidance algorithm. If 4 or more sets of F3SJ-B-01TS are installed and are not connected to each other, arrange them ...
- マニュアル
... two F3SJ-B-02TSs in series connection: 7 m max. No Connection Mutual interference is prevented in up to 3 sets, using interference light avoidance algorithm. If 4 or more sets of F3SJ-B-02TS are installed and are not connected to each other, arrange them ...